<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックWhich USB to power the FRDM-MCXA153 when using external MCU Link Debug Probe?</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Which-USB-to-power-the-FRDM-MCXA153-when-using-external-MCU-Link/m-p/2389933#M5597</link>
    <description>&lt;P&gt;Hello, I am new to NXP microcontrollers and the MCUxpresso IDE. I have purchased the FRDM-MCXA153 and also the MCU-Link Debug Probe. I want to use the external debug probe because that is what I will use on my custom printed circuit board. I have gotten the Blinky LED example code working and with using the external debug port J18 with the MCU-Link Debug Probe.&lt;/P&gt;&lt;P&gt;My question is which USB connector on the FRDM board should I use to power the board J18 or J8 while I an using the external debugger?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Thu, 02 Jul 2026 21:17:05 GMT</pubDate>
    <dc:creator>joe1652</dc:creator>
    <dc:date>2026-07-02T21:17:05Z</dc:date>
    <item>
      <title>Which USB to power the FRDM-MCXA153 when using external MCU Link Debug Probe?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Which-USB-to-power-the-FRDM-MCXA153-when-using-external-MCU-Link/m-p/2389933#M5597</link>
      <description>&lt;P&gt;Hello, I am new to NXP microcontrollers and the MCUxpresso IDE. I have purchased the FRDM-MCXA153 and also the MCU-Link Debug Probe. I want to use the external debug probe because that is what I will use on my custom printed circuit board. I have gotten the Blinky LED example code working and with using the external debug port J18 with the MCU-Link Debug Probe.&lt;/P&gt;&lt;P&gt;My question is which USB connector on the FRDM board should I use to power the board J18 or J8 while I an using the external debugger?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jul 2026 21:17:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Which-USB-to-power-the-FRDM-MCXA153-when-using-external-MCU-Link/m-p/2389933#M5597</guid>
      <dc:creator>joe1652</dc:creator>
      <dc:date>2026-07-02T21:17:05Z</dc:date>
    </item>
    <item>
      <title>Re: Which USB to power the FRDM-MCXA153 when using external MCU Link Debug Probe?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Which-USB-to-power-the-FRDM-MCXA153-when-using-external-MCU-Link/m-p/2394616#M5634</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138937"&gt;@joe1652&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;I recommend using J8 as the power supply input.&lt;/DIV&gt;
&lt;P&gt;Thank you.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jul 2026 04:03:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Which-USB-to-power-the-FRDM-MCXA153-when-using-external-MCU-Link/m-p/2394616#M5634</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2026-07-14T04:03:35Z</dc:date>
    </item>
  </channel>
</rss>