<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: 32-Bit Parallel Receive on Rising Edge Pin (FRDM-MCXN947)</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2388551#M5592</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264226"&gt;@Flexin_On_The_IO&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your post!&lt;/P&gt;
&lt;P&gt;Could you please share the current behavior you see in your register?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Which test data are you trying to receive and what you currently get?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please share which MCXN are you using?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Is it a custom board? if not, please specify the board you are using&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 30 Jun 2026 17:37:59 GMT</pubDate>
    <dc:creator>carlos_o</dc:creator>
    <dc:date>2026-06-30T17:37:59Z</dc:date>
    <item>
      <title>32-Bit Parallel Receive on Rising Edge Pin (FRDM-MCXN947)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2387811#M5586</link>
      <description>&lt;P&gt;I am currently trying to configure a 32-bit parallel Shifter to receive data from an external device with one of the pins (FLEX_D4/DATA_VALID) being used as a signal to Shift in the data.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;The progress I have made has allowed me to read in the 32-bit data when DATA_VALID has triggered and move the data into an eDMA Ping-Pong buffer. I am currently testing through Printf statements of reading the buffer data to a console and if the Shifter has any errors (usually indicating Overrun according to the datasheet) they will print to the console as well.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I believe my main issue is with the TimerConfig as it is triggering the Shifter to read too many times on one rising edge of DATA_VALID but I have not found a configuration that allows me to read only once while actually moving the correct data.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Console Output:&amp;nbsp;&lt;/P&gt;&lt;P&gt;Reading Buffer A: 0x3fffefff&lt;BR /&gt;Shifter Error Code: 0x8&lt;BR /&gt;Shifter Status: 0x0&lt;BR /&gt;SHIFTSDEN: 0x8&lt;BR /&gt;DMA CSR: 0x0&lt;BR /&gt;DMA Error: 0x0&lt;BR /&gt;TCD BITER: 0x2 CSR: 0x12&lt;BR /&gt;CH_MUX: 0x40&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Reading Buffer B: 0x3fffefff&lt;BR /&gt;Shifter Error Code: 0x8&lt;BR /&gt;Shifter Status: 0x0&lt;BR /&gt;SHIFTSDEN: 0x8&lt;BR /&gt;DMA CSR: 0x0&lt;BR /&gt;DMA Error: 0x0&lt;BR /&gt;TCD BITER: 0x2 CSR: 0x12&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;My FLEX_IO setup is attached.&amp;nbsp;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jun 2026 14:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2387811#M5586</guid>
      <dc:creator>Flexin_On_The_IO</dc:creator>
      <dc:date>2026-06-29T14:46:27Z</dc:date>
    </item>
    <item>
      <title>Re: 32-Bit Parallel Receive on Rising Edge Pin (FRDM-MCXN947)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2387820#M5587</link>
      <description>&lt;P&gt;Update: I was able to deduce that "&lt;SPAN&gt;kFLEXIO_TimerDisableOnTriggerFallingEdge&lt;/SPAN&gt;" was keeping my CPU in the callback.&lt;BR /&gt;&lt;BR /&gt;I believe I want to disable after a Timer Compare but with this option SHIFTBUF only reports a value of 0x0 but with no SHIFTERR flag.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jun 2026 15:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2387820#M5587</guid>
      <dc:creator>Flexin_On_The_IO</dc:creator>
      <dc:date>2026-06-29T15:33:27Z</dc:date>
    </item>
    <item>
      <title>Re: 32-Bit Parallel Receive on Rising Edge Pin (FRDM-MCXN947)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2388551#M5592</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264226"&gt;@Flexin_On_The_IO&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your post!&lt;/P&gt;
&lt;P&gt;Could you please share the current behavior you see in your register?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Which test data are you trying to receive and what you currently get?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please share which MCXN are you using?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Is it a custom board? if not, please specify the board you are using&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jun 2026 17:37:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2388551#M5592</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-06-30T17:37:59Z</dc:date>
    </item>
    <item>
      <title>Re: 32-Bit Parallel Receive on Rising Edge Pin (FRDM-MCXN947)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2388562#M5593</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241501"&gt;@carlos_o&lt;/a&gt;&amp;nbsp;thank you for the reply!&lt;/P&gt;&lt;P&gt;I was able to get the Timer reading on DATA_VALID edge like I wanted but did not update the thread. My current code is attached.&lt;/P&gt;&lt;P&gt;The problem I am facing now is getting the FlexIO to keep up with other devices. In my current setup I am basically sampling DATA_VALID and at higher speeds, the Shifter can get Overrun. My thinking is that my design requires a shared clock between the MCX &amp;amp; host device that would be sending the 32-bit data. I can use a pin within the 32-bit data bus to be this signal so I do not need to breakup the FlexIO pins. Any input on this idea would be welcome!&lt;BR /&gt;&lt;BR /&gt;To answer your previous questions:&lt;/P&gt;&lt;P&gt;1. The registers are populating as intended at lower speeds. On every DATA_VALID falling edge, the SHIFTBUF stores data from the 32 Pins and the EDMA transfers to my Ping-Pong buffer via a Scatter-Gather method.&lt;/P&gt;&lt;P&gt;2. I am simulating input through an Analog Discovery 2, since that only has 16 data pins I am just writing the upper values of the 32-bits, simulating a clock on the DATA_VALID pin, and tying the unused pins down. Test data is matching correctly at low speeds.&lt;/P&gt;&lt;P&gt;3. I am using the FRDM-MCXN947&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jun 2026 17:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2388562#M5593</guid>
      <dc:creator>Flexin_On_The_IO</dc:creator>
      <dc:date>2026-06-30T17:54:16Z</dc:date>
    </item>
    <item>
      <title>Re: 32-Bit Parallel Receive on Rising Edge Pin (FRDM-MCXN947)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2389968#M5598</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264226"&gt;@Flexin_On_The_IO&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Apologize the late reply,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please specify the speeds you are trying to achieve?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You could review&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/AN14284/page/topics/introduction.html" target="_blank"&gt;AN14284: Timing Parameter Tuning for FlexIO Emulated Interface&lt;/A&gt;, this app note could have some helpful information to your goal.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jul 2026 22:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2389968#M5598</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-07-02T22:25:34Z</dc:date>
    </item>
    <item>
      <title>Re: 32-Bit Parallel Receive on Rising Edge Pin (FRDM-MCXN947)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2393793#M5625</link>
      <description>&lt;P&gt;Hello again,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241501"&gt;@carlos_o&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The bare minimum speed I am trying to reach is 18.5MHz. I can confirm the Shifter does keep up at around 6.25MHz but I was having issues at higher speeds due to my hardware limitations :P.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below is my Analog Discovery 2 waveform where I am just providing the MCLK signal, a binary counter for the data (12-bit only due to low pin count on AD2), and manually controlling the DATA_VALID signal.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Flexin_On_The_IO_0-1783689475176.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/392001i58079F617D00D1C1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Flexin_On_The_IO_0-1783689475176.png" alt="Flexin_On_The_IO_0-1783689475176.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When I get to higher frequencies (20 MHz) I realize the AD2 cannot actually provide a decent square wave and may be causing my FRDM to trigger undesired Shifts due bad signal integrity.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Flexin_On_The_IO_1-1783690391552.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/392005i887F450F1EA6C61A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Flexin_On_The_IO_1-1783690391552.png" alt="Flexin_On_The_IO_1-1783690391552.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I was looking at the file you sent me and I think it may be a solution to an issue I want to take care of. If DATA_VALID rises/falls at the same time as MCLK I believe it misses the a Shift of data since the clock was not able to fully decrement.&lt;/P&gt;&lt;P&gt;My main question is do the Shifters usually require a delayed clock/Timer in order to complete their full shift cycle even after the Trigger from the other device has gone low? My current setup requires the DATA_VALID to remain high between MCLK edges to not miss the data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jul 2026 14:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/32-Bit-Parallel-Receive-on-Rising-Edge-Pin-FRDM-MCXN947/m-p/2393793#M5625</guid>
      <dc:creator>Flexin_On_The_IO</dc:creator>
      <dc:date>2026-07-10T14:00:27Z</dc:date>
    </item>
  </channel>
</rss>