<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Spi communication with arduino in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Spi-communication-with-arduino/m-p/1901158#M557</link>
    <description>&lt;UL&gt;&lt;LI&gt;FRDM33772BSPIEVB&lt;/LI&gt;&lt;LI&gt;Evaluation Board for MC33772 with SPI Communication.&lt;/LI&gt;&lt;LI&gt;This board need to communicated with arduino uno with spi how to do it any references for it.&lt;/LI&gt;&lt;LI&gt;also checked the document but no register related information found.. Any supportive document for this??&lt;/LI&gt;&lt;LI&gt;Thanx : )&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Sun, 07 Jul 2024 13:23:45 GMT</pubDate>
    <dc:creator>Texe07</dc:creator>
    <dc:date>2024-07-07T13:23:45Z</dc:date>
    <item>
      <title>Spi communication with arduino</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Spi-communication-with-arduino/m-p/1901158#M557</link>
      <description>&lt;UL&gt;&lt;LI&gt;FRDM33772BSPIEVB&lt;/LI&gt;&lt;LI&gt;Evaluation Board for MC33772 with SPI Communication.&lt;/LI&gt;&lt;LI&gt;This board need to communicated with arduino uno with spi how to do it any references for it.&lt;/LI&gt;&lt;LI&gt;also checked the document but no register related information found.. Any supportive document for this??&lt;/LI&gt;&lt;LI&gt;Thanx : )&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Sun, 07 Jul 2024 13:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Spi-communication-with-arduino/m-p/1901158#M557</guid>
      <dc:creator>Texe07</dc:creator>
      <dc:date>2024-07-07T13:23:45Z</dc:date>
    </item>
    <item>
      <title>Re: Spi communication with arduino</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Spi-communication-with-arduino/m-p/1903034#M716</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236125"&gt;@Texe07&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can check the user guide in order to see some specification of how to use the FRDM33772BSPIEVB with Arduino UNO.&lt;/P&gt;
&lt;P&gt;The first thing would be the connections, since the SPI modules in both boards need to be connected correctly.&lt;BR /&gt;&lt;EM&gt;See Table 12. Jumper Setting to Work with Arduino R3 of the user guide.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;Once the connections are correct you can check the information about the SPI interface in the user guide.&lt;BR /&gt;&lt;EM&gt;See section 4.13 SPI communication interface of the user guide.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;Since Arduino UNO is not a NXP product we don't have any specific documentation regarding the implementation of the FRDM33772BSPIEVB with Arduino UNO, but you can take a look to the following post where it explains the SPI communication setup between S32K1xx boards and MC3377xBSPI Battery Cell Controllers.&lt;/P&gt;
&lt;P&gt;Post: &lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/BMS-amp-MBDT-MC33771B-MC33772B-SPI-communication-with-S32K/ta-p/1152835" target="_blank"&gt;MC33771B/MC33772B communication with S32K on SPI (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, you can refer to the following GUI design based on KL25Z.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pablo_Ramos_1-1720471735661.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/287624i6B87E0C94EE7B012/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pablo_Ramos_1-1720471735661.png" alt="Pablo_Ramos_1-1720471735661.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;User Guide: &lt;A href="https://www.nxp.com/docs/en/user-guide/FRDM33772BSPIEVBUG.pdf" target="_blank"&gt;Featuring the MC33772B battery cell controller IC (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps you!&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jul 2024 20:53:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Spi-communication-with-arduino/m-p/1903034#M716</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2024-07-08T20:53:58Z</dc:date>
    </item>
  </channel>
</rss>