<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Voltage specification for externally provided clock signal (MCX A185 VLH) in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Voltage-specification-for-externally-provided-clock-signal-MCX/m-p/2383558#M5542</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194626"&gt;@wyss-11&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The VEC specification refers to the minimum voltage levels required by the external oscillator input to recognize valid low and high states.&lt;/P&gt;
&lt;P&gt;When VDD = 3.3 V, 2.31 V is the minimum voltage that will be detected as a valid high level.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 19 Jun 2026 17:52:05 GMT</pubDate>
    <dc:creator>carlos_o</dc:creator>
    <dc:date>2026-06-19T17:52:05Z</dc:date>
    <item>
      <title>Voltage specification for externally provided clock signal (MCX A185 VLH)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Voltage-specification-for-externally-provided-clock-signal-MCX/m-p/2383149#M5538</link>
      <description>&lt;P&gt;I can not find the max. voltage allowed at the EXTAL48M pin for the MCXA185VLH MCU in the datasheets.&lt;/P&gt;&lt;P&gt;I know from the LPCxxx families of microcontrollers that the oscillator input is very picky about this amplitude (0.85Vpp or similar).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can I feed an externally generated 3.3V oscillator clock signal directly to the EXTAL48M pin?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jun 2026 13:17:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Voltage-specification-for-externally-provided-clock-signal-MCX/m-p/2383149#M5538</guid>
      <dc:creator>wyss-11</dc:creator>
      <dc:date>2026-06-18T13:17:10Z</dc:date>
    </item>
    <item>
      <title>Re: Voltage specification for externally provided clock signal (MCX A185 VLH)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Voltage-specification-for-externally-provided-clock-signal-MCX/m-p/2383296#M5539</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194626"&gt;@wyss-11&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post!&lt;/P&gt;
&lt;P&gt;MCXA18 does have an EXTAL48M input voltage definition, but it is specified indirectly through the standard input thresholds VIH/VIL relative to VDD, not as a separate fixed EXTAL48M voltage value.&lt;/P&gt;
&lt;P&gt;The datasheet only stands the&amp;nbsp;Peak-to-peak amplitude of oscillation as typical value of 0.6V.&lt;/P&gt;
&lt;P&gt;When VDD is 3.3 V, EXTAL48M can be driven by a 3.3 V external oscillator as long as the clock meets the VIH/VIL thresholds and does not exceed the VDD + 0.3 V input limit.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jun 2026 21:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Voltage-specification-for-externally-provided-clock-signal-MCX/m-p/2383296#M5539</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-06-18T21:02:14Z</dc:date>
    </item>
    <item>
      <title>Re: Voltage specification for externally provided clock signal (MCX A185 VLH)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Voltage-specification-for-externally-provided-clock-signal-MCX/m-p/2383409#M5541</link>
      <description>&lt;P&gt;Thanks for your post.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, the datasheet specifies Vec (Externally provided input clock amplitude) with max. voltage as VIH. But as VIH is 0.7xVDD, this would mean that with VDD=3.3V, Vec max. would be 2.31V only.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So either this datasheet specification is wrong, or Vec max. is really 2.31V in case of VDD=3.3V?&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jun 2026 08:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Voltage-specification-for-externally-provided-clock-signal-MCX/m-p/2383409#M5541</guid>
      <dc:creator>wyss-11</dc:creator>
      <dc:date>2026-06-19T08:36:19Z</dc:date>
    </item>
    <item>
      <title>Re: Voltage specification for externally provided clock signal (MCX A185 VLH)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Voltage-specification-for-externally-provided-clock-signal-MCX/m-p/2383558#M5542</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194626"&gt;@wyss-11&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The VEC specification refers to the minimum voltage levels required by the external oscillator input to recognize valid low and high states.&lt;/P&gt;
&lt;P&gt;When VDD = 3.3 V, 2.31 V is the minimum voltage that will be detected as a valid high level.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jun 2026 17:52:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Voltage-specification-for-externally-provided-clock-signal-MCX/m-p/2383558#M5542</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-06-19T17:52:05Z</dc:date>
    </item>
  </channel>
</rss>