<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TRGMUX Assistance - MCXE316 in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2382114#M5526</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/129422"&gt;@brucebowling&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for the post!&lt;/P&gt;
&lt;P&gt;Your understanding of how the TRGMUX SELx works is correct the EMIOS0_0 is for channel 1 to 4, EMIOS0_1 is for channels 5 to 7 and 9, as shown in the TRGMUX_connectivity.xlsx the channels 0 and 8 are not able.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also,&lt;/P&gt;
&lt;P&gt;I was able to reproduce the issue on my side. I will review it internally and share any relevant information that may help resolve it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jun 2026 20:29:28 GMT</pubDate>
    <dc:creator>carlos_o</dc:creator>
    <dc:date>2026-06-16T20:29:28Z</dc:date>
    <item>
      <title>TRGMUX Assistance - MCXE316</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2381407#M5516</link>
      <description>&lt;P&gt;I am attempting to use the TRGMUX method to route the output of the comparator LPCMP0 to the input of eMIOS0_CH7 (which is configured an an input capture). I am using the MCXE316 device. Part of my issue is understanding the inputs/outputs and wrapping my brain around the nomenclature, and the second I believe is a bug in the PERI_TRGMUX.h file.&lt;/P&gt;&lt;P&gt;I have the eMIOS0 channel 7 configured as a simple input capture, this works properly when assigned to a physical pin. But, I wish to have the input capture triggered instead by the output of the LPCMP0 comparator. Accordingly I should be able to have TRGMUX route the output of the comparator to the input of the input capture of eMIOS0_7.&lt;/P&gt;&lt;P&gt;I look at the MCXE31_TRGMUX_connectivity.xlsx file attached to the reference manual, and I see on the left side "input number", which I am assuming i the input into the TRGMUX. I see LPCMP_0_COUT listed there, with an input number of 5, what I think I am after. Along the top I see "EMIOS_0_ipp_ind_emios_ch[7]" and I see the output register no. of 9 above it. I also see that channels 5, 6, and 9 also have this same number as well.&lt;/P&gt;&lt;P&gt;So, my first question - how to I tell the TRGMUX that the LPCMP0 trigger output goes to channel 7 and not 5 or 6 or 9? I know that the internals of the TRGMUX register has SEL0, SEL1, SEL2, and SEL3 - do I use one of these to choose the channel selection? If so how is this mapped (SEL0 is channel 5, etc), or is there some other mapping, or no mapping? I have looked in the manual and I have not stumbled on this.&lt;/P&gt;&lt;P&gt;Using my best guess that SEL3 is for channel 7 (just for a test), I attepted to use the TRGMUX method in the SDK - here is my calling sequence:&lt;/P&gt;&lt;P&gt;&amp;nbsp; TRGMUX_SetTriggerSource(TRGMUX, kTRGMUX_Emios0_1, kTRGMUX_TriggerInput2, kTRGMUX_SourceLpcmp0 );&lt;/P&gt;&lt;P&gt;with the TRGMUX being the register base, kTRGMUX_Emios0_1 is the TRGMUX register for the eMIOS0 (define value is 9), kTRGMUX_TriggerInput2 is the SEL2 input of the register, and kTRGMUX_SourceLpcmp0 is the source of the trigger (define value is 5).&lt;/P&gt;&lt;P&gt;The problem is that the routine throws a hard fault within this method itself. Here is the actual SDK code for this method:&lt;/P&gt;&lt;P&gt;status_t TRGMUX_SetTriggerSource(TRGMUX_Type *base, uint32_t index, trgmux_trigger_input_t input, uint32_t trigger_src)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; uint32_t value;&lt;BR /&gt;&amp;nbsp; status_t status;&lt;/P&gt;&lt;P&gt;&amp;nbsp; value = base-&amp;gt;TRGCFG[index];&lt;BR /&gt;&amp;nbsp; if (0U != (value &amp;amp; TRGMUX_TRGCFG_LK_MASK))&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp; &amp;nbsp;status = kStatus_TRGMUX_Locked;&lt;BR /&gt;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp; else&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp; &amp;nbsp;/* Since all SEL bitfileds in TRGCFG register have the same length, SEL0's mask is used to&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;access other SEL&lt;BR /&gt;&amp;nbsp; &amp;nbsp;* bitfileds. */&lt;BR /&gt;&amp;nbsp; &amp;nbsp;value = (value &amp;amp; ~((uint32_t)TRGMUX_TRGCFG_SEL0_MASK &amp;lt;&amp;lt; (uint32_t)input)) |&lt;BR /&gt;&amp;nbsp; &amp;nbsp;((trigger_src &amp;amp; (uint32_t)TRGMUX_TRGCFG_SEL0_MASK) &amp;lt;&amp;lt; (uint32_t)input);&lt;BR /&gt;&amp;nbsp; &amp;nbsp;base-&amp;gt;TRGCFG[index] = value;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;status = kStatus_Success;&lt;BR /&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; return status;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;The routine crashes on the first line&lt;BR /&gt;value= base-&amp;gt;TRGCFG[index];&lt;/P&gt;&lt;P&gt;If I look at the debug output, it appears that the TRGCFG array has never been initialized - this variable is defined in PERI_TRGMUX.h and the structure is:&lt;/P&gt;&lt;P&gt;/** TRGMUX - Size of Registers Arrays */&lt;BR /&gt;#define TRGMUX_TRGCFG_COUNT 40u&lt;/P&gt;&lt;P&gt;/** TRGMUX - Register Layout Typedef */&lt;BR /&gt;typedef struct {&lt;BR /&gt;__IO uint32_t TRGCFG[TRGMUX_TRGCFG_COUNT]; /**&amp;lt; TRGMUX ADC12_0 Register..TRGMUX CM7_RXEV Register, array offset: 0x0, array step: 0x4, valid indices: [0-1, 3, 6-18, 21-39] */&lt;BR /&gt;} TRGMUX_Type;&lt;/P&gt;&lt;P&gt;I am just not finding where the TRGCFG is actually defined anywhere. In the debugger the whole array is set to 199661, all 40 elements, which must be garbage. I am accessing element 9 (index is 9).&lt;/P&gt;&lt;P&gt;So my second question is am I using this method correctly and my assumptions OK or is there an issue within the SDK routine?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jun 2026 16:34:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2381407#M5516</guid>
      <dc:creator>brucebowling</dc:creator>
      <dc:date>2026-06-15T16:34:15Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX Assistance - MCXE316</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2382114#M5526</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/129422"&gt;@brucebowling&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for the post!&lt;/P&gt;
&lt;P&gt;Your understanding of how the TRGMUX SELx works is correct the EMIOS0_0 is for channel 1 to 4, EMIOS0_1 is for channels 5 to 7 and 9, as shown in the TRGMUX_connectivity.xlsx the channels 0 and 8 are not able.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also,&lt;/P&gt;
&lt;P&gt;I was able to reproduce the issue on my side. I will review it internally and share any relevant information that may help resolve it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jun 2026 20:29:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2382114#M5526</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-06-16T20:29:28Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX Assistance - MCXE316</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2385209#M5560</link>
      <description>&lt;P&gt;I am checking in to see if there is any new feedback regarding the SDK and TRGMUX functions?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since the TRGMUX is just one register per peripheral, I attempted to just write directly to it with the following one line:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; *(volatile uint32_t *)0x40080024UL = 0x00050000UL;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The TRGMUX base address (according to the RM) is 0x4008_000 and the TRGMUX_eMIOS0_1 register offset is 0x24 giving the absolute address 0x40080024. The SELx field for the LPCMP0_COUT is 0x05 - I shift this up to the SEL2 bit locations (bits 16:23). The lock bit should be 0 from reset (unlocked) and I leave it unlocked.&lt;/P&gt;&lt;P&gt;This one line causes a hard-fault crash and burn every time (inprecise fault). I have tried modifying the other SELx locations, still crashes. I have tried assigning this before I set up the eMIOS and LPCMP, and also tried after full peripheral setup, crashes every time.&lt;/P&gt;&lt;P&gt;Leads me to a couple of questions that I can't seem to find in the manual:&lt;/P&gt;&lt;P&gt;1) Do you set up the TRGMUX linkage before or after the peripheral has been initialized and enabled?&lt;/P&gt;&lt;P&gt;2) Is there any module clocks or similar for the TRGMUX? I know that accessing a module before enabling clocking can cause a Hard-Fault like what I am experiencing. I don't see anything specifically, and I am under the impression that the TRGMUX register is part of each peripheral, so enabling the clock for a peripheral should also enable any required TRGMUX clocking?&lt;/P&gt;&lt;P&gt;Thank you for the assistance.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jun 2026 17:08:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2385209#M5560</guid>
      <dc:creator>brucebowling</dc:creator>
      <dc:date>2026-06-23T17:08:25Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX Assistance - MCXE316</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2386485#M5574</link>
      <description>&lt;P&gt;OK, still having the crashing issue, but further digging into this appears that I need to set the SIUL2 IMCR register before setting the TRGMUX. In the IOMUX xls file attached to the reference manual, I see that for eMIOS0_CH[7] that the SSS bits need to be set to 4 to select TRGMUX_INT_OUT38, is is done with the SIUL_IMCR567 (need to subtract 512 from the 567 due to the 512 offset in naming). Here is the line of code I used to do this, followed by the line to set the TRGMUX:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; SIUL2-&amp;gt;IMCR[55] = SIUL2_IMCR_SSS(4);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; *(volatile uint32_t *)0x40080024UL = TRGMUX_TRGCFG_SEL3(kTRGMUX_SourceLpcmp0);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am still experiencing the TRGMUX hard fault.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jun 2026 15:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2386485#M5574</guid>
      <dc:creator>brucebowling</dc:creator>
      <dc:date>2026-06-25T15:12:08Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX Assistance - MCXE316</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2386559#M5575</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/129422"&gt;@brucebowling&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Apologies for the late reply.&lt;/P&gt;
&lt;P&gt;We noticed that the TRGMUX clock is not enabled by default. Attempting to access the TRGMUX registers while the clock is disabled leads to a HardFault. Your assumption that a clock was missing was correct.&lt;/P&gt;
&lt;P&gt;Could you please add the following line before calling TRGMUX_SetTriggerSource?&lt;/P&gt;
&lt;P&gt;CLOCK_EnableClock(kCLOCK_Trgmux);&lt;/P&gt;
&lt;P&gt;This change resolves the issue on my side.&lt;/P&gt;
&lt;P&gt;For reference, an example of TRGMUX usage can be found in the SDK at:&lt;BR /&gt;boards/frdmmcxe31b/demo_apps/mc_pmsm/pmsm_enc&lt;/P&gt;
&lt;P&gt;Please let me know if this solves the issue or if you have any further questions regarding TRGMUX.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jun 2026 18:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2386559#M5575</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-06-25T18:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX Assistance - MCXE316</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2386577#M5576</link>
      <description>&lt;P&gt;Yes adding this line for the clock corrected the hard fault, and the SDK method. And the direct-coded means that I came up with also worked as well.&lt;/P&gt;&lt;P&gt;So, in general, you have to enable the TRGMUX clock and set the IMCR register, along with calling the SDK method for TRGMUX linkage. With this the LPCMP triggers the eMIOS input capture properly.&lt;/P&gt;&lt;P&gt;Thank you fr the support.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jun 2026 19:46:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/TRGMUX-Assistance-MCXE316/m-p/2386577#M5576</guid>
      <dc:creator>brucebowling</dc:creator>
      <dc:date>2026-06-25T19:46:07Z</dc:date>
    </item>
  </channel>
</rss>