<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 Comparator pin description</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Comparator-pin-description/m-p/2379761#M5504</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In 172-pin QFP part&amp;nbsp;MCXN247VPBT, pins 135 &amp;amp; 139 only show CMP1_IN1 and do not have any suffix to indicate if these are CMP1_IN1P or CMP1_IN1N. Similarly, pins 156, 157, 162, 163 also have the same issue in datasheet as well as Config tool.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone from NXP update this information in datasheet as well as config tool?&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thanks,&lt;/P&gt;&lt;P&gt;Satish Acharya&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jun 2026 00:37:24 GMT</pubDate>
    <dc:creator>acharya_satishb</dc:creator>
    <dc:date>2026-06-11T00:37:24Z</dc:date>
    <item>
      <title>Comparator pin description</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Comparator-pin-description/m-p/2379761#M5504</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In 172-pin QFP part&amp;nbsp;MCXN247VPBT, pins 135 &amp;amp; 139 only show CMP1_IN1 and do not have any suffix to indicate if these are CMP1_IN1P or CMP1_IN1N. Similarly, pins 156, 157, 162, 163 also have the same issue in datasheet as well as Config tool.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone from NXP update this information in datasheet as well as config tool?&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thanks,&lt;/P&gt;&lt;P&gt;Satish Acharya&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jun 2026 00:37:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Comparator-pin-description/m-p/2379761#M5504</guid>
      <dc:creator>acharya_satishb</dc:creator>
      <dc:date>2026-06-11T00:37:24Z</dc:date>
    </item>
    <item>
      <title>Re: Comparator pin description</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Comparator-pin-description/m-p/2379830#M5505</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/140873"&gt;@acharya_satishb&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think there is no issue with either the datasheet or the Config Tool.&lt;BR /&gt;The reason is that the pins you mentioned can be configured as either CMPx_INxP or CMPx_INxN.&lt;BR /&gt;For example, pin 135 (also referred to as P0_3). As shown in “Table 375. CMP input connections” in reference manual, both CMP1_IN1P and CMP1_IN1N are mapped to P0_3.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1781148101856.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/388644i0E2C8B4528ECF0E9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_0-1781148101856.png" alt="Celeste_Liu_0-1781148101856.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_1-1781148118393.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/388645i8B27AEB048CDA6D9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_1-1781148118393.png" alt="Celeste_Liu_1-1781148118393.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;The same applies to other pins such as 139, 156, 157, 162, and 163.&lt;BR /&gt;According to the table, only the inputs with index 4 and 5 are special cases. Therefore, these are explicitly differentiated in the pinmux. For instance, P4_15 is defined as CMP0_IN4&lt;STRONG&gt;P&lt;/STRONG&gt; in the pinmux.&lt;/P&gt;
&lt;P&gt;About selecting the input used for the positive or negative mux, you can&amp;nbsp;sconfigure the MSEL and PSEL bits in the CCR2 register.&amp;nbsp;&amp;nbsp;And noted that PSEL should not be same as MSEL.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_2-1781148389923.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/388647iCCD7C75ED67BA540/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_2-1781148389923.png" alt="Celeste_Liu_2-1781148389923.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it helps.&amp;nbsp;If you needs further help please do not hesitate to reach out.&lt;/P&gt;
&lt;P&gt;Any new issues, welcome to create a new post.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;--------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;BR /&gt;--------------------------------------------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jun 2026 03:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Comparator-pin-description/m-p/2379830#M5505</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-06-11T03:36:16Z</dc:date>
    </item>
    <item>
      <title>Re: Comparator pin description</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Comparator-pin-description/m-p/2379837#M5506</link>
      <description>&lt;P&gt;Thank you, Celeste. This answers my question.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jun 2026 03:51:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Comparator-pin-description/m-p/2379837#M5506</guid>
      <dc:creator>acharya_satishb</dc:creator>
      <dc:date>2026-06-11T03:51:40Z</dc:date>
    </item>
  </channel>
</rss>