<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 Re: MCXN527 USB ISP</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2377296#M5483</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;in the meantime I measured the DCDC_LX output of 3 different microcontrollers after soldering them on the pcb.&lt;/P&gt;&lt;P&gt;First is 1.08V, second is 1.34V and the third is 1.11V.&lt;/P&gt;&lt;P&gt;Hardware design is as in UG10092 guide for HQLFP100 package (DCDC configuration) described. I took the value for the inductor and capacitor from the FRDM-MCXN947 design.&lt;/P&gt;&lt;P&gt;None of them connects via USB.&lt;/P&gt;&lt;P&gt;Is the difference in DCDC_LX normal? Chips are from Digikey.&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jun 2026 08:05:36 GMT</pubDate>
    <dc:creator>BuS</dc:creator>
    <dc:date>2026-06-05T08:05:36Z</dc:date>
    <item>
      <title>MCXN527 USB ISP</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2366265#M5393</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i am new to the MCX Controllers, and i can not establish an USB connection.&lt;/P&gt;&lt;P&gt;I use a MCXN527VKLT Controller, and I have connected:&lt;/P&gt;&lt;P&gt;-USB0-DM and -DP&lt;/P&gt;&lt;P&gt;-VDD_USB (over a 3.3V regulator)&lt;/P&gt;&lt;P&gt;-VSS_USB&lt;/P&gt;&lt;P&gt;-USB0_VBUS_DET to 5V from USB&lt;/P&gt;&lt;P&gt;My expectations are that when I pull ISPMODE_N pin to GND via a switch, then plug in USB in my computer, open the ISPMODE_N switch, the controller should be seen as an HID?&lt;/P&gt;&lt;P&gt;I also tried testing the connection with the secure provisioning tool.&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;&lt;P&gt;Thanks in advance and sorry for this beginner question.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;</description>
      <pubDate>Fri, 15 May 2026 14:34:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2366265#M5393</guid>
      <dc:creator>BuS</dc:creator>
      <dc:date>2026-05-15T14:34:31Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN527 USB ISP</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2366341#M5394</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262824"&gt;@BuS&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your post,&lt;/P&gt;
&lt;P&gt;Could you confirm your external crystal oscillator value?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The &lt;A href="https://docs.nxp.com/bundle/UG10092/page/topics/digital_interfaces.html#topic_84dff212-a633-4700-8932-f3871a62ec94" target="_blank"&gt;UG10092: MCX N Series Hardware Design Guide | NXP Semiconductors&lt;/A&gt;&amp;nbsp;has a note that is relevant in the case of ISP over USB:&amp;nbsp;If using the HS USB in In-system programming (ISP) mode, a 24 MHz crystal must be used in at least the first access of the device. However, the user can modify the security fuse configuration to allow a different crystal. However, the user must configure it. For example, factory configuration requires a 24 MHz crystal for HS USB ISP operation.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;</description>
      <pubDate>Fri, 15 May 2026 19:56:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2366341#M5394</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-05-15T19:56:16Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN527 USB ISP</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2366495#M5395</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;there is a 24MHz crystal attached to pin P1_30 and P1_31.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;</description>
      <pubDate>Sat, 16 May 2026 11:03:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2366495#M5395</guid>
      <dc:creator>BuS</dc:creator>
      <dc:date>2026-05-16T11:03:25Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN527 USB ISP</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2367125#M5400</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262824"&gt;@BuS&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;thank you for clarifying!&lt;/P&gt;
&lt;P&gt;Please review the VDD_CORE voltage.&lt;/P&gt;
&lt;P&gt;USB HS is not supported when VDD_CORE &amp;lt; 1.1 V&lt;/P&gt;
&lt;P&gt;Also review that your system follows the&amp;nbsp;&lt;STRONG&gt;2.5 Required Power-On-Reset (POR) Sequencing&lt;/STRONG&gt; described at&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/data-sheet/MCXNP184M150F70.pdf" target="_blank"&gt;Highly integrated low-power dual-core Arm Cortex M33 MCU with on-chip accelerators&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Could you confirm if you were able to use your custom board before?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 May 2026 20:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2367125#M5400</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-05-18T20:53:51Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN527 USB ISP</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2371749#M5433</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;this is the first prototype of the custom PCB. So this has not worked before.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use the on chip DCDC_CORE to power LDO_CORE as shown in chapter 35 in the reference manual. I read 1.08V on LDO_CORE.&lt;/P&gt;&lt;P&gt;I also ordered new controllers and the problem is still the same.&lt;/P&gt;&lt;P&gt;Can you please confirm my assumption that this controller should be seen as HID when connected to USB? Is there any kind of driver that must be installed before pluging in?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;</description>
      <pubDate>Wed, 27 May 2026 07:44:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2371749#M5433</guid>
      <dc:creator>BuS</dc:creator>
      <dc:date>2026-05-27T07:44:27Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN527 USB ISP</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2377296#M5483</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;in the meantime I measured the DCDC_LX output of 3 different microcontrollers after soldering them on the pcb.&lt;/P&gt;&lt;P&gt;First is 1.08V, second is 1.34V and the third is 1.11V.&lt;/P&gt;&lt;P&gt;Hardware design is as in UG10092 guide for HQLFP100 package (DCDC configuration) described. I took the value for the inductor and capacitor from the FRDM-MCXN947 design.&lt;/P&gt;&lt;P&gt;None of them connects via USB.&lt;/P&gt;&lt;P&gt;Is the difference in DCDC_LX normal? Chips are from Digikey.&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jun 2026 08:05:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN527-USB-ISP/m-p/2377296#M5483</guid>
      <dc:creator>BuS</dc:creator>
      <dc:date>2026-06-05T08:05:36Z</dc:date>
    </item>
  </channel>
</rss>