<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックMicrocontroller selection for entry-level consumer graphical application</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Microcontroller-selection-for-entry-level-consumer-graphical/m-p/2364986#M5388</link>
    <description>&lt;P&gt;Hi support Team,&lt;/P&gt;&lt;P&gt;I&amp;nbsp; am looking for support in selecting an entry-level microcontroller for a consumer graphical application.&lt;/P&gt;&lt;P&gt;Requirements:&lt;/P&gt;&lt;P&gt;Display:&amp;nbsp;small display up to&amp;nbsp;320 × 240&lt;BR /&gt;Memory:&amp;nbsp;around&amp;nbsp;1 MB Flash&amp;nbsp;and&amp;nbsp;256 KB RAM&lt;BR /&gt;Power:&amp;nbsp;preferably&amp;nbsp;mainstream or low-power&lt;BR /&gt;Peripherals:&lt;BR /&gt;3 SPI instances&lt;BR /&gt;2 I2C instances&lt;BR /&gt;2 ADC channels&lt;BR /&gt;The peripherals will be used with&amp;nbsp;dedicated sensors&lt;/P&gt;&lt;P&gt;The application is a consumer product with a small graphical interface and dedicated sensor connections. I am looking for a cost-effective microcontroller that can support the display, peripheral interfaces, and basic graphics requirements in an entry-level solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;Could you recommend suitable microcontroller families or specific part numbers that best match these requirements?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there an existing example or reference project that could be used as a starting point for development?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Nuyuan&lt;/P&gt;</description>
    <pubDate>Wed, 13 May 2026 15:36:27 GMT</pubDate>
    <dc:creator>Yuza</dc:creator>
    <dc:date>2026-05-13T15:36:27Z</dc:date>
    <item>
      <title>Microcontroller selection for entry-level consumer graphical application</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Microcontroller-selection-for-entry-level-consumer-graphical/m-p/2364986#M5388</link>
      <description>&lt;P&gt;Hi support Team,&lt;/P&gt;&lt;P&gt;I&amp;nbsp; am looking for support in selecting an entry-level microcontroller for a consumer graphical application.&lt;/P&gt;&lt;P&gt;Requirements:&lt;/P&gt;&lt;P&gt;Display:&amp;nbsp;small display up to&amp;nbsp;320 × 240&lt;BR /&gt;Memory:&amp;nbsp;around&amp;nbsp;1 MB Flash&amp;nbsp;and&amp;nbsp;256 KB RAM&lt;BR /&gt;Power:&amp;nbsp;preferably&amp;nbsp;mainstream or low-power&lt;BR /&gt;Peripherals:&lt;BR /&gt;3 SPI instances&lt;BR /&gt;2 I2C instances&lt;BR /&gt;2 ADC channels&lt;BR /&gt;The peripherals will be used with&amp;nbsp;dedicated sensors&lt;/P&gt;&lt;P&gt;The application is a consumer product with a small graphical interface and dedicated sensor connections. I am looking for a cost-effective microcontroller that can support the display, peripheral interfaces, and basic graphics requirements in an entry-level solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;Could you recommend suitable microcontroller families or specific part numbers that best match these requirements?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there an existing example or reference project that could be used as a starting point for development?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Nuyuan&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 15:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Microcontroller-selection-for-entry-level-consumer-graphical/m-p/2364986#M5388</guid>
      <dc:creator>Yuza</dc:creator>
      <dc:date>2026-05-13T15:36:27Z</dc:date>
    </item>
    <item>
      <title>Re: Microcontroller selection for entry-level consumer graphical application</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Microcontroller-selection-for-entry-level-consumer-graphical/m-p/2368366#M5408</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262735"&gt;@Yuza&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Based on your requirements, we would recommend MCX N94x / N54x.&lt;/P&gt;
&lt;P&gt;MCXN94x/54x:&amp;nbsp;&lt;A href="https://www.nxp.com/products/MCX-N94-N54-N53-N52-N24?page=1&amp;amp;nrnd=false" target="_blank" rel="noopener"&gt;MCX N94, N54, N53, N52 and N24 MCUs | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The main reason is memory fit. Your target is around 1 MB Flash and 256 KB RAM , while the MCXN546 / MCXN946 devices provide 1 MB Flash and 352 KB SRAM , and the MCXN547 / MCXN947 devices provide 2 MB Flash and 512 KB SRAM , all running at up to 150 MHz.&lt;/P&gt;
&lt;P&gt;This family is also a good fit for a small graphical interface. NXP positions the MCX N family for industrial/consumer HMI applications and highlights display support in the portfolio overview. The MCX N series includes SmartDMA for display and fast I/O use cases, and FlexIO can be used for LCD interfaces.&lt;/P&gt;
&lt;P&gt;The MCX N94x / N54x series integrates 10 low-power Flexcomm instances , and these encapsulate LPSPI, LPUART, and LPI2C functions, giving sufficient serial interface resources for requirements such as 3x SPI and 2x I2C .&lt;/P&gt;
&lt;P&gt;The documentation includes &lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN14172.pdf" target="_self"&gt;AN14172&lt;/A&gt;, Using SmartDMA for Graphic on MCX N Series MCU , which describes graphics-oriented data handling on MCX N and includes an SDK example named &lt;STRONG&gt;lvgl_demo_widgets_bm&lt;/STRONG&gt; . That example uses FlexIO to emulate an MCU8080 interface to drive a 3.5-inch LCD , with SmartDMA transferring data to the FlexIO data registers. In addition, MCX N is listed in NXP’s MCUXpresso GUI ecosystem as a supported platform for LVGL-based development. We also have LVGL demos in our SDK.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1779271794344.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/386168i37CBCF3CD52D6739/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_0-1779271794344.png" alt="Celeste_Liu_0-1779271794344.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We also have EVK board for your evaluation:&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM-MCXN947" target="_blank" rel="noopener"&gt;MCXN947 FRDM Board for Industrial IoT Solutions | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Wed, 20 May 2026 10:10:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Microcontroller-selection-for-entry-level-consumer-graphical/m-p/2368366#M5408</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-05-20T10:10:07Z</dc:date>
    </item>
  </channel>
</rss>