<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is There Arduino Support or Board Package Available for i.MX RT1041? in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Is-There-Arduino-Support-or-Board-Package-Available-for-i-MX/m-p/2356032#M5292</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253824"&gt;@Harisha&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;We do not have an Arduino board package for the i.MX RT1041.&lt;/P&gt;
&lt;P&gt;Instead, you can refer to the i.MX RT1040 EVK, which is the closest supported implementation to the i.MX RT1041. For this board, we provide SDK examples covering different modules.&lt;/P&gt;
&lt;P&gt;You can obtain the SDK from the &lt;A href="https://mcuxpresso.nxp.com/" target="_blank"&gt;MCUXpresso SDK Builder&lt;/A&gt;. The SDK is designed to be used with MCUXpresso IDE or MCUXpresso for Visual Studio Code, and I highly recommend using one of these IDEs.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
    <pubDate>Fri, 24 Apr 2026 21:55:11 GMT</pubDate>
    <dc:creator>Pablo_Ramos</dc:creator>
    <dc:date>2026-04-24T21:55:11Z</dc:date>
    <item>
      <title>Is There Arduino Support or Board Package Available for i.MX RT1041?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Is-There-Arduino-Support-or-Board-Package-Available-for-i-MX/m-p/2355644#M5286</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently working on the i.MX RT1041 and I want to use it with the Arduino IDE, similar to how we use boards like ESP32 or Seeeduino.&lt;/P&gt;&lt;P&gt;For RT1052 (RT1050 EVKB), I have already achieved this by flashing the Seeeduino Arch Mix Arduino bootloader. After that, the board behaves like a Seeeduino board in the Arduino IDE, and I can successfully upload Arduino programs. I have already tested peripherals like I2C, SPI, UART (Modbus RTU), PWM, etc., and everything is working fine.&lt;/P&gt;&lt;P&gt;Now, I want to do the same for RT1041. However, unlike RT1052, there are no official Arduino-compatible boards (like Seeeduino) available for RT1041.&lt;/P&gt;&lt;P&gt;As far as I understand, there are two ways to add a board to Arduino IDE:&lt;/P&gt;&lt;P&gt;Using an existing board package via Board Manager&lt;BR /&gt;Manually creating a custom board support package&lt;/P&gt;&lt;P&gt;The second option is more complex. So my question is:&lt;/P&gt;&lt;P&gt;&lt;LI-EMOJI id="lia_backhand-index-pointing-right" title=":backhand_index_pointing_right:"&gt;&lt;/LI-EMOJI&gt; Is there any existing Arduino board package or support available for RT1041 that I can directly install and use in Arduino IDE?&lt;/P&gt;</description>
      <pubDate>Fri, 24 Apr 2026 06:45:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Is-There-Arduino-Support-or-Board-Package-Available-for-i-MX/m-p/2355644#M5286</guid>
      <dc:creator>Harisha</dc:creator>
      <dc:date>2026-04-24T06:45:06Z</dc:date>
    </item>
    <item>
      <title>Re: Is There Arduino Support or Board Package Available for i.MX RT1041?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Is-There-Arduino-Support-or-Board-Package-Available-for-i-MX/m-p/2356032#M5292</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253824"&gt;@Harisha&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;We do not have an Arduino board package for the i.MX RT1041.&lt;/P&gt;
&lt;P&gt;Instead, you can refer to the i.MX RT1040 EVK, which is the closest supported implementation to the i.MX RT1041. For this board, we provide SDK examples covering different modules.&lt;/P&gt;
&lt;P&gt;You can obtain the SDK from the &lt;A href="https://mcuxpresso.nxp.com/" target="_blank"&gt;MCUXpresso SDK Builder&lt;/A&gt;. The SDK is designed to be used with MCUXpresso IDE or MCUXpresso for Visual Studio Code, and I highly recommend using one of these IDEs.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Fri, 24 Apr 2026 21:55:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Is-There-Arduino-Support-or-Board-Package-Available-for-i-MX/m-p/2356032#M5292</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2026-04-24T21:55:11Z</dc:date>
    </item>
  </channel>
</rss>