<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Power consumption in sleep mode is higher than expected for the MCXA153 in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2355055#M5276</link>
    <description>&lt;P&gt;Hi.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the link.&lt;BR /&gt;I see that this is the same example as &lt;A href="https://github.com/nxp-appcodehub/an-low-power-implementation-mcxa156" target="_blank"&gt;https://github.com/nxp-appcodehub/an-low-power-implementation-mcxa156&lt;/A&gt;, which I tested earlier, but it crashed with a HardFault.&lt;BR /&gt;So I debugged it and removed the problematic parts of the code for the MCXA156 to make the program compatible with the MCXA153.&lt;BR /&gt;The result is a current of 0.40–0.41 mA, which is very close to the figure in the PDF, where the current is listed as 0.34 mA. And that’s acceptable.&lt;/P&gt;&lt;P&gt;From my perspective, however, there is a bit of an issue with both programs for the AN1447 and AN14558. They are not fully compatible with the SDK and MCUXpresso. The clock_config.* files contain a lot of changes and cannot be used with Clock ConfigTools. The fsl_cmc.c file has also been modified.&lt;/P&gt;&lt;P&gt;So using the examples isn’t just a simple kids’ game like: find ten differences &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Apr 2026 08:09:24 GMT</pubDate>
    <dc:creator>petrolivka</dc:creator>
    <dc:date>2026-04-23T08:09:24Z</dc:date>
    <item>
      <title>Power consumption in sleep mode is higher than expected for the MCXA153</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2345511#M5148</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I read AN14558 (Low Power Implementation on MCX A153 MCU Series) and used the program included in this application note. I obtained almost identical results, which match those shown in &lt;A href="https://www.youtube.com/watch?v=Rj9QANRU3rA" target="_blank"&gt;https://www.youtube.com/watch?v=Rj9QANRU3rA&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;In sleep mode with slow wake-up (options B and 3 in the terminal), the current is 0.85 mA.&lt;/P&gt;&lt;P&gt;In the&amp;nbsp;MCXAP64M96FS3 datasheet, the table 14 in section 3.2.6.1 states that IDD_SLEEP_MD should be 0.34 mA. That is less than half of the value specified in AN14558.&lt;/P&gt;&lt;P&gt;What else needs to be changed in the program to get the current closer to 0.34 mA?&lt;/P&gt;&lt;P&gt;I’ve studied the application note and the source code; in my opinion, everything is set for minimum current consumption.&lt;/P&gt;&lt;P&gt;Thank you, Petr&lt;/P&gt;</description>
      <pubDate>Sun, 05 Apr 2026 18:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2345511#M5148</guid>
      <dc:creator>petrolivka</dc:creator>
      <dc:date>2026-04-05T18:48:22Z</dc:date>
    </item>
    <item>
      <title>Re: Power consumption in sleep mode is higher than expected for the MCXA153</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2346296#M5157</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/159682"&gt;@petrolivka&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;Could you please let me know whether you are using your own board or an NXP demo board?&lt;BR /&gt;If you are using a demo board, please provide a photo showing the hardware connections during the measurement, as well as the code that is running on the board.&lt;/DIV&gt;
&lt;DIV&gt;&lt;BR /&gt;Thank you.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;BR&lt;/DIV&gt;
&lt;DIV&gt;Alice&lt;/DIV&gt;</description>
      <pubDate>Tue, 07 Apr 2026 10:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2346296#M5157</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2026-04-07T10:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: Power consumption in sleep mode is higher than expected for the MCXA153</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2346398#M5160</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I primarily measured the FRDM-MCXA153, but I also have two other custom boards with the MCXA153 and MCXA142. The current is nearly identical in all three cases.&lt;BR /&gt;I’m attaching the measurements taken with MCU-Link Pro and with a multimeter.&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;</description>
      <pubDate>Tue, 07 Apr 2026 13:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2346398#M5160</guid>
      <dc:creator>petrolivka</dc:creator>
      <dc:date>2026-04-07T13:58:40Z</dc:date>
    </item>
    <item>
      <title>Re: Power consumption in sleep mode is higher than expected for the MCXA153</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2351519#M5245</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/159682"&gt;@petrolivka&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;I’m sorry for the late reply.&lt;BR /&gt;Due to an issue with the community system, I did not receive any notification, and I just saw your response.&lt;BR /&gt;I will perform the measurements on my side and get back to you as soon as possible.&lt;BR /&gt;Thank you for your patience.&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Apr 2026 10:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2351519#M5245</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2026-04-15T10:52:52Z</dc:date>
    </item>
    <item>
      <title>Re: Power consumption in sleep mode is higher than expected for the MCXA153</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2352248#M5249</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/159682"&gt;@petrolivka&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;This power consumption code is based on the MCXA156 and can achieve results the same with the values shown in the datasheet. Please refer to the following link for details:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note-software/AN14447SW.zip" target="_blank"&gt;https://www.nxp.com/docs/en/application-note-software/AN14447SW.zip&lt;/A&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;BR&lt;/DIV&gt;
&lt;DIV&gt;Alice&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Apr 2026 10:16:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2352248#M5249</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2026-04-16T10:16:28Z</dc:date>
    </item>
    <item>
      <title>Re: Power consumption in sleep mode is higher than expected for the MCXA153</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2355055#M5276</link>
      <description>&lt;P&gt;Hi.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the link.&lt;BR /&gt;I see that this is the same example as &lt;A href="https://github.com/nxp-appcodehub/an-low-power-implementation-mcxa156" target="_blank"&gt;https://github.com/nxp-appcodehub/an-low-power-implementation-mcxa156&lt;/A&gt;, which I tested earlier, but it crashed with a HardFault.&lt;BR /&gt;So I debugged it and removed the problematic parts of the code for the MCXA156 to make the program compatible with the MCXA153.&lt;BR /&gt;The result is a current of 0.40–0.41 mA, which is very close to the figure in the PDF, where the current is listed as 0.34 mA. And that’s acceptable.&lt;/P&gt;&lt;P&gt;From my perspective, however, there is a bit of an issue with both programs for the AN1447 and AN14558. They are not fully compatible with the SDK and MCUXpresso. The clock_config.* files contain a lot of changes and cannot be used with Clock ConfigTools. The fsl_cmc.c file has also been modified.&lt;/P&gt;&lt;P&gt;So using the examples isn’t just a simple kids’ game like: find ten differences &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Apr 2026 08:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Power-consumption-in-sleep-mode-is-higher-than-expected-for-the/m-p/2355055#M5276</guid>
      <dc:creator>petrolivka</dc:creator>
      <dc:date>2026-04-23T08:09:24Z</dc:date>
    </item>
  </channel>
</rss>