<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックMCX A secure/signed mode in rom bootloader?</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCX-A-secure-signed-mode-in-rom-bootloader/m-p/2315623#M4828</link>
    <description>&lt;P&gt;Lets assume we want to design a system using MCX A-series that uses the ROM bootloader feature for end-customer firmware upgrades.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Upgrades could happen via web-serial-&amp;gt;usb or in-system updates via UART from another mcu, both talking directly to the rom boot code.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I haven't looked in detail whats available in the newer MCX-series rom implementation, but the questions are:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;is there a way to require a signed binary when using ROM boot?&lt;BR /&gt;&lt;UL&gt;&lt;LI&gt;i.e. write "otp-keys" to flash and force the bootloader to only accept valid binaries to be written&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;are there ways to prevent raw reads from flash while still having erase/write enabled?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in my case mcu pick would be: MCXA156VPJ&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ps. fully aware I can write my own 2nd stage BL to achieve this, but the whole point here is to design a simple + brick-proof system.&lt;/P&gt;</description>
    <pubDate>Tue, 10 Feb 2026 12:26:14 GMT</pubDate>
    <dc:creator>dav1</dc:creator>
    <dc:date>2026-02-10T12:26:14Z</dc:date>
    <item>
      <title>MCX A secure/signed mode in rom bootloader?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCX-A-secure-signed-mode-in-rom-bootloader/m-p/2315623#M4828</link>
      <description>&lt;P&gt;Lets assume we want to design a system using MCX A-series that uses the ROM bootloader feature for end-customer firmware upgrades.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Upgrades could happen via web-serial-&amp;gt;usb or in-system updates via UART from another mcu, both talking directly to the rom boot code.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I haven't looked in detail whats available in the newer MCX-series rom implementation, but the questions are:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;is there a way to require a signed binary when using ROM boot?&lt;BR /&gt;&lt;UL&gt;&lt;LI&gt;i.e. write "otp-keys" to flash and force the bootloader to only accept valid binaries to be written&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;are there ways to prevent raw reads from flash while still having erase/write enabled?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in my case mcu pick would be: MCXA156VPJ&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ps. fully aware I can write my own 2nd stage BL to achieve this, but the whole point here is to design a simple + brick-proof system.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Feb 2026 12:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCX-A-secure-signed-mode-in-rom-bootloader/m-p/2315623#M4828</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2026-02-10T12:26:14Z</dc:date>
    </item>
    <item>
      <title>Re: MCX A secure/signed mode in rom bootloader?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCX-A-secure-signed-mode-in-rom-bootloader/m-p/2316189#M4835</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83226"&gt;@dav1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;The MCXA series does not support secure or signed mode in the ROM bootloader.&lt;BR /&gt;Please consider using the MCXN series, which does support this feature.&lt;/DIV&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-n-series-microcontrollers:MCX-N-SERIES" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-n-series-microcontrollers:MCX-N-SERIES&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 11 Feb 2026 09:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCX-A-secure-signed-mode-in-rom-bootloader/m-p/2316189#M4835</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2026-02-11T09:23:11Z</dc:date>
    </item>
    <item>
      <title>Re: MCX A secure/signed mode in rom bootloader?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCX-A-secure-signed-mode-in-rom-bootloader/m-p/2326451#M4945</link>
      <description>&lt;P&gt;1)&lt;/P&gt;&lt;P&gt;the N-series are too expensive for the application.&lt;BR /&gt;what other mcx'es do support secure rom-boot?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2)&lt;/P&gt;&lt;P&gt;are you 100% sure there isn't a way to achieve a secure update-path on A-series?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Mar 2026 14:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCX-A-secure-signed-mode-in-rom-bootloader/m-p/2326451#M4945</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2026-03-04T14:32:49Z</dc:date>
    </item>
  </channel>
</rss>