<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 FRDM-MCXN947 Ethernet Issue</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-Ethernet-Issue/m-p/2311174#M4798</link>
    <description>&lt;P&gt;Hi NXP Community,&lt;BR /&gt;&lt;BR /&gt;I just purchased 3 FRDM-MCXN947 dev kits for a company project and I can't get the Ethernet port to pass data on one of them. &amp;nbsp;I am using Zephyr v4.3.0 and I have tested using the `http_server` sample. &amp;nbsp;This works on the other two but I can't get DHCP or static IPs to work on the remaining on. &amp;nbsp;The link lights are lit but it just times out trying to get a DHCP address and when static it's not routable. &amp;nbsp;The device also doesn't show up as a client in our network management tools.&lt;/P&gt;&lt;P&gt;Thoughts on other tests I can run? &amp;nbsp;Has this happened before?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Daz&lt;/P&gt;</description>
    <pubDate>Wed, 04 Feb 2026 17:37:35 GMT</pubDate>
    <dc:creator>WestCoastDaz</dc:creator>
    <dc:date>2026-02-04T17:37:35Z</dc:date>
    <item>
      <title>FRDM-MCXN947 Ethernet Issue</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-Ethernet-Issue/m-p/2311174#M4798</link>
      <description>&lt;P&gt;Hi NXP Community,&lt;BR /&gt;&lt;BR /&gt;I just purchased 3 FRDM-MCXN947 dev kits for a company project and I can't get the Ethernet port to pass data on one of them. &amp;nbsp;I am using Zephyr v4.3.0 and I have tested using the `http_server` sample. &amp;nbsp;This works on the other two but I can't get DHCP or static IPs to work on the remaining on. &amp;nbsp;The link lights are lit but it just times out trying to get a DHCP address and when static it's not routable. &amp;nbsp;The device also doesn't show up as a client in our network management tools.&lt;/P&gt;&lt;P&gt;Thoughts on other tests I can run? &amp;nbsp;Has this happened before?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Daz&lt;/P&gt;</description>
      <pubDate>Wed, 04 Feb 2026 17:37:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-Ethernet-Issue/m-p/2311174#M4798</guid>
      <dc:creator>WestCoastDaz</dc:creator>
      <dc:date>2026-02-04T17:37:35Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MCXN947 Ethernet Issue</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-Ethernet-Issue/m-p/2312475#M4803</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258562"&gt;@WestCoastDaz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;May I ask if all three chips are the same? Has the board been reworked?&lt;/P&gt;
&lt;P&gt;I think you can also test the&amp;nbsp;SDK lwIP demos.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1770257886923.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/375587iB74B5BE6E90DF9A0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1770257886923.png" alt="Harry_Zhang_0-1770257886923.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Harry_Zhang_0-1770257886923.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If lwIP also fails to get DHCP or cannot respond to ping, I think this may be a hardware issue.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Thu, 05 Feb 2026 02:19:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-Ethernet-Issue/m-p/2312475#M4803</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-02-05T02:19:18Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MCXN947 Ethernet Issue</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-Ethernet-Issue/m-p/2313228#M4809</link>
      <description>Unfortunately I can't compare the chip versions as 2 of the DKs are being used in prototypes and I don't have access to them. The box on the non-working DK has a date code from 2429.&lt;BR /&gt;&lt;BR /&gt;I don't have MCUXsspresso SDK installed only Zephyr is there another Zephyr example I could try?&lt;BR /&gt;&lt;BR /&gt;Thanks,</description>
      <pubDate>Thu, 05 Feb 2026 22:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-Ethernet-Issue/m-p/2313228#M4809</guid>
      <dc:creator>WestCoastDaz</dc:creator>
      <dc:date>2026-02-05T22:20:37Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MCXN947 Ethernet Issue</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-Ethernet-Issue/m-p/2314243#M4820</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258562"&gt;@WestCoastDaz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you don't&amp;nbsp;have MCUXsspresso SDK installed.&lt;/P&gt;
&lt;P&gt;I think you can try to test the&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;samples/net/sockets/echo_server/&lt;/LI-CODE&gt;
&lt;P&gt;or&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;samples/net/dhcpv4_client&lt;/LI-CODE&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 09 Feb 2026 02:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-Ethernet-Issue/m-p/2314243#M4820</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-02-09T02:13:55Z</dc:date>
    </item>
  </channel>
</rss>