<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Code loaded onto MCXN546VKLT will not run in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2303235#M4774</link>
    <description>&lt;P&gt;I wanted to confirm the startup power of the device. You can see from attached that the power up sequence is as expected.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Yellow trace - 3.3 V from external LDO&lt;/LI&gt;&lt;LI&gt;Pink trace - 1.0V from internal LDO VDD_CORE&lt;/LI&gt;&lt;LI&gt;Blue trace - RESET_B line&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;As you can see, the VDD_CORE is essentially stable when the MCU releases the RESET_B line and allows to go high through our pullup.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Startup power sequence" style="width: 800px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374854i4959342D4668BD75/image-size/large?v=v2&amp;amp;px=999" role="button" title="MitosysBaseStartup.png" alt="Startup power sequence" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Startup power sequence&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Jan 2026 20:46:46 GMT</pubDate>
    <dc:creator>DBML</dc:creator>
    <dc:date>2026-01-29T20:46:46Z</dc:date>
    <item>
      <title>Code loaded onto MCXN546VKLT will not run</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2298766#M4712</link>
      <description>&lt;P&gt;I follow the same basic procedure to create a project for the MCXN947 on the FRDM board and initialize and assert the P2_0 pin. It loads and performs as expected. Following the exact same procedure for a. MCXN546 project and selecting the VKLT variant of chip, the code does not run on our platform. I have checked the&amp;nbsp; boot condition of the processor on our board and it appears good.&lt;BR /&gt;&lt;BR /&gt;I am able to use ISP with our board with no issues. Just cannot get it to run basic code.&lt;BR /&gt;&lt;BR /&gt;AI searching talks about corrupting CMPA or CFPA regions of flash causing rom to decide to not boot our code. AI also mentions to look for flash config in startup, but in my exploring sdk and created projects, I cannot see any details of flash config.&lt;BR /&gt;&lt;BR /&gt;Considering this version of part does not have BOOT_MODE pins, how do we ensure that the system will run with our loaded code.&lt;BR /&gt;&lt;BR /&gt;Note that I have confirmed all power conditions and that the RESET_B appears to transition properly on power up.&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jan 2026 06:34:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2298766#M4712</guid>
      <dc:creator>DBML</dc:creator>
      <dc:date>2026-01-23T06:34:02Z</dc:date>
    </item>
    <item>
      <title>Re: Code loaded onto MCXN546VKLT will not run</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2298921#M4715</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243189"&gt;@DBML&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think you can try to download the&amp;nbsp;MCXN546 chip SDK.&lt;/P&gt;
&lt;P&gt;And create a project.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1769157865678.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374055iCE6C8924070362B8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1769157865678.png" alt="Harry_Zhang_0-1769157865678.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_1-1769157873914.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374056iE492ECAD45B3150D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_1-1769157873914.png" alt="Harry_Zhang_1-1769157873914.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_2-1769157882075.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374057i0019A0B04B6D147F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_2-1769157882075.png" alt="Harry_Zhang_2-1769157882075.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jan 2026 08:45:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2298921#M4715</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-01-23T08:45:13Z</dc:date>
    </item>
    <item>
      <title>Re: Code loaded onto MCXN546VKLT will not run</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2299376#M4722</link>
      <description>&lt;P&gt;I have of course created my project from the correct SDK and have selected the correct processor package (VKLT). The target board I am loading using blhost - do not have general access to the debugger. Developed functionality using evk and then plan is to port code to target processor and load direct.&lt;BR /&gt;&lt;BR /&gt;Cannot get a simple project, toggling GPIO to execute on target.&lt;BR /&gt;&lt;BR /&gt;Any other suggestions - again, all examples seem to be centered around devices that have access to BOOT0 and BOOT1 pins, this package does not have those pins.&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jan 2026 16:53:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2299376#M4722</guid>
      <dc:creator>DBML</dc:creator>
      <dc:date>2026-01-23T16:53:04Z</dc:date>
    </item>
    <item>
      <title>Re: Code loaded onto MCXN546VKLT will not run</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2300200#M4734</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243189"&gt;@DBML&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think you can refer to this.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.jp/docs/en/application-note/AN14460.pdf" target="_blank"&gt;How to program MCX N series internal flash through ISP&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;As you previously described, cmpa and cfpa can also be configured in SEC tools.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING" target="_blank"&gt;MCUXpresso Secure Provisioning Tool | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1769411861924.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374190i7CA338BE6B0116C6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1769411861924.png" alt="Harry_Zhang_0-1769411861924.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jan 2026 07:19:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2300200#M4734</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-01-26T07:19:42Z</dc:date>
    </item>
    <item>
      <title>Re: Code loaded onto MCXN546VKLT will not run</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2303230#M4773</link>
      <description>Harry,&lt;BR /&gt;&lt;BR /&gt;Thanks, I will review and try. I was travelling on Tuesday, thus slow reply.&lt;BR /&gt;&lt;BR /&gt;Yesterday I tried to connect with MCU Link. Can connect and identify the MCU, but will not load code and execute from debugger. Going to explore this more as well as trying to load basic app reviewing the referenced materials above</description>
      <pubDate>Thu, 29 Jan 2026 20:42:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2303230#M4773</guid>
      <dc:creator>DBML</dc:creator>
      <dc:date>2026-01-29T20:42:59Z</dc:date>
    </item>
    <item>
      <title>Re: Code loaded onto MCXN546VKLT will not run</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2303235#M4774</link>
      <description>&lt;P&gt;I wanted to confirm the startup power of the device. You can see from attached that the power up sequence is as expected.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Yellow trace - 3.3 V from external LDO&lt;/LI&gt;&lt;LI&gt;Pink trace - 1.0V from internal LDO VDD_CORE&lt;/LI&gt;&lt;LI&gt;Blue trace - RESET_B line&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;As you can see, the VDD_CORE is essentially stable when the MCU releases the RESET_B line and allows to go high through our pullup.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Startup power sequence" style="width: 800px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374854i4959342D4668BD75/image-size/large?v=v2&amp;amp;px=999" role="button" title="MitosysBaseStartup.png" alt="Startup power sequence" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Startup power sequence&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jan 2026 20:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2303235#M4774</guid>
      <dc:creator>DBML</dc:creator>
      <dc:date>2026-01-29T20:46:46Z</dc:date>
    </item>
    <item>
      <title>Re: Code loaded onto MCXN546VKLT will not run</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2304497#M4782</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243189"&gt;@DBML&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1770020340848.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/375129i4AEF8F1944417DAE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1770020340848.png" alt="Harry_Zhang_0-1770020340848.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Based on the oscilloscope waveforms you provided, I think power‑up sequence is behaving as expected and is fully aligned with the POR requirements in the datasheet.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 02 Feb 2026 08:19:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2304497#M4782</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-02-02T08:19:34Z</dc:date>
    </item>
    <item>
      <title>Re: Code loaded onto MCXN546VKLT will not run</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2321470#M4883</link>
      <description>&lt;P&gt;I have loaded the chip SDK for the 546 and created project I believe correctly.&lt;BR /&gt;&lt;BR /&gt;Note, last week I decided to purchase and populate board with the&amp;nbsp;&lt;SPAN&gt;MCXN947VKLT, worked right off the bat with my base schematic, etc. I did not need to change anything.&lt;BR /&gt;&lt;BR /&gt;Unfortunately 947 is not a solution for me as in this package, USB HS does not exist (seems odd to loose USB HS in your highest end part). I cannot seem to source anywhere the&amp;nbsp;MCXN547VKLT (wonder if this is cause we are all having problems with the 546).&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Feb 2026 20:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Code-loaded-onto-MCXN546VKLT-will-not-run/m-p/2321470#M4883</guid>
      <dc:creator>DBML</dc:creator>
      <dc:date>2026-02-23T20:05:56Z</dc:date>
    </item>
  </channel>
</rss>