<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCXN947 USB hardware design in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2300600#M4741</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241501"&gt;@carlos_o&lt;/a&gt;&lt;BR /&gt;&lt;BR /&gt;Thank you for the response. I followed your guidance and connected the 5V pin directly to the usb_vbus MCXN pin without the voltage divider. The rest of the pins are configured as attached above and I am not using the CC logic chip that controls OTG, not sure if its required. Regardless, I am still not able to get USB to work. I suspect it's a firmware issue at this point.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks for the help!&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jan 2026 16:47:28 GMT</pubDate>
    <dc:creator>ashwinanil</dc:creator>
    <dc:date>2026-01-26T16:47:28Z</dc:date>
    <item>
      <title>MCXN947 USB hardware design</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2299400#M4724</link>
      <description>&lt;P&gt;I would like to configure USB 2.0 HS (USB1) as Peripheral only on the MCXN947VDFT.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I do not need OTG functionality and do not want to add the VBUS Power Control or CC Logic ICs as demonstrated on the FRDM-MCXN947 dev board if not needed.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;I’m using USB type C connector&lt;/LI&gt;&lt;LI&gt;CC1 and CC2 pins are pulled down using 5.1k resistors&lt;/LI&gt;&lt;LI&gt;Can the ID pin remain floating on the uC side?&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Do I need the resistor divider for the USB1_VBUS pin.&amp;nbsp; The MCX-N9XX-EVK adds the divider.&amp;nbsp; The FRDM-MCXN947 does not.&amp;nbsp; Pin is stated to be 5V tolerant.&lt;BR /&gt;&lt;BR /&gt;Will this design work? Any insight is appreciated. Thank you&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ashwinanil_0-1769192484237.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374113iE615DCC143E86138/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ashwinanil_0-1769192484237.png" alt="ashwinanil_0-1769192484237.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ashwinanil_1-1769192493342.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374114iF9D5C94B27301460/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ashwinanil_1-1769192493342.png" alt="ashwinanil_1-1769192493342.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jan 2026 18:25:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2299400#M4724</guid>
      <dc:creator>ashwinanil</dc:creator>
      <dc:date>2026-01-23T18:25:10Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN947 USB hardware design</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2299472#M4727</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254097"&gt;@ashwinanil&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post&lt;/P&gt;
&lt;P&gt;Please refer to the&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/UG10092/page/topics/introduction.html" target="_blank"&gt;UG10092: MCXNx4x Hardware Design Guide | NXP Semiconductors&lt;/A&gt;, there you focus on the chapter&amp;nbsp;&lt;STRONG&gt;8.3 High-speed USB&lt;/STRONG&gt; (that also refers to chapter 8.1) and&amp;nbsp;&lt;STRONG&gt;11 Unused pins&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;The VBUS recommendation is to connect it directly to the USB connector, without using a resistor divider. As noted in the documentation: "The USB VBUS pin is a unique pin in that it is the only 5 V tolerant pin. The VBUS pin from the connector must be routed directly to the USB_VBUS MCX pin."&lt;/P&gt;
&lt;P&gt;The USB_ID the recommendation is leave unconnected&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="carlos_o_0-1769207337822.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374126i880BF357CFD50817/image-size/medium?v=v2&amp;amp;px=400" role="button" title="carlos_o_0-1769207337822.png" alt="carlos_o_0-1769207337822.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Let me know if this information helps.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jan 2026 22:37:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2299472#M4727</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-01-23T22:37:06Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN947 USB hardware design</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2300600#M4741</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241501"&gt;@carlos_o&lt;/a&gt;&lt;BR /&gt;&lt;BR /&gt;Thank you for the response. I followed your guidance and connected the 5V pin directly to the usb_vbus MCXN pin without the voltage divider. The rest of the pins are configured as attached above and I am not using the CC logic chip that controls OTG, not sure if its required. Regardless, I am still not able to get USB to work. I suspect it's a firmware issue at this point.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks for the help!&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jan 2026 16:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2300600#M4741</guid>
      <dc:creator>ashwinanil</dc:creator>
      <dc:date>2026-01-26T16:47:28Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN947 USB hardware design</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2301511#M4758</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254097"&gt;@ashwinanil&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;How are you testing the USB functionality?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jan 2026 20:42:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2301511#M4758</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-01-27T20:42:19Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN947 USB hardware design</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2301518#M4759</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241501"&gt;@carlos_o&lt;/a&gt;&lt;BR /&gt;we are using zephyr&lt;A href="https://github.com/zephyrproject-rtos/zephyr/blob/main//samples/subsys/usb/testusb/README.rst" target="_self"&gt;&amp;nbsp;testusb sample&lt;/A&gt;&amp;nbsp;in Linux for testing. when using the evk we can see the device enumeration and, we can run the usb tests. but when we try to use the custom bord we are getting enumeration error&amp;nbsp; see below dmesg log from the host side.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115238.671144] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: new high-speed USB device number 36 using xhci_hcd &lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115238.785192] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: device descriptor read/64, error -71&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115239.003075] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: device descriptor read/64, error -71&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115239.219143] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: new high-speed USB device number 37 using xhci_hcd &lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115239.333176] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: device descriptor read/64, error -71&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115239.555205] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: device descriptor read/64, error -71&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115239.657153] &lt;/SPAN&gt;&lt;SPAN&gt;usb usb1-port2&lt;/SPAN&gt;&lt;SPAN&gt;: attempt power cycle &lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115240.037109] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: new high-speed USB device number 38 using xhci_hcd &lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115240.037252] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: Device not responding to setup address.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115240.241247] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: Device not responding to setup address.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115240.449124] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: device not accepting address 38, error -71&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115240.562935] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: new high-speed USB device number 39 using xhci_hcd &lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115240.563074] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: Device not responding to setup address.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115240.769196] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: Device not responding to setup address.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115240.977079] &lt;/SPAN&gt;&lt;SPAN&gt;usb 1-2&lt;/SPAN&gt;&lt;SPAN&gt;: device not accepting address 39, error -71&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="courier new,courier" size="1 2 3 4 5 6 7" color="#000000"&gt;&lt;SPAN&gt;[1115240.977312] &lt;/SPAN&gt;&lt;SPAN&gt;usb usb1-port2&lt;/SPAN&gt;&lt;SPAN&gt;: unable to enumerate USB device&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;Indicating that device in this case custom board is not responding to setup packet from Host&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jan 2026 21:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2301518#M4759</guid>
      <dc:creator>wima88</dc:creator>
      <dc:date>2026-01-27T21:07:04Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN947 USB hardware design</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2305502#M4789</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243115"&gt;@wima88&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Apologies the late reply&lt;/P&gt;
&lt;P&gt;Since you are using Zephyr with a custom board, please refer to the following &lt;A href="https://community.nxp.com/t5/Zephyr-Project-Knowledge-Base/Zephyr-custom-boards-and-applications/ta-p/2008567" target="_blank"&gt;Zephyr custom boards and applications&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There are some tips you could follow when developing code to a custom board using Zephyr.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 18:58:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2305502#M4789</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-02-03T18:58:05Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN947 USB hardware design</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2343097#M5130</link>
      <description>&lt;P&gt;This was resolve , thanks for the support&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241501"&gt;@carlos_o&lt;/a&gt;&amp;nbsp;. issue was mismatched clock frequency on HW /FW setup&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Mar 2026 13:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-USB-hardware-design/m-p/2343097#M5130</guid>
      <dc:creator>wima88</dc:creator>
      <dc:date>2026-03-31T13:58:13Z</dc:date>
    </item>
  </channel>
</rss>