<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FreeRTOS Task Not Created on CM4 in MIMXRT1176 Dual-Core Setup in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/FreeRTOS-Task-Not-Created-on-CM4-in-MIMXRT1176-Dual-Core-Setup/m-p/2299439#M4726</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256480"&gt;@meetbhatt2113&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;When debugging, do you see if the CM4 core was booted successfully? How do you see the task creation failed? What parameters are you using to create the task on each core?&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Fri, 23 Jan 2026 20:34:18 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2026-01-23T20:34:18Z</dc:date>
    <item>
      <title>FreeRTOS Task Not Created on CM4 in MIMXRT1176 Dual-Core Setup</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FreeRTOS-Task-Not-Created-on-CM4-in-MIMXRT1176-Dual-Core-Setup/m-p/2296011#M4676</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I am working with the MIMXRT1176 and trying to run the same application on both the CM7 and CM4 cores using FreeRTOS.&lt;/P&gt;&lt;P&gt;I used these SDK examples as the base for my code:&lt;BR /&gt;evkbmimxrt1170_hello_world_secondary_core_boot_primary_core_cm7&lt;BR /&gt;evkbmimxrt1170_hello_world_secondary_core_boot_secondary_core_cm4&lt;/P&gt;&lt;P&gt;On the CM7 core, the FreeRTOS task is created and runs successfully.&lt;BR /&gt;However, when I run the same application logic on the CM4 core, the FreeRTOS task creation fails and the task does not start.&lt;/P&gt;&lt;P&gt;I am not sure what is causing this difference between CM7 and CM4.&lt;BR /&gt;Could this be related to memory allocation, linker script settings, heap or stack size, or any CM4-specific FreeRTOS or clock initialization requirements?&lt;/P&gt;&lt;P&gt;I would appreciate your guidance on what I should check next or how to resolve this issue.&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jan 2026 12:56:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FreeRTOS-Task-Not-Created-on-CM4-in-MIMXRT1176-Dual-Core-Setup/m-p/2296011#M4676</guid>
      <dc:creator>meetbhatt2113</dc:creator>
      <dc:date>2026-01-19T12:56:20Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS Task Not Created on CM4 in MIMXRT1176 Dual-Core Setup</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FreeRTOS-Task-Not-Created-on-CM4-in-MIMXRT1176-Dual-Core-Setup/m-p/2299439#M4726</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256480"&gt;@meetbhatt2113&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;When debugging, do you see if the CM4 core was booted successfully? How do you see the task creation failed? What parameters are you using to create the task on each core?&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jan 2026 20:34:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FreeRTOS-Task-Not-Created-on-CM4-in-MIMXRT1176-Dual-Core-Setup/m-p/2299439#M4726</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2026-01-23T20:34:18Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS Task Not Created on CM4 in MIMXRT1176 Dual-Core Setup</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FreeRTOS-Task-Not-Created-on-CM4-in-MIMXRT1176-Dual-Core-Setup/m-p/2300844#M4746</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the CM7 core, I added a debug print before starting the secondary core. That message appears correctly on the terminal, which confirms that CM7 is running as expected.&lt;/P&gt;&lt;P&gt;Then I switch the debugger to the CM4 core. I added a print statement at the beginning of the CM4 code, and that message also appears successfully on the terminal. This confirms that the CM4 core is booted and executing code properly.&lt;/P&gt;&lt;P&gt;After this initial print on CM4, I attempt to create a FreeRTOS task. At this point, the task creation fails, and an error message is printed on the terminal. The task never enters the running state.&lt;/P&gt;&lt;P&gt;I have attached a snapshot of the terminal output showing the successful CM4 boot message followed by the task creation failure.&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cm4_task_fail.png" style="width: 788px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374329iE31980111F6CAAEF/image-size/large?v=v2&amp;amp;px=999" role="button" title="cm4_task_fail.png" alt="cm4_task_fail.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;cm4_task_fail.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jan 2026 04:54:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FreeRTOS-Task-Not-Created-on-CM4-in-MIMXRT1176-Dual-Core-Setup/m-p/2300844#M4746</guid>
      <dc:creator>meetbhatt2113</dc:creator>
      <dc:date>2026-01-27T04:54:54Z</dc:date>
    </item>
  </channel>
</rss>