<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8Mimi LPDDR4 ZQ0 and ZQ1 ZQ calibration reference design in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/i-MX8Mimi-LPDDR4-ZQ0-and-ZQ1-ZQ-calibration-reference-design/m-p/2296225#M4677</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252903"&gt;@Zack8&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No need to connect R6. One ZQ calibration&amp;nbsp;resistance is fine.&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
    <pubDate>Tue, 20 Jan 2026 02:12:29 GMT</pubDate>
    <dc:creator>pengyong_zhang</dc:creator>
    <dc:date>2026-01-20T02:12:29Z</dc:date>
    <item>
      <title>i.MX8Mimi LPDDR4 ZQ0 and ZQ1 ZQ calibration reference design</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/i-MX8Mimi-LPDDR4-ZQ0-and-ZQ1-ZQ-calibration-reference-design/m-p/2295741#M4672</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I find file SPF31399, R6 is DNP; another file SPF47712 is same, the MT53D512M32D2DS is dual die,&amp;nbsp;So, should 240-ohm resistors be placed R6?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which vision is the latest?&lt;/P&gt;&lt;P&gt;MT53D512M32D2DS will EOL, we wanted to replace it to MT53E1G32D2FW, may I ask which parts of the hardware need to be modified? Or is it completely compatible without the need to modify the PCB?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;A href="https://community.nxp.com/t5/forums/postpage/choose-node/true/attachments-key/0043819e-2bea-4415-8d48-6c208c41b44a/board-id/MCX#" target="_blank" rel="noopener"&gt; HW-Open-Source&lt;/A&gt;&amp;nbsp;#i.MX8 mini&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jan 2026 07:30:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/i-MX8Mimi-LPDDR4-ZQ0-and-ZQ1-ZQ-calibration-reference-design/m-p/2295741#M4672</guid>
      <dc:creator>Zack8</dc:creator>
      <dc:date>2026-01-19T07:30:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8Mimi LPDDR4 ZQ0 and ZQ1 ZQ calibration reference design</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/i-MX8Mimi-LPDDR4-ZQ0-and-ZQ1-ZQ-calibration-reference-design/m-p/2296225#M4677</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252903"&gt;@Zack8&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No need to connect R6. One ZQ calibration&amp;nbsp;resistance is fine.&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jan 2026 02:12:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/i-MX8Mimi-LPDDR4-ZQ0-and-ZQ1-ZQ-calibration-reference-design/m-p/2296225#M4677</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2026-01-20T02:12:29Z</dc:date>
    </item>
  </channel>
</rss>