<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Operations over the SD card on MCX A14x/A15x in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Operations-over-the-SD-card-on-MCX-A14x-A15x/m-p/1888202#M466</link>
    <description>&lt;P&gt;Hello I would like to use MCXN EVK For Data Logging Application with this shield: &lt;A href="https://botland.store/arduino-shield-communication/8238-datalogger-shield-v10-rtc-ds1307-with-sd-card-reader-shield-for-arduino-iduino-st1046-5903351241205.html" target="_blank"&gt;https://botland.store/arduino-shield-communication/8238-datalogger-shield-v10-rtc-ds1307-with-sd-card-reader-shield-for-arduino-iduino-st1046-5903351241205.html&lt;/A&gt;, is&amp;nbsp;unfortunately I didn't find any example for writing/reading from SD card that I could use.&amp;nbsp;Is there an example to base it on?&lt;/P&gt;</description>
    <pubDate>Sat, 15 Jun 2024 18:47:57 GMT</pubDate>
    <dc:creator>Doly02</dc:creator>
    <dc:date>2024-06-15T18:47:57Z</dc:date>
    <item>
      <title>Operations over the SD card on MCX A14x/A15x</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Operations-over-the-SD-card-on-MCX-A14x-A15x/m-p/1888202#M466</link>
      <description>&lt;P&gt;Hello I would like to use MCXN EVK For Data Logging Application with this shield: &lt;A href="https://botland.store/arduino-shield-communication/8238-datalogger-shield-v10-rtc-ds1307-with-sd-card-reader-shield-for-arduino-iduino-st1046-5903351241205.html" target="_blank"&gt;https://botland.store/arduino-shield-communication/8238-datalogger-shield-v10-rtc-ds1307-with-sd-card-reader-shield-for-arduino-iduino-st1046-5903351241205.html&lt;/A&gt;, is&amp;nbsp;unfortunately I didn't find any example for writing/reading from SD card that I could use.&amp;nbsp;Is there an example to base it on?&lt;/P&gt;</description>
      <pubDate>Sat, 15 Jun 2024 18:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Operations-over-the-SD-card-on-MCX-A14x-A15x/m-p/1888202#M466</guid>
      <dc:creator>Doly02</dc:creator>
      <dc:date>2024-06-15T18:47:57Z</dc:date>
    </item>
    <item>
      <title>Re: Operations over the SD card on MCX A14x/A15x</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Operations-over-the-SD-card-on-MCX-A14x-A15x/m-p/1889924#M479</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235054"&gt;@Doly02&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can download the&amp;nbsp;SDK_2_14_0_FRDM-MCXN947 from the NXP official websit.&lt;/P&gt;
&lt;P&gt;Under this path SDK_2_14_0_FRDM-MCXN947\boards\frdmmcxn947\sdmmc_examples&lt;/P&gt;
&lt;P&gt;You can find the SD example.&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jun 2024 02:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Operations-over-the-SD-card-on-MCX-A14x-A15x/m-p/1889924#M479</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-19T02:38:52Z</dc:date>
    </item>
  </channel>
</rss>