<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックFRDM-MCXW72</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXW72/m-p/2289480#M4607</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I just received two FRDM-MCXW72 boards, I have MCUXpresso for VCS setup and was going to try to compile/run the wireless ranging example. I saw a note that the NBU should be updated to the latest, but in the binaries folder I do not see a file for the FRDM-MCXW72 with HADM in the file name there are only two. and they are:&lt;/P&gt;&lt;P&gt;mcxw72_nbu_ble_all_hosted.bin&lt;/P&gt;&lt;P&gt;mcxw72_nbu_ble_xp_hosted.bin&lt;/P&gt;&lt;P&gt;Does either of these include HADM in them?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, when will training materials be available, and when will the FRDM-MCXW72 board be a selection in the SDK builder tool&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jan 2026 13:06:20 GMT</pubDate>
    <dc:creator>brianmohlman</dc:creator>
    <dc:date>2026-01-07T13:06:20Z</dc:date>
    <item>
      <title>FRDM-MCXW72</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXW72/m-p/2289480#M4607</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I just received two FRDM-MCXW72 boards, I have MCUXpresso for VCS setup and was going to try to compile/run the wireless ranging example. I saw a note that the NBU should be updated to the latest, but in the binaries folder I do not see a file for the FRDM-MCXW72 with HADM in the file name there are only two. and they are:&lt;/P&gt;&lt;P&gt;mcxw72_nbu_ble_all_hosted.bin&lt;/P&gt;&lt;P&gt;mcxw72_nbu_ble_xp_hosted.bin&lt;/P&gt;&lt;P&gt;Does either of these include HADM in them?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, when will training materials be available, and when will the FRDM-MCXW72 board be a selection in the SDK builder tool&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jan 2026 13:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXW72/m-p/2289480#M4607</guid>
      <dc:creator>brianmohlman</dc:creator>
      <dc:date>2026-01-07T13:06:20Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MCXW72</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXW72/m-p/2290388#M4615</link>
      <description>&lt;P lang="es-419"&gt;Hello, hope you are doing well.&lt;/P&gt;
&lt;P lang="es-419"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To run the wireless ranging examples in MCXW72, the "mcxw72_nbu_ble_all_hosted.bin" file can be used, as this binary file includes supported HADM/CS features. The FRDM-MCXW72 SDK can be downloaded from the &lt;A href="https://mcuxpresso.nxp.com/" target="_blank"&gt;MCUXpresso SDK Builder&lt;/A&gt; and the binary files are provided in the following SDK path: ../mcuxsdk/middleware/wireless/ble_controller/bin&lt;/P&gt;
&lt;P lang="es-419"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can also follow this guide: &lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/middleware/wireless/bluetooth/doc/CS%20Wireless%20Ranging%20Demo%20Application%20User%20Guide/topics/wireless_ranging_demo_application_setup.html#wireless-ranging-demo-application-setup" target="_blank"&gt;Wireless ranging demo application setup — MCUXpresso SDK Documentation&lt;/A&gt;&lt;/P&gt;
&lt;P lang="es-419"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P lang="es-419"&gt;Hope this helps!&lt;/P&gt;
&lt;P lang="es-419"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P lang="es-419"&gt;Best regards,&lt;BR /&gt;Ana Sofia.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jan 2026 17:37:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXW72/m-p/2290388#M4615</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2026-01-08T17:37:35Z</dc:date>
    </item>
  </channel>
</rss>