<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 Re: RT600+KEIL5+JLINK(FLM flash programming issue)</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/RT600-KEIL5-JLINK-FLM-flash-programming-issue/m-p/2269058#M4559</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225639"&gt;@Jokerufo&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I tested with on board JLink and it works.&lt;/P&gt;
&lt;P&gt;First, ensure that the FLM you selected is the two with the FlexSPI_B suffix. If this step is confirmed correct, put the board into serial download mode and use SEC or MCUBootUtility to erase the Flash before attempting reprogramming.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
    <pubDate>Fri, 26 Dec 2025 02:16:12 GMT</pubDate>
    <dc:creator>Gavin_Jia</dc:creator>
    <dc:date>2025-12-26T02:16:12Z</dc:date>
    <item>
      <title>RT600+KEIL5+JLINK(FLM flash programming issue)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/RT600-KEIL5-JLINK-FLM-flash-programming-issue/m-p/2268777#M4555</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I am developing audio product on RT685-AUD-EVK, i use KEIL5 as devl tool, there are some issues when i use arm algorithm FLM file to program flash, attachment is FLM i used, please help me to solve those issue, thanks.&lt;/P&gt;&lt;P&gt;1)MIMXRT685-AUD-EVK&lt;/P&gt;&lt;P&gt;2)Program LPC4322 to jlink MODE&lt;/P&gt;&lt;P&gt;3) JLINK CAN ACCESS RT586 chip&lt;/P&gt;&lt;P&gt;4)keil program flash incounter can't halt CPU&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;JLink Info: InitTarget() start&lt;BR /&gt;JLink Info:&amp;nbsp;&lt;BR /&gt;JLink Info: J-Link script: i.MXRT6xx Cortex-M33 core J-Link script&lt;BR /&gt;JLink Info:&amp;nbsp;&lt;BR /&gt;JLink Info: DAP-IDCODE:0x002A0000&lt;BR /&gt;JLink Info: InitTarget() end&lt;BR /&gt;JLink Info: Found SW-DP with ID 0x6BA02477&lt;BR /&gt;JLink Info: DPIDR: 0x6BA02477&lt;BR /&gt;JLink Info: CoreSight SoC-400 or earlier&lt;BR /&gt;JLink Info: Scanning AP map to find all available APs&lt;BR /&gt;JLink Info: AP[1]: Stopped AP scan as end of AP map has been reached&lt;BR /&gt;JLink Info: AP[0]: AHB-AP (IDR: 0x84770001)&lt;BR /&gt;JLink Info: Iterating through AP map to find AHB-AP to use&lt;BR /&gt;JLink Info: AP[0]: Core found&lt;BR /&gt;JLink Info: AP[0]: AHB-AP ROM base: 0xE00FE000&lt;BR /&gt;JLink Info: CPUID register: 0x410FD213. Implementer code: 0x41 (ARM)&lt;BR /&gt;JLink Info: Feature set: Mainline&lt;BR /&gt;JLink Info: Found Cortex-M33 r0p3, Little endian.&lt;BR /&gt;JLink Info: FPUnit: 8 code (BP) slots and 0 literal slots&lt;BR /&gt;JLink Info: Security extension: implemented&lt;BR /&gt;JLink Info: Secure debug: enabled&lt;BR /&gt;JLink Info: CoreSight components:&lt;BR /&gt;JLink Info: ROMTbl[0] @ E00FE000&lt;BR /&gt;JLink Info: [0][0]: E00FF000 CID B105100D PID 000BB4C9 ROM Table&lt;BR /&gt;JLink Info: ROMTbl[1] @ E00FF000&lt;BR /&gt;JLink Info: [1][0]: E000E000 CID B105900D PID 000BBD21 DEVARCH 47702A04 DEVTYPE 00 Cortex-M33&lt;BR /&gt;JLink Info: [1][1]: E0001000 CID B105900D PID 000BBD21 DEVARCH 47701A02 DEVTYPE 00 DWT&lt;BR /&gt;JLink Info: [1][2]: E0002000 CID B105900D PID 000BBD21 DEVARCH 47701A03 DEVTYPE 00 FPB&lt;BR /&gt;JLink Info: [1][3]: E0000000 CID B105900D PID 000BBD21 DEVARCH 47701A01 DEVTYPE 43 ITM&lt;BR /&gt;JLink Info: [1][5]: E0041000 CID B105900D PID 002BBD21 DEVARCH 47724A13 DEVTYPE 13 ETM&lt;BR /&gt;JLink Info: [1][6]: E0042000 CID B105900D PID 000BBD21 DEVARCH 47701A14 DEVTYPE 14 CSS600-CTI&lt;BR /&gt;JLink Info: [0][1]: E0040000 CID B105900D PID 000BBD21 DEVARCH 00000000 DEVTYPE 11 TPIU&lt;BR /&gt;ROMTableAddr = 0xE00FE000&lt;BR /&gt;JLink Info: ResetTarget() start&lt;BR /&gt;JLink Info: Reset external flash&lt;BR /&gt;JLink Info: Set watch point&lt;BR /&gt;JLink Info: Execute SYSRESETREQ via AIRCR&lt;BR /&gt;JLink Info: ResetTarget() end&lt;BR /&gt;JLink Info: CPU could not be halted&lt;BR /&gt;JLink Error: Failed to halt CPU.&lt;BR /&gt;JLink Info: CPU could not be halted&lt;BR /&gt;Warning: Secure Cortex-M device stop can be delayed!&lt;BR /&gt;Error: Flash Download failed - Target DLL has been cancelled&lt;BR /&gt;Flash Load finished at 20:52:32&lt;/P&gt;</description>
      <pubDate>Thu, 25 Dec 2025 02:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/RT600-KEIL5-JLINK-FLM-flash-programming-issue/m-p/2268777#M4555</guid>
      <dc:creator>Jokerufo</dc:creator>
      <dc:date>2025-12-25T02:25:15Z</dc:date>
    </item>
    <item>
      <title>Re: RT600+KEIL5+JLINK(FLM flash programming issue)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/RT600-KEIL5-JLINK-FLM-flash-programming-issue/m-p/2269058#M4559</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225639"&gt;@Jokerufo&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I tested with on board JLink and it works.&lt;/P&gt;
&lt;P&gt;First, ensure that the FLM you selected is the two with the FlexSPI_B suffix. If this step is confirmed correct, put the board into serial download mode and use SEC or MCUBootUtility to erase the Flash before attempting reprogramming.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Fri, 26 Dec 2025 02:16:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/RT600-KEIL5-JLINK-FLM-flash-programming-issue/m-p/2269058#M4559</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2025-12-26T02:16:12Z</dc:date>
    </item>
  </channel>
</rss>