<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NHS3152UK/A1Z in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/NHS3152UK-A1Z/m-p/2260793#M4506</link>
    <description>&lt;P&gt;1. Connect to VCC with a pull-up resistor.&lt;/P&gt;
&lt;P&gt;2. Use software reset if RESETN not use&lt;/P&gt;
&lt;P&gt;3. Yes for initial development.&amp;nbsp; It is better to use NHS3152 board as there are some features different.&lt;/P&gt;</description>
    <pubDate>Fri, 12 Dec 2025 08:26:43 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2025-12-12T08:26:43Z</dc:date>
    <item>
      <title>NHS3152UK/A1Z</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/NHS3152UK-A1Z/m-p/2258494#M4488</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am designing a new board around the&amp;nbsp;NHS3152UK/A1Z product. I have the following specific questions:&lt;/P&gt;&lt;P&gt;1) I have no need for a hardware reset. What should I do with the RESETN Pin (leave it unconnected, tied to VCC, or what)?&lt;/P&gt;&lt;P&gt;2) If I don't use the RESETN Pin (as I intend) how can the device be reset during the firmware development? Note that for firware development, the intent is to use the development board refernced in&amp;nbsp;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/ntag-smartsensor/nhs3100-sensor-board:NHS3100SENSORADK" target="_blank"&gt;NHS3100 Sensor Board | NXP Semiconductors&lt;/A&gt;&amp;nbsp;using I2C pins to download the firmware.&lt;/P&gt;&lt;P&gt;3) Can the NHS3100 Development Board be used to develop firmware for the NHS3152 Device?&lt;/P&gt;</description>
      <pubDate>Wed, 10 Dec 2025 00:56:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/NHS3152UK-A1Z/m-p/2258494#M4488</guid>
      <dc:creator>MoAbdol</dc:creator>
      <dc:date>2025-12-10T00:56:29Z</dc:date>
    </item>
    <item>
      <title>Re: NHS3152UK/A1Z</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/NHS3152UK-A1Z/m-p/2260793#M4506</link>
      <description>&lt;P&gt;1. Connect to VCC with a pull-up resistor.&lt;/P&gt;
&lt;P&gt;2. Use software reset if RESETN not use&lt;/P&gt;
&lt;P&gt;3. Yes for initial development.&amp;nbsp; It is better to use NHS3152 board as there are some features different.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Dec 2025 08:26:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/NHS3152UK-A1Z/m-p/2260793#M4506</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2025-12-12T08:26:43Z</dc:date>
    </item>
    <item>
      <title>Re: NHS3152UK/A1Z</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/NHS3152UK-A1Z/m-p/2265313#M4538</link>
      <description>&lt;P&gt;Thank you for your prompt response.&lt;/P&gt;&lt;P&gt;We have completed the hardware development. Now, I need to get started on the custom firmware we would like to run the&amp;nbsp;&lt;SPAN&gt;NHS3152UK/A1Z Device. I am a fully-experienced C/C++ Programmer but need some help to get started, as listed below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;a) I would like a link to the Eclipse IDE to download and install on my development platform&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;b) I need a "walkthrough" to show me the main steps for loading a simple (like the Blinky) application source code into Eclipse, build it and deploy it for testing&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please help me with the above steps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Mo&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 19:37:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/NHS3152UK-A1Z/m-p/2265313#M4538</guid>
      <dc:creator>MoAbdol</dc:creator>
      <dc:date>2025-12-17T19:37:22Z</dc:date>
    </item>
  </channel>
</rss>