<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Reduce Frequency of IMX93 by accesing resistors from userspace in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Reduce-Frequency-of-IMX93-by-accesing-resistors-from-userspace/m-p/1883124#M427</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;CPU Frequency is changed between Low Power Modes (ND, OD, etc.). Please refer to &lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX93-It-have-no-cpufreq-directory-under-sys-fs/m-p/1706119" target="_self"&gt;this post&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jun 2024 23:22:31 GMT</pubDate>
    <dc:creator>JosephAtNXP</dc:creator>
    <dc:date>2024-06-06T23:22:31Z</dc:date>
    <item>
      <title>Reduce Frequency of IMX93 by accesing resistors from userspace</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Reduce-Frequency-of-IMX93-by-accesing-resistors-from-userspace/m-p/1882732#M424</link>
      <description>&lt;P&gt;I am using IMX93 EVK where I required to reduce cpu frequency of A core which is currently 1600MHz.&lt;BR /&gt;&lt;BR /&gt;I want to reduce it up to 200MHz,&lt;BR /&gt;&lt;BR /&gt;Earlier for IMX8ULP EVK I followed below method and I was able to control frequency on A core with accessing appropriate resisters&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;PRE&gt;# Switch a35 to FRO 192 MHz
/unit_tests/memtool -32 0x292c0014=0x08000000

# Set PLLEN to 0
/unit_tests/memtool -32 0x292c0500=0x03000000

# Read and set the division and multiplication factors
/unit_tests/memtool -32 0x292c0014 1
/unit_tests/memtool -32 0x292c0510 1


# Set PLLEN to 1"
/unit_tests/memtool -32 0x292c0500=0x03000001

# Switch a35 to PLL2"
/unit_tests/memtool -32 0x292c0014=0x18000000

mhz&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;I checked reference manual of IMX93, but I am not able to get resistor by which I can control clock,&lt;BR /&gt;&lt;BR /&gt;Can anyone guide me on this?&lt;BR /&gt;&lt;BR /&gt;&lt;LI-PRODUCT title="IMX93QSB" id="IMX93QSB"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jun 2024 11:59:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Reduce-Frequency-of-IMX93-by-accesing-resistors-from-userspace/m-p/1882732#M424</guid>
      <dc:creator>dhruvinrajpura</dc:creator>
      <dc:date>2024-06-06T11:59:59Z</dc:date>
    </item>
    <item>
      <title>Re: Reduce Frequency of IMX93 by accesing resistors from userspace</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Reduce-Frequency-of-IMX93-by-accesing-resistors-from-userspace/m-p/1883124#M427</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;CPU Frequency is changed between Low Power Modes (ND, OD, etc.). Please refer to &lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX93-It-have-no-cpufreq-directory-under-sys-fs/m-p/1706119" target="_self"&gt;this post&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jun 2024 23:22:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Reduce-Frequency-of-IMX93-by-accesing-resistors-from-userspace/m-p/1883124#M427</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-06-06T23:22:31Z</dc:date>
    </item>
  </channel>
</rss>