<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: How to create a portable manufacturing package with MCUXpresso Secure Provisioning Tool 25.06?</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/How-to-create-a-portable-manufacturing-package-with-MCUXpresso/m-p/2181209#M4154</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255584"&gt;@fabiorossi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;the manufacturing package should be portable. The script uses environment variable to access tool path, if the tool is installed in different directory, see&amp;nbsp;&lt;SPAN&gt;SPT_INSTALL_BIN&lt;/SPAN&gt;.&lt;/P&gt;
&lt;P&gt;Info the tool documentation:&amp;nbsp;&lt;A href="https://docs.mcuxpresso.nxp.com/secure/latest/07_generic_workflows.html#manufacturing-operations" target="_blank" rel="noopener"&gt;Generic workflows — MCUXpresso Secure Provisioning Tool 25.06&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Note: manufacturing package can be installed only to the same tool version, that was used to create the package.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 07 Oct 2025 12:59:15 GMT</pubDate>
    <dc:creator>marek-trmac</dc:creator>
    <dc:date>2025-10-07T12:59:15Z</dc:date>
    <item>
      <title>How to create a portable manufacturing package with MCUXpresso Secure Provisioning Tool 25.06?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/How-to-create-a-portable-manufacturing-package-with-MCUXpresso/m-p/2181153#M4153</link>
      <description>&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;I am currently using the MCUX Secure Provisioning Tool v25.06 to generate a manufacturing package for an i.MX RT1052 device.&lt;BR /&gt;The package is successfully created and works correctly on the same PC where it was generated. However, when I try to use the same manufacturing package on a different computer, the provisioning process fails because several directory paths are not found.&lt;/P&gt;&lt;P&gt;It seems that the exported package contains absolute file paths instead of relative ones, and the required files are not automatically included inside the .zip package.&lt;BR /&gt;As a result, the package is not portable between different environments or PCs.&lt;/P&gt;&lt;P&gt;Could you please confirm if this is the expected behavior in version 25.06, or if there is an option to export a fully self-contained (portable) manufacturing package that includes all dependencies and uses relative paths?&lt;BR /&gt;If not, is there a recommended procedure or update to make the generated package portable?&lt;/P&gt;&lt;P&gt;Thank you in advance for your help and clarification.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Fabio Rossi&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 11:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/How-to-create-a-portable-manufacturing-package-with-MCUXpresso/m-p/2181153#M4153</guid>
      <dc:creator>fabiorossi</dc:creator>
      <dc:date>2025-10-07T11:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to create a portable manufacturing package with MCUXpresso Secure Provisioning Tool 25.06?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/How-to-create-a-portable-manufacturing-package-with-MCUXpresso/m-p/2181209#M4154</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255584"&gt;@fabiorossi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;the manufacturing package should be portable. The script uses environment variable to access tool path, if the tool is installed in different directory, see&amp;nbsp;&lt;SPAN&gt;SPT_INSTALL_BIN&lt;/SPAN&gt;.&lt;/P&gt;
&lt;P&gt;Info the tool documentation:&amp;nbsp;&lt;A href="https://docs.mcuxpresso.nxp.com/secure/latest/07_generic_workflows.html#manufacturing-operations" target="_blank" rel="noopener"&gt;Generic workflows — MCUXpresso Secure Provisioning Tool 25.06&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Note: manufacturing package can be installed only to the same tool version, that was used to create the package.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 12:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/How-to-create-a-portable-manufacturing-package-with-MCUXpresso/m-p/2181209#M4154</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2025-10-07T12:59:15Z</dc:date>
    </item>
  </channel>
</rss>