<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCXN947 EVK cannot initialize PHY in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-EVK-cannot-initialize-PHY/m-p/2175916#M4115</link>
    <description>&lt;P&gt;I am starting a new project using the MCXN947. I have both the FRDM-MCXN947 and the MCX-N9XX-EVK demo boards. I will be utilizing LWIP so I downloaded the LWIP-PING examples for both boards. The example runs fine on the FRDM but will not run on the EVK. I keep getting "Cannot initialize PHY" on the EVK. Both boards seem to have the same PHY chip (lan8741A-EN). Can someone offer a little guidance on the issue, it would be much appreciated.&lt;/P&gt;</description>
    <pubDate>Thu, 25 Sep 2025 15:10:20 GMT</pubDate>
    <dc:creator>embedbytes</dc:creator>
    <dc:date>2025-09-25T15:10:20Z</dc:date>
    <item>
      <title>MCXN947 EVK cannot initialize PHY</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-EVK-cannot-initialize-PHY/m-p/2175916#M4115</link>
      <description>&lt;P&gt;I am starting a new project using the MCXN947. I have both the FRDM-MCXN947 and the MCX-N9XX-EVK demo boards. I will be utilizing LWIP so I downloaded the LWIP-PING examples for both boards. The example runs fine on the FRDM but will not run on the EVK. I keep getting "Cannot initialize PHY" on the EVK. Both boards seem to have the same PHY chip (lan8741A-EN). Can someone offer a little guidance on the issue, it would be much appreciated.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Sep 2025 15:10:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-EVK-cannot-initialize-PHY/m-p/2175916#M4115</guid>
      <dc:creator>embedbytes</dc:creator>
      <dc:date>2025-09-25T15:10:20Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN947 EVK cannot initialize PHY</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-EVK-cannot-initialize-PHY/m-p/2177698#M4126</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186131"&gt;@embedbytes&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Are you making sure to follow the board setting that are listed on the "example_board_readme.md" file for the &lt;SPAN&gt;MCX-N9XX-EVK? These include:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Connecting JP13 2-3 pin.&lt;BR /&gt;Populating R274 to sync reference clock.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR,&lt;BR /&gt;Edwin.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 20:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-EVK-cannot-initialize-PHY/m-p/2177698#M4126</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-09-29T20:27:57Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN947 EVK cannot initialize PHY</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-EVK-cannot-initialize-PHY/m-p/2200897#M4331</link>
      <description>&lt;P&gt;Yes, Thank for the guidance , all is good now&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Nov 2025 14:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-EVK-cannot-initialize-PHY/m-p/2200897#M4331</guid>
      <dc:creator>embedbytes</dc:creator>
      <dc:date>2025-11-07T14:35:02Z</dc:date>
    </item>
  </channel>
</rss>