<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 MIMXRT1189 interface</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MIMXRT1189-interface/m-p/2171993#M4080</link>
    <description>&lt;P&gt;hi, we are planning to use&amp;nbsp;&lt;SPAN&gt;MIMXRT1189CVM8C for one of the applications where 3 MII interfaces are required.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have chosen all 3 MII interfaces on TSN fabric and using iMX pin config tool MCUXpresso Config tool ver 25.6.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. ETH2 and ETH3 for 2 PHYs, want to use shared MDIO/MDC for these 2 PHYs&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. ETH1 for another MII based PHY, here dedicated MDIO/MDC is preferred.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Now as per config tool, ETH2 and ETH3 both have MDIO/MDC signals but ETH0 and ETH1 don't.&lt;/P&gt;&lt;P&gt;First of all, can I share MDIO/MDC as mentioned in point 1 &amp;amp; 2.&lt;/P&gt;&lt;P&gt;Second, on ETH1, CRS and COL signals are getting omitted if I chose one MDIO/MDC pair to be used, now these signals are required if HALF duplex operation is needed.&lt;BR /&gt;&lt;BR /&gt;Can you please help with correct interfacing scheme here.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 18 Sep 2025 11:49:31 GMT</pubDate>
    <dc:creator>sunney79</dc:creator>
    <dc:date>2025-09-18T11:49:31Z</dc:date>
    <item>
      <title>MIMXRT1189 interface</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MIMXRT1189-interface/m-p/2171993#M4080</link>
      <description>&lt;P&gt;hi, we are planning to use&amp;nbsp;&lt;SPAN&gt;MIMXRT1189CVM8C for one of the applications where 3 MII interfaces are required.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have chosen all 3 MII interfaces on TSN fabric and using iMX pin config tool MCUXpresso Config tool ver 25.6.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. ETH2 and ETH3 for 2 PHYs, want to use shared MDIO/MDC for these 2 PHYs&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. ETH1 for another MII based PHY, here dedicated MDIO/MDC is preferred.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Now as per config tool, ETH2 and ETH3 both have MDIO/MDC signals but ETH0 and ETH1 don't.&lt;/P&gt;&lt;P&gt;First of all, can I share MDIO/MDC as mentioned in point 1 &amp;amp; 2.&lt;/P&gt;&lt;P&gt;Second, on ETH1, CRS and COL signals are getting omitted if I chose one MDIO/MDC pair to be used, now these signals are required if HALF duplex operation is needed.&lt;BR /&gt;&lt;BR /&gt;Can you please help with correct interfacing scheme here.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 11:49:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MIMXRT1189-interface/m-p/2171993#M4080</guid>
      <dc:creator>sunney79</dc:creator>
      <dc:date>2025-09-18T11:49:31Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1189 interface</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MIMXRT1189-interface/m-p/2173704#M4097</link>
      <description>&lt;P&gt;Yes, MDIO/MDC can be shared.&lt;/P&gt;
&lt;P&gt;If the MCUXpresso Config Tool doesn’t show MDIO/MDC for ETH1, it’s likely due to pin-muxing limitations. AN14251 confirms that not all ENET instances have dedicated MDIO/MDC pins, and sometimes you must share the bus or use alternate pin functions&lt;BR /&gt;These are the CRS and COL signals for ETH1:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Omar_Anguiano_0-1758565419126.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358011i1F5E9B20CCE64119/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Omar_Anguiano_0-1758565419126.png" alt="Omar_Anguiano_0-1758565419126.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Omar_Anguiano_0-1758565419126.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Omar&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Sep 2025 18:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MIMXRT1189-interface/m-p/2173704#M4097</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-09-22T18:24:31Z</dc:date>
    </item>
  </channel>
</rss>