<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic cmsis_enet_1G and 100m in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/cmsis-enet-1G-and-100m/m-p/2164274#M3909</link>
    <description>&lt;P&gt;I am working on a project with the i.MX/RT platform and I need to run both 100 Mbps Ethernet (ENET) and 1 Gbps Ethernet (ENET_QOS) in the same application.&lt;/P&gt;&lt;P&gt;Is it possible to manage both interfaces together in a single project using the CMSIS-Driver (Driver_ETH_MAC + Driver_ETH_PHY)?&lt;/P&gt;&lt;P&gt;If yes, what is the recommended approach for initialization and task handling (e.g., separate instances of the CMSIS driver for each port)?&lt;/P&gt;&lt;P&gt;If one Ethernet interface is running with the CMSIS driver and the other is managed using a different driver stack (non-CMSIS, platform-specific), will both coexist and work correctly? Or do they need to be aligned under the same framework?&lt;/P&gt;&lt;P&gt;Any reference examples or documentation for handling dual Ethernet (100M + 1G) simultaneously would be very helpful.&amp;nbsp; &lt;LI-PRODUCT title="i.MX-RT1170" id="i.MX-RT1170"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 05 Sep 2025 08:55:02 GMT</pubDate>
    <dc:creator>raviraj13</dc:creator>
    <dc:date>2025-09-05T08:55:02Z</dc:date>
    <item>
      <title>cmsis_enet_1G and 100m</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/cmsis-enet-1G-and-100m/m-p/2164274#M3909</link>
      <description>&lt;P&gt;I am working on a project with the i.MX/RT platform and I need to run both 100 Mbps Ethernet (ENET) and 1 Gbps Ethernet (ENET_QOS) in the same application.&lt;/P&gt;&lt;P&gt;Is it possible to manage both interfaces together in a single project using the CMSIS-Driver (Driver_ETH_MAC + Driver_ETH_PHY)?&lt;/P&gt;&lt;P&gt;If yes, what is the recommended approach for initialization and task handling (e.g., separate instances of the CMSIS driver for each port)?&lt;/P&gt;&lt;P&gt;If one Ethernet interface is running with the CMSIS driver and the other is managed using a different driver stack (non-CMSIS, platform-specific), will both coexist and work correctly? Or do they need to be aligned under the same framework?&lt;/P&gt;&lt;P&gt;Any reference examples or documentation for handling dual Ethernet (100M + 1G) simultaneously would be very helpful.&amp;nbsp; &lt;LI-PRODUCT title="i.MX-RT1170" id="i.MX-RT1170"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Sep 2025 08:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/cmsis-enet-1G-and-100m/m-p/2164274#M3909</guid>
      <dc:creator>raviraj13</dc:creator>
      <dc:date>2025-09-05T08:55:02Z</dc:date>
    </item>
    <item>
      <title>Re: cmsis_enet_1G and 100m</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/cmsis-enet-1G-and-100m/m-p/2165386#M3921</link>
      <description>&lt;P&gt;If no MII connection is used (only RMII and RGMII is used), all three interfaces can be used simultaneously. Each interface has to use a different set of pins. MDIO, MDC pins can be shared by more PHYs or each PHY can be connected to an individual pair of MDC, MDIO pins.&lt;BR /&gt;To achieve this, it is suggested to use different instances of CMSIS driver.&lt;BR /&gt;Unfortunately, we don’t have any example to run multiple interfaces on the same application.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 08 Sep 2025 18:33:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/cmsis-enet-1G-and-100m/m-p/2165386#M3921</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-09-08T18:33:52Z</dc:date>
    </item>
  </channel>
</rss>