<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックMCXE317MPA</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXE317MPA/m-p/2163981#M3903</link>
    <description>&lt;P&gt;I saw on the official website that there is a document for the MCXE317MPA chip, which seems similar to the S32K312. Are there any differences between these two chips, or have they solved any bugs of the S32K312?&lt;/P&gt;</description>
    <pubDate>Fri, 05 Sep 2025 02:24:49 GMT</pubDate>
    <dc:creator>Neo1096</dc:creator>
    <dc:date>2025-09-05T02:24:49Z</dc:date>
    <item>
      <title>MCXE317MPA</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXE317MPA/m-p/2163981#M3903</link>
      <description>&lt;P&gt;I saw on the official website that there is a document for the MCXE317MPA chip, which seems similar to the S32K312. Are there any differences between these two chips, or have they solved any bugs of the S32K312?&lt;/P&gt;</description>
      <pubDate>Fri, 05 Sep 2025 02:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXE317MPA/m-p/2163981#M3903</guid>
      <dc:creator>Neo1096</dc:creator>
      <dc:date>2025-09-05T02:24:49Z</dc:date>
    </item>
    <item>
      <title>Re: MCXE317MPA</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXE317MPA/m-p/2165527#M3922</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229677"&gt;@Neo1096&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&amp;nbsp;They are very similar, but not exactly the same.&lt;/P&gt;
&lt;P&gt;We proposes 2 portfolios of microcontrollers with similar hardware configuration: S32K31 automotive microcontrollers focus on automotive applications requiring Automotive-grade components and certification.&lt;/P&gt;
&lt;P&gt;MCX E31 focuses on industrial applications with industrial mission profiles and certification.&lt;BR /&gt;While S32K31 also serves industrial applications. MCX E31 provides a complete and more coherent environment with the rest of MCX portfolio for industrial applications.&lt;/P&gt;
&lt;P&gt;For details on the key differences between the S32K31 and MCX E31 microcontroller families, as well as information regarding software-related aspects, please refer to this application note.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN14792.pdf" target="_blank"&gt;S32K31x to MCX E31x Migration Guidelines&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;BRs,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;BR /&gt;------------------------------------------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 09 Sep 2025 02:44:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXE317MPA/m-p/2165527#M3922</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2025-09-09T02:44:28Z</dc:date>
    </item>
  </channel>
</rss>