<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 Re: Flash Programming Failure with LinkServer when no external memory present</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Flash-Programming-Failure-with-LinkServer-when-no-external/m-p/2161189#M3852</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243115"&gt;@wima88&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;LinkServer&amp;nbsp; will always try to probe and initialize flash interfaces it knows about for the selected target.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;For the MCXN947 EVK, the default configuration includes internal flash at 0x00000000 and external QSPI FlexSPI flash mapped at 0x80000000 / 0x90000000.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;
&lt;P&gt;If the base address of the image is in the 0x0 region, use the internal Flash driver (MCXNxxx. cfx).&lt;/P&gt;
&lt;P&gt;If the base address of the image is in the 0x8000-0000 area, use an external FlexSPI Flash driver (MCXN9xx_SFDPFlexSPI. cfx).&lt;/P&gt;
&lt;P&gt;So your image address is 0x8000000, which won't initialize MCXN9xx_SFDPFlexSPI. cfx.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;
&lt;/DIV&gt;</description>
    <pubDate>Mon, 01 Sep 2025 06:11:15 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2025-09-01T06:11:15Z</dc:date>
    <item>
      <title>Flash Programming Failure with LinkServer when no external memory present</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Flash-Programming-Failure-with-LinkServer-when-no-external/m-p/2160083#M3826</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Processor:&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;MCX N Series - MCXN947&lt;/SPAN&gt;&lt;BR /&gt;&lt;STRONG&gt;Tool:&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;NXP LinkServer (v25.3.31)&lt;/SPAN&gt;&lt;BR /&gt;&lt;STRONG&gt;Debug Probe:&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;MCU-LINK (Firmware: r0C7)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;STRONG&gt;IDE&lt;/STRONG&gt;&amp;nbsp;: VScode with MCUXpresso extension&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;I am unable to flash a binary to MCXN947 evaluation board (MCX-N9XX-EVK) using the NXP LinkServer tool. The operation fails with a critical error and exit code&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;4294967295. The primary error appears to be related to the initialization of external FlexSPI flash drivers, which fails and prevents the entire flash process from completing. The target processor is in secure mode, and I am attempting to program the secure flash region at&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;0x10000000. Since we need to repurpose the QSPI lines&amp;nbsp;&amp;nbsp;&lt;STRONG&gt;The power to the on-board external flash chip has been physically disabled on our EVK by removing a 0-ohm resistor.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;H4&gt;&lt;STRONG&gt;Attempted Troubleshooting&lt;/STRONG&gt;&lt;/H4&gt;&lt;UL&gt;&lt;LI&gt;&lt;P class=""&gt;&lt;STRONG&gt;Root Cause:&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;The LinkServer tool is attempting to auto-detect and initialize all memory interfaces, including the external FlexSPI flash at addresses&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;0x80000000&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;and&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;0x90000000. The required flash driver (MCXN9xx_SFDP_FlexSPI.cfx) is failing its dynamic initialization, which causes the entire programming sequence to abort.&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;&lt;STRONG&gt;This failure is expected and confirms our hardware setup, as we have physically removed power from this flash chip.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;&lt;STRONG&gt;Proof of Concept Successful:&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;&lt;STRONG&gt;We have verified that the internal flash works correctly.&lt;/STRONG&gt;&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;After removing power to the external flash and resetting the board, a previously programmed application runs from the internal flash as expected. This proves our goal is achievable and the issue is solely with the LinkServer tool's workflow.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Check the selected build configuration&lt;/STRONG&gt;&amp;nbsp;for correct board selection to "&lt;STRONG&gt;NXP MCX-N9XX-EVK&lt;/STRONG&gt;" and not the "&lt;STRONG&gt;NXP MCX-N9XX-EVK QSPI&lt;/STRONG&gt;" variant&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;&lt;EM&gt;&lt;STRONG&gt;Given that the external flash is intentionally powered down:&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P class=""&gt;What is the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;correct and working&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;method to completely disable the external FlexSPI flash initialization in the LinkServer command or configuration to avoid this failure?&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 16:43:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Flash-Programming-Failure-with-LinkServer-when-no-external/m-p/2160083#M3826</guid>
      <dc:creator>wima88</dc:creator>
      <dc:date>2025-08-28T16:43:22Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Programming Failure with LinkServer when no external memory present</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Flash-Programming-Failure-with-LinkServer-when-no-external/m-p/2161189#M3852</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243115"&gt;@wima88&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;LinkServer&amp;nbsp; will always try to probe and initialize flash interfaces it knows about for the selected target.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;For the MCXN947 EVK, the default configuration includes internal flash at 0x00000000 and external QSPI FlexSPI flash mapped at 0x80000000 / 0x90000000.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;
&lt;P&gt;If the base address of the image is in the 0x0 region, use the internal Flash driver (MCXNxxx. cfx).&lt;/P&gt;
&lt;P&gt;If the base address of the image is in the 0x8000-0000 area, use an external FlexSPI Flash driver (MCXN9xx_SFDPFlexSPI. cfx).&lt;/P&gt;
&lt;P&gt;So your image address is 0x8000000, which won't initialize MCXN9xx_SFDPFlexSPI. cfx.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Mon, 01 Sep 2025 06:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Flash-Programming-Failure-with-LinkServer-when-no-external/m-p/2161189#M3852</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-09-01T06:11:15Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Programming Failure with LinkServer when no external memory present</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Flash-Programming-Failure-with-LinkServer-when-no-external/m-p/2162544#M3864</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243115"&gt;@wima88&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can change the&amp;nbsp;FRDM-MCXN947.json in file&amp;nbsp;C:\nxp\LinkServer_25.3.31\devices.&lt;/P&gt;
&lt;P&gt;You can copy the JSON of the board and delete the external Flash region.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1756872595024.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/355286iA12358BD65A912E9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1756872595024.png" alt="Harry_Zhang_0-1756872595024.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_1-1756872677955.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/355287iC4850C2E10E4867E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_1-1756872677955.png" alt="Harry_Zhang_1-1756872677955.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Wed, 03 Sep 2025 04:11:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Flash-Programming-Failure-with-LinkServer-when-no-external/m-p/2162544#M3864</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-09-03T04:11:29Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Programming Failure with LinkServer when no external memory present</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Flash-Programming-Failure-with-LinkServer-when-no-external/m-p/2163009#M3870</link>
      <description>&lt;P&gt;Thanks !&amp;nbsp; Changers to the JSON helped&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Sep 2025 15:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Flash-Programming-Failure-with-LinkServer-when-no-external/m-p/2163009#M3870</guid>
      <dc:creator>wima88</dc:creator>
      <dc:date>2025-09-03T15:26:53Z</dc:date>
    </item>
  </channel>
</rss>