<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollersのトピックimx8ulp EVK-HID(W): LIBUSB_ERROR_PIPE (-9)</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/imx8ulp-EVK-HID-W-LIBUSB-ERROR-PIPE-9/m-p/2149035#M3711</link>
    <description>&lt;P&gt;Hi, i am following up the&amp;nbsp;&lt;SPAN&gt;Getting Started with the i.MX 8ULP EVK document. In the part of loading bsp image into board using uuu.exe, i get an error which is&amp;nbsp;HID(W): LIBUSB_ERROR_PIPE (-9) . the commands ı tried to execute are :&amp;nbsp;uuu -b emmc_all imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 and uuu.exe&amp;nbsp;LF_v6.12.20-2.0.0_images_IMX8ULPEVK.zip. In the both execute i get the same error and in the serial port of the linux core, it says:&amp;nbsp;[ERROR] DFI error. Please check DDR configuration. What could be the reason and solution?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 08 Aug 2025 08:21:23 GMT</pubDate>
    <dc:creator>MadKEm</dc:creator>
    <dc:date>2025-08-08T08:21:23Z</dc:date>
    <item>
      <title>imx8ulp EVK-HID(W): LIBUSB_ERROR_PIPE (-9)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/imx8ulp-EVK-HID-W-LIBUSB-ERROR-PIPE-9/m-p/2149035#M3711</link>
      <description>&lt;P&gt;Hi, i am following up the&amp;nbsp;&lt;SPAN&gt;Getting Started with the i.MX 8ULP EVK document. In the part of loading bsp image into board using uuu.exe, i get an error which is&amp;nbsp;HID(W): LIBUSB_ERROR_PIPE (-9) . the commands ı tried to execute are :&amp;nbsp;uuu -b emmc_all imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 and uuu.exe&amp;nbsp;LF_v6.12.20-2.0.0_images_IMX8ULPEVK.zip. In the both execute i get the same error and in the serial port of the linux core, it says:&amp;nbsp;[ERROR] DFI error. Please check DDR configuration. What could be the reason and solution?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Aug 2025 08:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/imx8ulp-EVK-HID-W-LIBUSB-ERROR-PIPE-9/m-p/2149035#M3711</guid>
      <dc:creator>MadKEm</dc:creator>
      <dc:date>2025-08-08T08:21:23Z</dc:date>
    </item>
    <item>
      <title>Re: imx8ulp EVK-HID(W): LIBUSB_ERROR_PIPE (-9)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/imx8ulp-EVK-HID-W-LIBUSB-ERROR-PIPE-9/m-p/2150403#M3728</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253610"&gt;@MadKEm&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you should run the uuu -b emmc &amp;lt;&amp;nbsp;flash.bin&amp;gt;, or uuu -b emmc_all &amp;lt;.wic image&amp;gt;&lt;/P&gt;
&lt;P&gt;please run the uuu -h see the uuu UG.&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 01:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/imx8ulp-EVK-HID-W-LIBUSB-ERROR-PIPE-9/m-p/2150403#M3728</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-08-12T01:49:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx8ulp EVK-HID(W): LIBUSB_ERROR_PIPE (-9)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/imx8ulp-EVK-HID-W-LIBUSB-ERROR-PIPE-9/m-p/2151403#M3741</link>
      <description>&lt;P&gt;Hello&amp;nbsp;@&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202673" target="_self"&gt;&lt;SPAN class=""&gt;pengyong_zhang&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I even tried that but it didn't work. So, after all of this I downloaded Linux and followed the process below:&lt;/P&gt;&lt;P&gt;I downloaded the following packages and binaries to create the standalone image(flash.bin): uboot-imx.git, imx-atf.git, &amp;nbsp;firmware-sentinel-0.10.bin and &amp;nbsp;firmware-upower-1.3.0.bin. I have extracted all the required files from the mentioned packages to create the flash.bin. I used VSCode and imported evk9mimx8ulp_hello_world_cm33 project. I renamed the hello_world.bin to m33_image.bin. Then used imx-mkimage with the following command to generate the flash.bin "make SOC=iMX8ULP REV=A2 flash_singleboot_m33".&amp;nbsp; Then used "uuu -b emmc flash.bin" but after this ı get HID(W):LIBUSB_ERROR_TIMEOUT. In the serial port it prints:&lt;/P&gt;&lt;P&gt;"invalid container image&amp;nbsp;&lt;/P&gt;&lt;P&gt;Download -65712, Total size 0&lt;/P&gt;&lt;P&gt;ROM download failure -65712&lt;/P&gt;&lt;P&gt;Wrong Container, no image foundSPL: failed to boot from all boot devices"&lt;/P&gt;&lt;P&gt;These are the files that I use the generate the .bin file: mx8ulpa2-ahab-container.img, upower_a1.bin (fimware-upower-1.3.0), bl31.bin , u-boot.bin, u-boot-spl.bin and the m33_image.bin. Used command "make imx8ulp_evk_defconfig " to generate the u boot files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Aug 2025 06:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/imx8ulp-EVK-HID-W-LIBUSB-ERROR-PIPE-9/m-p/2151403#M3741</guid>
      <dc:creator>MadKEm</dc:creator>
      <dc:date>2025-08-13T06:37:02Z</dc:date>
    </item>
    <item>
      <title>Re: imx8ulp EVK-HID(W): LIBUSB_ERROR_PIPE (-9)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/imx8ulp-EVK-HID-W-LIBUSB-ERROR-PIPE-9/m-p/2151459#M3743</link>
      <description>&lt;P&gt;I was able to program it currently. The problem was related to the released version of the packages. I downloaded the meta-imx&amp;nbsp;Release - Linux 6.12.20-2.0.0 and extracted all the required files to build the flash image. Then it worked. The "ROM download failure" problem looks like it is related to u boot binaries.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Aug 2025 07:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/imx8ulp-EVK-HID-W-LIBUSB-ERROR-PIPE-9/m-p/2151459#M3743</guid>
      <dc:creator>MadKEm</dc:creator>
      <dc:date>2025-08-13T07:53:02Z</dc:date>
    </item>
  </channel>
</rss>