<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックIMX93 evk Machine name missing in Yocto build configuration</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/IMX93-evk-Machine-name-missing-in-Yocto-build-configuration/m-p/1871814#M370</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i was new to this nxp porting stuff, recently i have ordered the nxp imx93 evk board.&lt;/P&gt;&lt;P&gt;i was trying to setup the build yocto/sdk build env, for the the initial stage in build compilation.&lt;/P&gt;&lt;P&gt;below is the command using for the yocto build config:&lt;/P&gt;&lt;P&gt;DISTRO=&amp;lt;xxxx&amp;gt; MACHINE=&amp;lt;xxxx&amp;gt; source imx-setup-release.sh -b &amp;lt;build-dir&amp;gt;&lt;/P&gt;&lt;P&gt;when i run the "imx-setup-release.sh" file, i could only the below options for imx93 board type&lt;BR /&gt;imx93-11x11-lpddr4x-evk&lt;BR /&gt;imx93-14x14-lpddr4x-evk&lt;BR /&gt;imx93-9x9-lpddr4-qsb&lt;BR /&gt;&lt;BR /&gt;not able to find the imx93-evk machine name.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Naveen&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 23 May 2024 09:15:53 GMT</pubDate>
    <dc:creator>Naveen0507</dc:creator>
    <dc:date>2024-05-23T09:15:53Z</dc:date>
    <item>
      <title>IMX93 evk Machine name missing in Yocto build configuration</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/IMX93-evk-Machine-name-missing-in-Yocto-build-configuration/m-p/1871814#M370</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i was new to this nxp porting stuff, recently i have ordered the nxp imx93 evk board.&lt;/P&gt;&lt;P&gt;i was trying to setup the build yocto/sdk build env, for the the initial stage in build compilation.&lt;/P&gt;&lt;P&gt;below is the command using for the yocto build config:&lt;/P&gt;&lt;P&gt;DISTRO=&amp;lt;xxxx&amp;gt; MACHINE=&amp;lt;xxxx&amp;gt; source imx-setup-release.sh -b &amp;lt;build-dir&amp;gt;&lt;/P&gt;&lt;P&gt;when i run the "imx-setup-release.sh" file, i could only the below options for imx93 board type&lt;BR /&gt;imx93-11x11-lpddr4x-evk&lt;BR /&gt;imx93-14x14-lpddr4x-evk&lt;BR /&gt;imx93-9x9-lpddr4-qsb&lt;BR /&gt;&lt;BR /&gt;not able to find the imx93-evk machine name.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Naveen&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 09:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/IMX93-evk-Machine-name-missing-in-Yocto-build-configuration/m-p/1871814#M370</guid>
      <dc:creator>Naveen0507</dc:creator>
      <dc:date>2024-05-23T09:15:53Z</dc:date>
    </item>
    <item>
      <title>Re: IMX93 evk Machine name missing in Yocto build configuration</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/IMX93-evk-Machine-name-missing-in-Yocto-build-configuration/m-p/1872043#M372</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234010"&gt;@Naveen0507&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can go to directory:&amp;nbsp;~/&amp;lt;yocto build&amp;gt;/sources/meta-imx/meta-imx-bsp/conf/machine&lt;/P&gt;
&lt;P&gt;And there run the command ls.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;$cd ~/&amp;lt;yocto build&amp;gt;/sources/meta-imx/meta-imx-bsp/conf/machine
$ls
&lt;/LI-CODE&gt;
&lt;P&gt;There are located all the arm64 NXP machines, and there is listed the&amp;nbsp;imx93evk.conf.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the machine name should be imx93evk.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this can helps to you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 13:29:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/IMX93-evk-Machine-name-missing-in-Yocto-build-configuration/m-p/1872043#M372</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2024-05-23T13:29:18Z</dc:date>
    </item>
  </channel>
</rss>