<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: Programming On-Chip Flash Memories of 56F80x Devices Using the JTAG/OnCE In</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Programming-On-Chip-Flash-Memories-of-56F80x-Devices-Using-the/m-p/2146754#M3692</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Then, are the MC56F837XX and MC56F847XX series also suitable for this?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;-&amp;gt; Yes, they use the same DSC56800AEX core. And you can also port the code to other platforms with any processor.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1754383367867.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/350953i5803F2B455A0B6CB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_0-1754383367867.png" alt="Celeste_Liu_0-1754383367867.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Celeste_Liu_0-1754383367867.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you. Any new issues, welcome to create new post.&lt;/P&gt;</description>
    <pubDate>Tue, 05 Aug 2025 08:45:14 GMT</pubDate>
    <dc:creator>Celeste_Liu</dc:creator>
    <dc:date>2025-08-05T08:45:14Z</dc:date>
    <item>
      <title>Programming On-Chip Flash Memories of 56F80x Devices Using the JTAG/OnCE In</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Programming-On-Chip-Flash-Memories-of-56F80x-Devices-Using-the/m-p/2145621#M3678</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am currently developing the NXP series MC56F827 series chips and want to program the on-chip FLASH of this chip through the JTAG interface. I found that the example code in the document "Programming On-Chip Flash Memories of 56F80x Devices Using the JTAG/OnCE Interface" only shows a part. I wonder if the official has detailed code examples or SDK packages.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 02 Aug 2025 02:48:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Programming-On-Chip-Flash-Memories-of-56F80x-Devices-Using-the/m-p/2145621#M3678</guid>
      <dc:creator>forcreat</dc:creator>
      <dc:date>2025-08-02T02:48:36Z</dc:date>
    </item>
    <item>
      <title>Re: Programming On-Chip Flash Memories of 56F80x Devices Using the JTAG/OnCE In</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Programming-On-Chip-Flash-Memories-of-56F80x-Devices-Using-the/m-p/2146036#M3682</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253400"&gt;@forcreat&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The 56F82x is an old product that has been around for more than 20 years. For the document "Programming On-Chip Flash Memories of 56F80x Devices Using the JTAG/OnCE Interface", we do not have detailed code examples.&lt;/P&gt;
&lt;P&gt;You may refer to &lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN4981.pdf" target="_blank"&gt;On-Chip Flash Programming of Freescale's MC56F827xx via JTAG Interface&lt;/A&gt;, which includes the corresponding software &lt;A href="https://www.nxp.com/docs/en/application-note-software/AN4981SW.zip" target="_blank"&gt;AN4981SW&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Hope it can help you.&lt;/P&gt;
&lt;P&gt;BRs,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 04 Aug 2025 08:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Programming-On-Chip-Flash-Memories-of-56F80x-Devices-Using-the/m-p/2146036#M3682</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2025-08-04T08:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: Programming On-Chip Flash Memories of 56F80x Devices Using the JTAG/OnCE In</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Programming-On-Chip-Flash-Memories-of-56F80x-Devices-Using-the/m-p/2146704#M3690</link>
      <description>Thank you very much for your effective reply. I saw the corresponding macro definitions and function names in AN4981SW. Then, are the MC56F837XX and MC56F847XX series also suitable for this?</description>
      <pubDate>Tue, 05 Aug 2025 07:50:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Programming-On-Chip-Flash-Memories-of-56F80x-Devices-Using-the/m-p/2146704#M3690</guid>
      <dc:creator>forcreat</dc:creator>
      <dc:date>2025-08-05T07:50:31Z</dc:date>
    </item>
    <item>
      <title>Re: Programming On-Chip Flash Memories of 56F80x Devices Using the JTAG/OnCE In</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Programming-On-Chip-Flash-Memories-of-56F80x-Devices-Using-the/m-p/2146754#M3692</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Then, are the MC56F837XX and MC56F847XX series also suitable for this?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;-&amp;gt; Yes, they use the same DSC56800AEX core. And you can also port the code to other platforms with any processor.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1754383367867.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/350953i5803F2B455A0B6CB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_0-1754383367867.png" alt="Celeste_Liu_0-1754383367867.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Celeste_Liu_0-1754383367867.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you. Any new issues, welcome to create new post.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Aug 2025 08:45:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Programming-On-Chip-Flash-Memories-of-56F80x-Devices-Using-the/m-p/2146754#M3692</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2025-08-05T08:45:14Z</dc:date>
    </item>
  </channel>
</rss>