<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックDriver V.2 dynamic startup failed - driver Init provided no flash parameters</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Driver-V-2-dynamic-startup-failed-driver-Init-provided-no-flash/m-p/2146665#M3689</link>
    <description>&lt;P&gt;MIMXRT1060 - EVK (board - MIMXRT1862DVL6A)&lt;/P&gt;&lt;P&gt;Have configured SW7 as 0010. Connected jumper to J7 and J1(5-6). J42 is not connected by jumper and the board is powered on via J41. We are trying to flash the application but are facing this error while flashing :&lt;BR /&gt;&lt;SPAN&gt;Driver V.2 dynamic startup failed - driver Init provided no flash parameters&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 05 Aug 2025 07:20:46 GMT</pubDate>
    <dc:creator>vrunda165</dc:creator>
    <dc:date>2025-08-05T07:20:46Z</dc:date>
    <item>
      <title>Driver V.2 dynamic startup failed - driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Driver-V-2-dynamic-startup-failed-driver-Init-provided-no-flash/m-p/2146665#M3689</link>
      <description>&lt;P&gt;MIMXRT1060 - EVK (board - MIMXRT1862DVL6A)&lt;/P&gt;&lt;P&gt;Have configured SW7 as 0010. Connected jumper to J7 and J1(5-6). J42 is not connected by jumper and the board is powered on via J41. We are trying to flash the application but are facing this error while flashing :&lt;BR /&gt;&lt;SPAN&gt;Driver V.2 dynamic startup failed - driver Init provided no flash parameters&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Aug 2025 07:20:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Driver-V-2-dynamic-startup-failed-driver-Init-provided-no-flash/m-p/2146665#M3689</guid>
      <dc:creator>vrunda165</dc:creator>
      <dc:date>2025-08-05T07:20:46Z</dc:date>
    </item>
    <item>
      <title>Re: Driver V.2 dynamic startup failed - driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Driver-V-2-dynamic-startup-failed-driver-Init-provided-no-flash/m-p/2146815#M3695</link>
      <description>&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;Please help me try the method mentioned in this thread：&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT-board-recovery-for-debugger-connect-issues/ta-p/1635260" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT-board-recovery-for-debugger-connect-issues/ta-p/1635260&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Tue, 05 Aug 2025 10:20:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Driver-V-2-dynamic-startup-failed-driver-Init-provided-no-flash/m-p/2146815#M3695</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2025-08-05T10:20:51Z</dc:date>
    </item>
  </channel>
</rss>