<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 mcxa153 and LCD Touch screen</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/mcxa153-and-LCD-Touch-screen/m-p/2140336#M3623</link>
    <description>&lt;P&gt;Hi, i have the FRDM MCXA153 , and i would like to know, if there are any examples with this board connected to a LCD TFT TouchScreen via SPI, or something like that. And is it possible to use it with LVGL..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot for your help....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nicolás Marconi&lt;/P&gt;</description>
    <pubDate>Thu, 24 Jul 2025 19:16:33 GMT</pubDate>
    <dc:creator>nicomarconi</dc:creator>
    <dc:date>2025-07-24T19:16:33Z</dc:date>
    <item>
      <title>mcxa153 and LCD Touch screen</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/mcxa153-and-LCD-Touch-screen/m-p/2140336#M3623</link>
      <description>&lt;P&gt;Hi, i have the FRDM MCXA153 , and i would like to know, if there are any examples with this board connected to a LCD TFT TouchScreen via SPI, or something like that. And is it possible to use it with LVGL..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot for your help....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nicolás Marconi&lt;/P&gt;</description>
      <pubDate>Thu, 24 Jul 2025 19:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/mcxa153-and-LCD-Touch-screen/m-p/2140336#M3623</guid>
      <dc:creator>nicomarconi</dc:creator>
      <dc:date>2025-07-24T19:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: mcxa153 and LCD Touch screen</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/mcxa153-and-LCD-Touch-screen/m-p/2140372#M3624</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232797"&gt;@nicomarconi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Unfortunately, we currently do not have any SDK or GUI Guider example codes on how to implement an SPI LCD display on the MCX A153.&lt;/P&gt;
&lt;P&gt;The best alternative would be to use a MCX N example code as base and port it to the MCX A. You can find this example on the SDK, by searching for lvgl examples.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Jul 2025 20:52:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/mcxa153-and-LCD-Touch-screen/m-p/2140372#M3624</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-07-24T20:52:52Z</dc:date>
    </item>
    <item>
      <title>Re: mcxa153 and LCD Touch screen</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/mcxa153-and-LCD-Touch-screen/m-p/2145141#M3672</link>
      <description>I bought the MCXN947 with the LCD-PARALEL-S35 , and I am getting used to it. I think the best way of interfacing a display is parallel. Thanks a lot for the advice you gave me .</description>
      <pubDate>Fri, 01 Aug 2025 10:57:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/mcxa153-and-LCD-Touch-screen/m-p/2145141#M3672</guid>
      <dc:creator>nicomarconi</dc:creator>
      <dc:date>2025-08-01T10:57:52Z</dc:date>
    </item>
  </channel>
</rss>