<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: [imx8qm] usb otg2 configuration</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/imx8qm-usb-otg2-configuration/m-p/1867920#M341</link>
    <description>&lt;P&gt;The i.MX8QM application processor has a specified USB3/USB2 OTG module to perform USB 3.0 dual-&lt;BR /&gt;role and USB 2.0 On-The-Go (OTG) compatible with the USB 3.0 specification. The processor has an&lt;BR /&gt;additional separate, independent USB 2.0 OTG controller which can be used simultaneously with this&lt;BR /&gt;USB 3.0.&lt;/P&gt;
&lt;P&gt;In our reference design we use the USB2 support dual role you can refer to.&lt;/P&gt;</description>
    <pubDate>Fri, 17 May 2024 09:05:26 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2024-05-17T09:05:26Z</dc:date>
    <item>
      <title>[imx8qm] usb otg2 configuration</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/imx8qm-usb-otg2-configuration/m-p/1867685#M338</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm developing it for imx8qm and I'd like to set usbotg2 to peripheral (device) mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I think I need to write "Target Controller Driver", is there a document or file that I can refer to?&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And if anyone knows how to set up a dts file, please let me know. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;(The circuit is designed as follows.)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="hihanna_1-1715923082503.png" style="width: 640px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/279275i67EDA8D58F610EF1/image-dimensions/640x224?v=v2" width="640" height="224" role="button" title="hihanna_1-1715923082503.png" alt="hihanna_1-1715923082503.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 May 2024 05:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/imx8qm-usb-otg2-configuration/m-p/1867685#M338</guid>
      <dc:creator>hihanna</dc:creator>
      <dc:date>2024-05-17T05:20:28Z</dc:date>
    </item>
    <item>
      <title>Re: [imx8qm] usb otg2 configuration</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/imx8qm-usb-otg2-configuration/m-p/1867920#M341</link>
      <description>&lt;P&gt;The i.MX8QM application processor has a specified USB3/USB2 OTG module to perform USB 3.0 dual-&lt;BR /&gt;role and USB 2.0 On-The-Go (OTG) compatible with the USB 3.0 specification. The processor has an&lt;BR /&gt;additional separate, independent USB 2.0 OTG controller which can be used simultaneously with this&lt;BR /&gt;USB 3.0.&lt;/P&gt;
&lt;P&gt;In our reference design we use the USB2 support dual role you can refer to.&lt;/P&gt;</description>
      <pubDate>Fri, 17 May 2024 09:05:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/imx8qm-usb-otg2-configuration/m-p/1867920#M341</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2024-05-17T09:05:26Z</dc:date>
    </item>
  </channel>
</rss>