<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックI need support for MCXN947 Integrated ADC Configuration</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/I-need-support-for-MCXN947-Integrated-ADC-Configuration/m-p/1867293#M336</link>
    <description>&lt;P&gt;I am trying to configure the integrated ADC of the MCXN947 as a differential pair voltage measure device. I had in mind to approach this by changing an example from the standard SDK repository however it uses CMSIS names that I cannot find anywhere. I am using MCUXpresso and the Config Tools but it seems to me that there is a way (maybe an additional program) to accomplish my specific use of the ADC. Can I find such a program somewhere or are there more aiding documents that I can use?&lt;/P&gt;</description>
    <pubDate>Thu, 16 May 2024 15:20:30 GMT</pubDate>
    <dc:creator>Dirk3</dc:creator>
    <dc:date>2024-05-16T15:20:30Z</dc:date>
    <item>
      <title>I need support for MCXN947 Integrated ADC Configuration</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/I-need-support-for-MCXN947-Integrated-ADC-Configuration/m-p/1867293#M336</link>
      <description>&lt;P&gt;I am trying to configure the integrated ADC of the MCXN947 as a differential pair voltage measure device. I had in mind to approach this by changing an example from the standard SDK repository however it uses CMSIS names that I cannot find anywhere. I am using MCUXpresso and the Config Tools but it seems to me that there is a way (maybe an additional program) to accomplish my specific use of the ADC. Can I find such a program somewhere or are there more aiding documents that I can use?&lt;/P&gt;</description>
      <pubDate>Thu, 16 May 2024 15:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/I-need-support-for-MCXN947-Integrated-ADC-Configuration/m-p/1867293#M336</guid>
      <dc:creator>Dirk3</dc:creator>
      <dc:date>2024-05-16T15:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: I need support for MCXN947 Integrated ADC Configuration</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/I-need-support-for-MCXN947-Integrated-ADC-Configuration/m-p/1869146#M352</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;There is no demo for ADC in differential mode, just those that you can find in the SDK. Sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;The only reference is the reference manual and also, such ADC mode is supported in Config Tools.&lt;/P&gt;
&lt;P&gt;Just take into account that the conversion in differential mode is only limited to the pairs that are available as differential channels.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Mon, 20 May 2024 21:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/I-need-support-for-MCXN947-Integrated-ADC-Configuration/m-p/1869146#M352</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-05-20T21:42:11Z</dc:date>
    </item>
  </channel>
</rss>