<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Unused NTC connections MC33775 in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Unused-NTC-connections-MC33775/m-p/2118695#M3205</link>
    <description>&lt;P&gt;Are there any hardware considerations for unused NTC/GPIO connections on the &lt;LI-PRODUCT title="MC33775" id="MC33775"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp; or &lt;LI-PRODUCT title="MC33774" id="MC33774"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;?&lt;/P&gt;&lt;P&gt;I found useful information for using the mentioned chips with less than 14 cell measurements, do unused GPIO pins need to be biased with hardware or just the registers disabled in software?&lt;/P&gt;</description>
    <pubDate>Wed, 18 Jun 2025 16:24:19 GMT</pubDate>
    <dc:creator>bg18</dc:creator>
    <dc:date>2025-06-18T16:24:19Z</dc:date>
    <item>
      <title>Unused NTC connections MC33775</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Unused-NTC-connections-MC33775/m-p/2118695#M3205</link>
      <description>&lt;P&gt;Are there any hardware considerations for unused NTC/GPIO connections on the &lt;LI-PRODUCT title="MC33775" id="MC33775"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp; or &lt;LI-PRODUCT title="MC33774" id="MC33774"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;?&lt;/P&gt;&lt;P&gt;I found useful information for using the mentioned chips with less than 14 cell measurements, do unused GPIO pins need to be biased with hardware or just the registers disabled in software?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 16:24:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Unused-NTC-connections-MC33775/m-p/2118695#M3205</guid>
      <dc:creator>bg18</dc:creator>
      <dc:date>2025-06-18T16:24:19Z</dc:date>
    </item>
    <item>
      <title>Re: Unused NTC connections MC33775</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Unused-NTC-connections-MC33775/m-p/2119026#M3210</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;bg18&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;It's a good practice to either configure the GPIO pin as an input and use a pull-up or pull-down resistor to provide a defined voltage level when the input is not connected, or configure the GPIO pin as an output and set it to a known state.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jun 2025 03:17:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Unused-NTC-connections-MC33775/m-p/2119026#M3210</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2025-06-19T03:17:06Z</dc:date>
    </item>
  </channel>
</rss>