<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM MCXN947 - question about uart pins for MCU-Link and MCXN947 in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-question-about-uart-pins-for-MCU-Link-and-MCXN947/m-p/2117725#M3193</link>
    <description>&lt;P&gt;Hello &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a&amp;nbsp;FRDM MCXN947 dev board. I have read the user manual for it and looked over the schematics.&lt;/P&gt;&lt;P&gt;As I understand, the UART Pins (RX/TX) of the MCU-Link (LPC55S69JEV98) are connected to the pins P1_9 / P1_8 of the target MCU&amp;nbsp;MCXN947&lt;/P&gt;&lt;P&gt;So I thought, when in ISP Mode, I could use that to flash the debugger.&lt;/P&gt;&lt;P&gt;Next, when I looked over the hello world example, the&amp;nbsp;MCXN947&amp;nbsp;P1_9 / P1_8 pins are ALSO used for UART. This time for outputting hello world.&lt;/P&gt;&lt;P&gt;Are those pins used for BOTH debug AND target MCU UART? Or am I wrong that I could use those pins for flashing the debugger?&lt;/P&gt;&lt;P&gt;And if used for both, do I have to switch something before using it for one or the other (maybe in non-isp mode of the debugger those pins are not connected/used on the debugger side)&lt;/P&gt;&lt;P&gt;Would be nice if anyone could shed light on this topic&lt;/P&gt;&lt;P&gt;Regards stejen&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jun 2025 11:23:57 GMT</pubDate>
    <dc:creator>stejen</dc:creator>
    <dc:date>2025-06-17T11:23:57Z</dc:date>
    <item>
      <title>FRDM MCXN947 - question about uart pins for MCU-Link and MCXN947</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-question-about-uart-pins-for-MCU-Link-and-MCXN947/m-p/2117725#M3193</link>
      <description>&lt;P&gt;Hello &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a&amp;nbsp;FRDM MCXN947 dev board. I have read the user manual for it and looked over the schematics.&lt;/P&gt;&lt;P&gt;As I understand, the UART Pins (RX/TX) of the MCU-Link (LPC55S69JEV98) are connected to the pins P1_9 / P1_8 of the target MCU&amp;nbsp;MCXN947&lt;/P&gt;&lt;P&gt;So I thought, when in ISP Mode, I could use that to flash the debugger.&lt;/P&gt;&lt;P&gt;Next, when I looked over the hello world example, the&amp;nbsp;MCXN947&amp;nbsp;P1_9 / P1_8 pins are ALSO used for UART. This time for outputting hello world.&lt;/P&gt;&lt;P&gt;Are those pins used for BOTH debug AND target MCU UART? Or am I wrong that I could use those pins for flashing the debugger?&lt;/P&gt;&lt;P&gt;And if used for both, do I have to switch something before using it for one or the other (maybe in non-isp mode of the debugger those pins are not connected/used on the debugger side)&lt;/P&gt;&lt;P&gt;Would be nice if anyone could shed light on this topic&lt;/P&gt;&lt;P&gt;Regards stejen&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 11:23:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-question-about-uart-pins-for-MCU-Link-and-MCXN947/m-p/2117725#M3193</guid>
      <dc:creator>stejen</dc:creator>
      <dc:date>2025-06-17T11:23:57Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM MCXN947 - question about uart pins for MCU-Link and MCXN947</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-question-about-uart-pins-for-MCU-Link-and-MCXN947/m-p/2120391#M3223</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/251666"&gt;@stejen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regarding&amp;nbsp;&lt;EM&gt;Are those pins used for BOTH debug AND target MCU UART?&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;Yes, you are correct. You do not need to configure anything else for the pins for UART debug and then communication over UART during ISP programming.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if you have any other question.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jun 2025 23:32:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-MCXN947-question-about-uart-pins-for-MCU-Link-and-MCXN947/m-p/2120391#M3223</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2025-06-20T23:32:27Z</dc:date>
    </item>
  </channel>
</rss>