<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB Driver for Windows 10/11 in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1860845#M305</link>
    <description>&lt;P&gt;Thanks for the reply. Unfortunately, many places where this system is used do not allow for that level of administrator access and, as such, the signature enforcement cannot be disabled by the user. Is there a template that can be used to write my own driver? I recently got to the point where I have the ability to sign drivers myself, so if I can create a driver that allows this to work, I can make it a signed driver and allow my customers to use it.&lt;/P&gt;</description>
    <pubDate>Tue, 07 May 2024 22:31:26 GMT</pubDate>
    <dc:creator>mechemike110</dc:creator>
    <dc:date>2024-05-07T22:31:26Z</dc:date>
    <item>
      <title>USB Driver for Windows 10/11</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1851783#M246</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am looking for a Windows driver to enable communication with an NXP MC9S08JM60 microcontroller via the on-chip USB. I currently have a driver that was written for Windows XP that causes the microcontroller to show up as a COM port. Unfortunately this driver is not signed and, as such, cannot be installed on Win10 without jumping through some hoops. Beyond that, many companies don't let their employees have that much control over their workstations, which is why I am asking about whether a driver exists for a more current OS. Is this something that is out there, or would it need to be a custom developed driver?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 17:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1851783#M246</guid>
      <dc:creator>mechemike110</dc:creator>
      <dc:date>2024-04-22T17:09:17Z</dc:date>
    </item>
    <item>
      <title>Re: USB Driver for Windows 10/11</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1857010#M281</link>
      <description>Unfortunately, there is no option for windows 10 and 11.&lt;BR /&gt;&lt;BR /&gt;1.- What I can suggest is to try the next steps:&lt;BR /&gt;2.- Click “Home”，enter “All settings”.&lt;BR /&gt;3.- Access “Update &amp;amp; Security”.&lt;BR /&gt;4.- Find “Recovery”. ...&lt;BR /&gt;5.- After restarting, choose “Troubleshoot”.&lt;BR /&gt;6.- Choose “Advanced options”.&lt;BR /&gt;7.- Choose "Start-up Settings".&lt;BR /&gt;8.- Click “Restart”.&lt;BR /&gt;9.- Enter "F7" to disable driver signature.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.terasic.com.tw/wiki/Disable_Driver_Signature_Enforcement_in_Windows10_x64" target="_blank"&gt;http://www.terasic.com.tw/wiki/Disable_Driver_Signature_Enforcement_in_Windows10_x64&lt;/A&gt;&lt;BR /&gt;</description>
      <pubDate>Mon, 29 Apr 2024 21:18:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1857010#M281</guid>
      <dc:creator>Itzzamna_Supp</dc:creator>
      <dc:date>2024-04-29T21:18:20Z</dc:date>
    </item>
    <item>
      <title>Re: USB Driver for Windows 10/11</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1860845#M305</link>
      <description>&lt;P&gt;Thanks for the reply. Unfortunately, many places where this system is used do not allow for that level of administrator access and, as such, the signature enforcement cannot be disabled by the user. Is there a template that can be used to write my own driver? I recently got to the point where I have the ability to sign drivers myself, so if I can create a driver that allows this to work, I can make it a signed driver and allow my customers to use it.&lt;/P&gt;</description>
      <pubDate>Tue, 07 May 2024 22:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1860845#M305</guid>
      <dc:creator>mechemike110</dc:creator>
      <dc:date>2024-05-07T22:31:26Z</dc:date>
    </item>
    <item>
      <title>Re: USB Driver for Windows 10/11</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1861750#M310</link>
      <description>&lt;P&gt;After some additional research I came across &lt;A href="https://learn.microsoft.com/en-us/windows-hardware/drivers/usbcon/usb-driver-installation-based-on-compatible-ids" target="_self"&gt;this site&lt;/A&gt; which, I think, provides a different way of fixing this issue. If I am understanding it correctly, if the device class and subclass codes are set to 02 (class code 02 = CDC device, subclass code 02 = abstract control model), then Windows 10 and 11 will automatically load usbser.sys (built into Win10 and 11) as the device driver.&lt;/P&gt;&lt;P&gt;Currently, the device I'm trying to talk to shows up in the task manager as "Unknown USB Device (Device Descriptor Request Failed)". When I right-click and select "Properties", under the details tab, it shows the class as "USB", which I believe would correlate to class code 00.&lt;/P&gt;&lt;P&gt;My new question is - how does one go about setting the device class &amp;amp; subclass? Is that defined by register values on the MCU, or is it accomplished in the C code that is written for the MCU?&lt;/P&gt;</description>
      <pubDate>Wed, 08 May 2024 19:27:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1861750#M310</guid>
      <dc:creator>mechemike110</dc:creator>
      <dc:date>2024-05-08T19:27:24Z</dc:date>
    </item>
    <item>
      <title>Re: USB Driver for Windows 10/11</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1864647#M322</link>
      <description>&lt;P&gt;Unfortunately, there is no template available from our side to help in this request. Sorry for the inconvenience.&lt;BR /&gt;&lt;BR /&gt;For this specific request, I recommend contacting PE micro support to verify if it happens that they have any template or driver that may help you for this USB inquiry at &lt;A href="https://www.pemicro.com/" target="_blank"&gt;https://www.pemicro.com/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your understanding&lt;/P&gt;</description>
      <pubDate>Mon, 13 May 2024 17:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/USB-Driver-for-Windows-10-11/m-p/1864647#M322</guid>
      <dc:creator>Itzzamna_Supp</dc:creator>
      <dc:date>2024-05-13T17:27:33Z</dc:date>
    </item>
  </channel>
</rss>