<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: LowPower Mode(lpidle)</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/LowPower-Mode-lpidle/m-p/2089667#M2965</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205915"&gt;@OneByte&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you share your code to see if there is any issue? What USB device are you using? How could I replicate the issue using our EVK? Have you tested any other low power modes?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 29 Apr 2025 20:57:58 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2025-04-29T20:57:58Z</dc:date>
    <item>
      <title>LowPower Mode(lpidle)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/LowPower-Mode-lpidle/m-p/2071689#M2829</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; When developing low-power functionality using the RT1052, after the system triggers low-power mode (lpIdle) and wakes up from lpIdle to overrun mode, a specific anomaly is observed during testing: If the module connected to the USB host is active, uSDHC access to eMMC becomes abnormal; if the module on the USB host is inactive, uSDHC can access eMMC normally. How can this issue be troubleshooted?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;#rt1052&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Apr 2025 06:10:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/LowPower-Mode-lpidle/m-p/2071689#M2829</guid>
      <dc:creator>OneByte</dc:creator>
      <dc:date>2025-04-01T06:10:09Z</dc:date>
    </item>
    <item>
      <title>Re: LowPower Mode(lpidle)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/LowPower-Mode-lpidle/m-p/2073127#M2841</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205915"&gt;@OneByte&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you please elaborate when you mean that the "&lt;SPAN&gt;uSDHC access to eMMC becomes abnormal&lt;/SPAN&gt;"? How is the USB host configured? What about the uSDHC? Does this also happen when transitioning between other power modes?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Apr 2025 19:35:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/LowPower-Mode-lpidle/m-p/2073127#M2841</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-04-02T19:35:23Z</dc:date>
    </item>
    <item>
      <title>Re: LowPower Mode(lpidle)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/LowPower-Mode-lpidle/m-p/2081615#M2889</link>
      <description>When powered on normally, there are no issues. It can be understood that the USB is configured as a host, connected to a module (acting as a device). After entering LP idle mode and then waking up into overrun mode:&lt;BR /&gt;&lt;BR /&gt;If the module connected to the USB host is not powered, normal read/write access to eMMC is possible.&lt;BR /&gt;&lt;BR /&gt;If the module connected via the USB interface is powered, normal read/write access to eMMC becomes unavailable.&lt;BR /&gt;Other low-power modes (LP modes) have not been tested."</description>
      <pubDate>Wed, 16 Apr 2025 09:18:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/LowPower-Mode-lpidle/m-p/2081615#M2889</guid>
      <dc:creator>OneByte</dc:creator>
      <dc:date>2025-04-16T09:18:45Z</dc:date>
    </item>
    <item>
      <title>Re: LowPower Mode(lpidle)</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/LowPower-Mode-lpidle/m-p/2089667#M2965</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205915"&gt;@OneByte&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you share your code to see if there is any issue? What USB device are you using? How could I replicate the issue using our EVK? Have you tested any other low power modes?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 20:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/LowPower-Mode-lpidle/m-p/2089667#M2965</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-04-29T20:57:58Z</dc:date>
    </item>
  </channel>
</rss>