<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ISP MODE NOT WORKING BY DEFAULT WITH FRDM-MCXC444 PROJECTS in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2077563#M2862</link>
    <description>Hi Diego,&lt;BR /&gt;&lt;BR /&gt;Thank you for the information and remembering my question. I will try this new software asap!</description>
    <pubDate>Wed, 09 Apr 2025 20:55:07 GMT</pubDate>
    <dc:creator>gvellet</dc:creator>
    <dc:date>2025-04-09T20:55:07Z</dc:date>
    <item>
      <title>ISP MODE NOT WORKING BY DEFAULT WITH FRDM-MCXC444 PROJECTS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2068905#M2811</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;With SDK example projects or new projects created from scratch, the ISP mode is not working when a valid application is in Flash.&lt;/P&gt;&lt;P&gt;I have traced the problem to the file startup/startup_mcxc444.c. At line 53, the struct&amp;nbsp; "Flash_config[3]" is set to value 0xFFFF3FFE. The byte value 0x3F correspond to the FOPT (Flash option register) where bit 1 (BOOTPIN_OPT) = 1. This setting disable the ISP_MODE pin 26.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have changed the byte value to 0x3D. Now when I press Reset and ISP_MODE together, the MCXC444 enters ISP mode every time.&lt;/P&gt;&lt;P&gt;My question is about MCUXpresso. I don't think it is a good practice to manually edit "startup_mcxc444.c", is there a project settings to customize the&amp;nbsp;Flash_config value in "startup_mcxc444.c"?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Mar 2025 18:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2068905#M2811</guid>
      <dc:creator>gvellet</dc:creator>
      <dc:date>2025-03-26T18:04:59Z</dc:date>
    </item>
    <item>
      <title>Re: ISP MODE NOT WORKING BY DEFAULT WITH FRDM-MCXC444 PROJECTS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2069791#M2815</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191227"&gt;@gvellet&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your interest and for sharing the solution to the problem you encountered.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I confirm that there&amp;nbsp; are no project options, to avoid manually&amp;nbsp;customizing the&amp;nbsp;&lt;SPAN&gt;Flash_config&amp;nbsp;structure, available in MCUXpresso IDE.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Diego&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Mar 2025 22:11:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2069791#M2815</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2025-03-27T22:11:52Z</dc:date>
    </item>
    <item>
      <title>Re: ISP MODE NOT WORKING BY DEFAULT WITH FRDM-MCXC444 PROJECTS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2077384#M2861</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191227"&gt;@gvellet&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I just want to follow up our thread with the below information!&lt;/P&gt;
&lt;P&gt;We just released MCUXpresso Secure Provisioning Tool v25. I believe the tool provides security settings for the MCX C that you could find really useful. Below an ilustrative image, where I changed the MCU Life cycle from Unsecure to Flash secure.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diego_charles_0-1744219929454.png" style="width: 726px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/332332iAE14CAE24381CEF3/image-dimensions/726x385?v=v2" width="726" height="385" role="button" title="diego_charles_0-1744219929454.png" alt="diego_charles_0-1744219929454.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;As you can see in the BCA/FCF settings,&amp;nbsp; the FSEC setting&amp;nbsp; enabled according to Flash secured life cycle.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The SPT, for short. creates bootable and secure images, you can provide a sample image for the MCX C or your custom image. The tool requires connection to the MCU over USB/UART.&lt;/P&gt;
&lt;P&gt;For more details about the SPT use, please refer to sections:&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;6.10 MCX C041/C242/C444 device workflow&lt;/EM&gt;&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;6.10.3.3 Life cycle for MCX C041/C242/C444 devices&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;of the&amp;nbsp;MCUXSPTUG , you can get it easily by doing this:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diego_charles_1-1744221155917.png" style="width: 528px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/332334i1AF04CBBB60A98E1/image-dimensions/528x168?v=v2" width="528" height="168" role="button" title="diego_charles_1-1744221155917.png" alt="diego_charles_1-1744221155917.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We can conclude that you can manually edit flash security settings for the MCU using the MCUXpresso IDE, however, we leveraged this to the MCUXpresso Secure Provisioining Tool&lt;/P&gt;
&lt;P&gt;hope this helps you,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
      <pubDate>Wed, 09 Apr 2025 17:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2077384#M2861</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2025-04-09T17:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: ISP MODE NOT WORKING BY DEFAULT WITH FRDM-MCXC444 PROJECTS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2077563#M2862</link>
      <description>Hi Diego,&lt;BR /&gt;&lt;BR /&gt;Thank you for the information and remembering my question. I will try this new software asap!</description>
      <pubDate>Wed, 09 Apr 2025 20:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2077563#M2862</guid>
      <dc:creator>gvellet</dc:creator>
      <dc:date>2025-04-09T20:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: ISP MODE NOT WORKING BY DEFAULT WITH FRDM-MCXC444 PROJECTS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2077615#M2863</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191227"&gt;@gvellet&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;My pleasure, we just release it yersterday,&amp;nbsp; please give it a try! Feel free to create another post, if you get any questions or feedback regarding the SPT. The MCX C support was just introduced.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;All the best,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
      <pubDate>Wed, 09 Apr 2025 21:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/ISP-MODE-NOT-WORKING-BY-DEFAULT-WITH-FRDM-MCXC444-PROJECTS/m-p/2077615#M2863</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2025-04-09T21:30:50Z</dc:date>
    </item>
  </channel>
</rss>