<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 Re: Upgrade imx6ull with linux kernel 4.5.2 or grater.</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Upgrade-imx6ull-with-linux-kernel-4-5-2-or-grater/m-p/2046236#M2498</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;From the link shared above, we could see that the kernel 4.19.325 is available. Also we could download it and see that the complete rootfs is available.&lt;/P&gt;&lt;P&gt;But the point for us different. We are looking for the kernel 4.19.325 along with the privilege to build it with the oldconfig changes and load it on the device.&lt;/P&gt;&lt;P&gt;Could we get any kernel packages alone to be build with the oldconfig (.config from the old kernel) and load/install the kernel on the device.&lt;/P&gt;&lt;P&gt;Please suggest.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Satya.&lt;/P&gt;</description>
    <pubDate>Tue, 18 Feb 2025 09:42:59 GMT</pubDate>
    <dc:creator>satya_62</dc:creator>
    <dc:date>2025-02-18T09:42:59Z</dc:date>
    <item>
      <title>Upgrade imx6ull with linux kernel 4.5.2 or grater.</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Upgrade-imx6ull-with-linux-kernel-4-5-2-or-grater/m-p/2039929#M2443</link>
      <description>&lt;P&gt;We have a product with imx6ull in the market for around 8 years. It went into market with kernel 4.1.15(built using rocko branch Yocto). Can we upgrade the kernel version in the device? please suggest us for the kernel &amp;gt; 4.5.2 as the Yocto branch is now EOL.&lt;/P&gt;&lt;P&gt;When the last build was made (may be during 2017) using Yocto - Rocko branch setup, a image was created and successfully booted on the imx6ull device.&lt;/P&gt;&lt;P&gt;It went on with the same kernel and frequent updates w.r.t application.&lt;/P&gt;&lt;P&gt;Now the ask is to upgrade to a kernel version which should be grater than 4.5.2. We are clear that the yocto branch is EOL. so cannot proceed over this method.&lt;/P&gt;&lt;P&gt;Can the kernel with 4.5.(&amp;gt;2) be applied on the same device; consider the kernel is build from ubuntu PC and copied here.&lt;/P&gt;&lt;P&gt;Please suggest the better way to do it.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 11:22:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Upgrade-imx6ull-with-linux-kernel-4-5-2-or-grater/m-p/2039929#M2443</guid>
      <dc:creator>satya_62</dc:creator>
      <dc:date>2025-02-07T11:22:32Z</dc:date>
    </item>
    <item>
      <title>Re: Upgrade imx6ull with linux kernel 4.5.2 or grater.</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Upgrade-imx6ull-with-linux-kernel-4-5-2-or-grater/m-p/2040943#M2456</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, you can migrate to your desire kernel version but I suggest the one used by NXP:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Feb 2025 13:57:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Upgrade-imx6ull-with-linux-kernel-4-5-2-or-grater/m-p/2040943#M2456</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-02-10T13:57:13Z</dc:date>
    </item>
    <item>
      <title>Re: Upgrade imx6ull with linux kernel 4.5.2 or grater.</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Upgrade-imx6ull-with-linux-kernel-4-5-2-or-grater/m-p/2046236#M2498</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;From the link shared above, we could see that the kernel 4.19.325 is available. Also we could download it and see that the complete rootfs is available.&lt;/P&gt;&lt;P&gt;But the point for us different. We are looking for the kernel 4.19.325 along with the privilege to build it with the oldconfig changes and load it on the device.&lt;/P&gt;&lt;P&gt;Could we get any kernel packages alone to be build with the oldconfig (.config from the old kernel) and load/install the kernel on the device.&lt;/P&gt;&lt;P&gt;Please suggest.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Satya.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Feb 2025 09:42:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Upgrade-imx6ull-with-linux-kernel-4-5-2-or-grater/m-p/2046236#M2498</guid>
      <dc:creator>satya_62</dc:creator>
      <dc:date>2025-02-18T09:42:59Z</dc:date>
    </item>
  </channel>
</rss>