<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: Inquiries about the use of MCIMX6L3EVN10AB / RTC module</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Inquiries-about-the-use-of-MCIMX6L3EVN10AB-RTC-module/m-p/2042968#M2469</link>
    <description>&lt;P&gt;Thank you for your reply&lt;/P&gt;&lt;P&gt;I have one more question.&lt;BR /&gt;The data sheet says that if It don't use an external crystal as shown below, use a ring oscillator.&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;"If no external crystal is present, then the ring oscillator is utilized"&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;As you said, if I set up RTC_XTALI, XTALO PIN, could it crash with the RTC module (36.768Khz) due to ring oscillator operation, causing boot problems or other problems? Or would it have no impact at all?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 13 Feb 2025 01:46:46 GMT</pubDate>
    <dc:creator>chung810</dc:creator>
    <dc:date>2025-02-13T01:46:46Z</dc:date>
    <item>
      <title>Inquiries about the use of MCIMX6L3EVN10AB / RTC module</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Inquiries-about-the-use-of-MCIMX6L3EVN10AB-RTC-module/m-p/2042559#M2467</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello, I'm Chung.&lt;BR /&gt;I use MCIMX6L3EVN10AB&amp;nbsp; now.&lt;/P&gt;&lt;P&gt;For save the current consumption, we don't use external crystals(32.768khz)&lt;BR /&gt;I want to use "RTC Module" (32.768Khz) through I2C.&lt;/P&gt;&lt;P&gt;How should I handle RTC_XTALI, RTC_XTALO PIN at this time?&lt;BR /&gt;GND? Or floating? NC?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Please check. Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Feb 2025 11:00:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Inquiries-about-the-use-of-MCIMX6L3EVN10AB-RTC-module/m-p/2042559#M2467</guid>
      <dc:creator>chung810</dc:creator>
      <dc:date>2025-02-12T11:00:32Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiries about the use of MCIMX6L3EVN10AB / RTC module</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Inquiries-about-the-use-of-MCIMX6L3EVN10AB-RTC-module/m-p/2042800#M2468</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;RTC_XTALI should be connected to ground.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;RTC_XTALO should be left floating.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Feb 2025 18:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Inquiries-about-the-use-of-MCIMX6L3EVN10AB-RTC-module/m-p/2042800#M2468</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-02-12T18:32:20Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiries about the use of MCIMX6L3EVN10AB / RTC module</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Inquiries-about-the-use-of-MCIMX6L3EVN10AB-RTC-module/m-p/2042968#M2469</link>
      <description>&lt;P&gt;Thank you for your reply&lt;/P&gt;&lt;P&gt;I have one more question.&lt;BR /&gt;The data sheet says that if It don't use an external crystal as shown below, use a ring oscillator.&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;"If no external crystal is present, then the ring oscillator is utilized"&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;As you said, if I set up RTC_XTALI, XTALO PIN, could it crash with the RTC module (36.768Khz) due to ring oscillator operation, causing boot problems or other problems? Or would it have no impact at all?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Feb 2025 01:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Inquiries-about-the-use-of-MCIMX6L3EVN10AB-RTC-module/m-p/2042968#M2469</guid>
      <dc:creator>chung810</dc:creator>
      <dc:date>2025-02-13T01:46:46Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiries about the use of MCIMX6L3EVN10AB / RTC module</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Inquiries-about-the-use-of-MCIMX6L3EVN10AB-RTC-module/m-p/2043552#M2479</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It will not impact the design.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Feb 2025 15:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Inquiries-about-the-use-of-MCIMX6L3EVN10AB-RTC-module/m-p/2043552#M2479</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-02-13T15:57:11Z</dc:date>
    </item>
  </channel>
</rss>