<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックSDIO driver SDK of IMX8MMini Cortex-M4</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/SDIO-driver-SDK-of-IMX8MMini-Cortex-M4/m-p/2039758#M2442</link>
    <description>&lt;P&gt;We are trying to use i.MX8MMini(Cortex-A53/-M4) and thinking about getting implement Wireless Module(SDIO I/F) in the Cortex-M4 Co-processor.&lt;BR /&gt;Regarding Freertos on the Cortex-M4, we got information from the NXP forum and are working on building an environment for the RTOS&lt;BR /&gt;We noticed that when we was porting the wireless driver after the build was complete.&lt;BR /&gt;The current source code for the RTOS does not include an SDIO driver.&lt;BR /&gt;Is SDIO not supported on the Cortex-M4 in the i.MX8MMini?&lt;BR /&gt;If it is supported, can you provide an SDIO driver for the Cortex-M4.&lt;/P&gt;</description>
    <pubDate>Fri, 07 Feb 2025 07:29:15 GMT</pubDate>
    <dc:creator>keisuke</dc:creator>
    <dc:date>2025-02-07T07:29:15Z</dc:date>
    <item>
      <title>SDIO driver SDK of IMX8MMini Cortex-M4</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/SDIO-driver-SDK-of-IMX8MMini-Cortex-M4/m-p/2039758#M2442</link>
      <description>&lt;P&gt;We are trying to use i.MX8MMini(Cortex-A53/-M4) and thinking about getting implement Wireless Module(SDIO I/F) in the Cortex-M4 Co-processor.&lt;BR /&gt;Regarding Freertos on the Cortex-M4, we got information from the NXP forum and are working on building an environment for the RTOS&lt;BR /&gt;We noticed that when we was porting the wireless driver after the build was complete.&lt;BR /&gt;The current source code for the RTOS does not include an SDIO driver.&lt;BR /&gt;Is SDIO not supported on the Cortex-M4 in the i.MX8MMini?&lt;BR /&gt;If it is supported, can you provide an SDIO driver for the Cortex-M4.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 07:29:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/SDIO-driver-SDK-of-IMX8MMini-Cortex-M4/m-p/2039758#M2442</guid>
      <dc:creator>keisuke</dc:creator>
      <dc:date>2025-02-07T07:29:15Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO driver SDK of IMX8MMini Cortex-M4</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/SDIO-driver-SDK-of-IMX8MMini-Cortex-M4/m-p/2047784#M2516</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203263"&gt;@keisuke&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thank you for your query.&lt;/P&gt;
&lt;P&gt;Unfortunately,&amp;nbsp;our M4 SDK doesn't support SDIO driver.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Feb 2025 04:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/SDIO-driver-SDK-of-IMX8MMini-Cortex-M4/m-p/2047784#M2516</guid>
      <dc:creator>yutaka_ando</dc:creator>
      <dc:date>2025-02-20T04:50:16Z</dc:date>
    </item>
  </channel>
</rss>