<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: Freemaster Communication with Labview</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Freemaster-Communication-with-Labview/m-p/2038355#M2430</link>
    <description>&lt;P&gt;Hi mich28，&lt;/P&gt;
&lt;P&gt;Freemaster is NXP's system debug tool and it doesn't have the feature of directly supporting Labview communication.&lt;BR /&gt;There may be some indirect methods. For example, Freemaster can transfer MCU data to LabView via UART. But we don't have demo on this becuase LabView is not NXP prodcut.&lt;/P&gt;
&lt;P&gt;Let's leave your question here, if other users have experiences about it, welcome to share.&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
    <pubDate>Wed, 05 Feb 2025 07:44:46 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2025-02-05T07:44:46Z</dc:date>
    <item>
      <title>Freemaster Communication with Labview</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Freemaster-Communication-with-Labview/m-p/2037762#M2426</link>
      <description>&lt;P&gt;Hello Community, I implemented and used the "mcbcom.dll" library with python 3.9 64 bit and now I can use it. Out of necessity I start using the same library with the "Call Library Function" on Labview 32bit 2015 but I continue to receive errors. I was wondering if anyone has already used this library and if this library is really 32bit as written in many forums, I tried to use it with python 3.13 32 bit and it doesn't work....has anyone had the same problem?&lt;/P&gt;&lt;P&gt;MCU:&amp;nbsp; &amp;nbsp; &amp;nbsp;LPC5536JBD100&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 15:17:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Freemaster-Communication-with-Labview/m-p/2037762#M2426</guid>
      <dc:creator>mich28</dc:creator>
      <dc:date>2025-02-04T15:17:51Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster Communication with Labview</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Freemaster-Communication-with-Labview/m-p/2038355#M2430</link>
      <description>&lt;P&gt;Hi mich28，&lt;/P&gt;
&lt;P&gt;Freemaster is NXP's system debug tool and it doesn't have the feature of directly supporting Labview communication.&lt;BR /&gt;There may be some indirect methods. For example, Freemaster can transfer MCU data to LabView via UART. But we don't have demo on this becuase LabView is not NXP prodcut.&lt;/P&gt;
&lt;P&gt;Let's leave your question here, if other users have experiences about it, welcome to share.&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Wed, 05 Feb 2025 07:44:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Freemaster-Communication-with-Labview/m-p/2038355#M2430</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2025-02-05T07:44:46Z</dc:date>
    </item>
  </channel>
</rss>