<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: MCXC444, SDMMC, and FatFS</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXC444-SDMMC-and-FatFS/m-p/2029702#M2365</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184079"&gt;@aaronm&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Although there is an sdmmc library in the middleware of the SDK, the MCXC444 does not support SDIO. As a result, there is neither an SD card example nor FatFS under the SDK.&lt;BR /&gt;If you need to use an SD card on the MCXC444, you can only implement it through the SPI interface.&lt;/P&gt;
&lt;P&gt;I recommend you to read the following documents in order to implement FatFs using SPI.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Porting-FatFs-file-system-to-KL26-SPI-SD-card-code/ta-p/1111095" target="_blank"&gt;Porting FatFs file system to KL26 SPI SD card code - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN10406.pdf?_gl=1*1yplqy3*_ga*NzI3NTQzNzk4LjE3MjIzMTk5NzY.*_ga_WM5LE0KMSH*MTczNzEwOTMwMy41MTYuMS4xNzM3MTA5NDkzLjAuMC4w" target="_blank"&gt;AN10406 Accessing SD/MMC card using SPI on LPC2000&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you.&lt;/P&gt;
&lt;P&gt;BRs,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;------------------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 17 Jan 2025 10:29:37 GMT</pubDate>
    <dc:creator>Celeste_Liu</dc:creator>
    <dc:date>2025-01-17T10:29:37Z</dc:date>
    <item>
      <title>MCXC444, SDMMC, and FatFS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXC444-SDMMC-and-FatFS/m-p/2029329#M2363</link>
      <description>&lt;P&gt;I have the SDK for the MCXC444 - 24.12.00 - and I see that it includes SDMMC stack support, but there's no FatFS support included. &amp;nbsp;Does that mean that the 444 does NOT support FatFS, even though SDMMC is inherently included? &amp;nbsp;Or are we expected to download the FatFS driver from Chan's site for each project that needs it?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 23:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXC444-SDMMC-and-FatFS/m-p/2029329#M2363</guid>
      <dc:creator>aaronm</dc:creator>
      <dc:date>2025-01-16T23:03:30Z</dc:date>
    </item>
    <item>
      <title>Re: MCXC444, SDMMC, and FatFS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXC444-SDMMC-and-FatFS/m-p/2029702#M2365</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184079"&gt;@aaronm&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Although there is an sdmmc library in the middleware of the SDK, the MCXC444 does not support SDIO. As a result, there is neither an SD card example nor FatFS under the SDK.&lt;BR /&gt;If you need to use an SD card on the MCXC444, you can only implement it through the SPI interface.&lt;/P&gt;
&lt;P&gt;I recommend you to read the following documents in order to implement FatFs using SPI.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Porting-FatFs-file-system-to-KL26-SPI-SD-card-code/ta-p/1111095" target="_blank"&gt;Porting FatFs file system to KL26 SPI SD card code - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN10406.pdf?_gl=1*1yplqy3*_ga*NzI3NTQzNzk4LjE3MjIzMTk5NzY.*_ga_WM5LE0KMSH*MTczNzEwOTMwMy41MTYuMS4xNzM3MTA5NDkzLjAuMC4w" target="_blank"&gt;AN10406 Accessing SD/MMC card using SPI on LPC2000&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you.&lt;/P&gt;
&lt;P&gt;BRs,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;------------------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jan 2025 10:29:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXC444-SDMMC-and-FatFS/m-p/2029702#M2365</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2025-01-17T10:29:37Z</dc:date>
    </item>
  </channel>
</rss>