<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCUXpresso + FRDM-MCXN947: Failed to import project from Application Code Hub in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCUXpresso-FRDM-MCXN947-Failed-to-import-project-from/m-p/2017582#M2217</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243125"&gt;@wycox&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for providing the information. We will resolve this issue as soon as possible.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
    <pubDate>Fri, 20 Dec 2024 03:23:04 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2024-12-20T03:23:04Z</dc:date>
    <item>
      <title>MCUXpresso + FRDM-MCXN947: Failed to import project from Application Code Hub</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCUXpresso-FRDM-MCXN947-Failed-to-import-project-from/m-p/2017132#M2214</link>
      <description>&lt;P&gt;Hi, I tried for many times to import eIQ project from Application Code Hub, and failed with an error msg " Currently selected project is not supported by MCUXpresso IDE", as shown in the upper left corner of the attached screen shot. However I do can import the project with the same name from installed SDK package. What could be the reason for this problem? Thanks for help.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="FailImportPrjFromACH.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/316698iFD5CC89994A67F2A/image-size/large?v=v2&amp;amp;px=999" role="button" title="FailImportPrjFromACH.png" alt="FailImportPrjFromACH.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Dec 2024 10:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCUXpresso-FRDM-MCXN947-Failed-to-import-project-from/m-p/2017132#M2214</guid>
      <dc:creator>wycox</dc:creator>
      <dc:date>2024-12-19T10:00:37Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso + FRDM-MCXN947: Failed to import project from Application Code Hub</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCUXpresso-FRDM-MCXN947-Failed-to-import-project-from/m-p/2017582#M2217</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243125"&gt;@wycox&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for providing the information. We will resolve this issue as soon as possible.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Fri, 20 Dec 2024 03:23:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCUXpresso-FRDM-MCXN947-Failed-to-import-project-from/m-p/2017582#M2217</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-12-20T03:23:04Z</dc:date>
    </item>
  </channel>
</rss>