<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013587#M2187</link>
    <description>&lt;P&gt;Another update.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I built a binary and skipped the validation (L2, the one causing the error). The board flashes BUT, it still doesn't run properly.&lt;/P&gt;&lt;P&gt;So, I downloaded (through Jlink save bbin command) the flashed program inside the rw612. It matches the one I tried to flash sniping the verification. So, my guess now is that the Bootloader (boot ROM) is pointing to the secure area (0x1800_0000) instead of pointing to the non-secure area (0x0800_0000). This guess gains traction with the fact the the default zephyr configuration has the following options:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;CONFIG_ARM_MPU=y
CONFIG_HW_STACK_PROTECTION=y
CONFIG_TRUSTED_EXECUTION_SECURE=y&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 13 Dec 2024 12:00:53 GMT</pubDate>
    <dc:creator>nguterresn</dc:creator>
    <dc:date>2024-12-13T12:00:53Z</dc:date>
    <item>
      <title>FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2012840#M2172</link>
      <description>&lt;P&gt;Hey!&lt;/P&gt;&lt;P&gt;I've been trying to make the FRDM RW612 work. I was able to flash for a couple of times, until I've connected the Adafruit TFT 2.8 LCD screen on top of the Arduino Header presented in the board, and, after that, I was able to flash a few more times until something went wrong and I couldn't anymore.&lt;/P&gt;&lt;P&gt;I've tried everything at this points:&lt;/P&gt;&lt;P&gt;- Downloaded MCUExpresso, created a default build for the board and tried to flash: failed.&lt;/P&gt;&lt;P&gt;- Downloaded the LinkServer, change from JLink probe to CMSIS, tried to flash: failed.&lt;/P&gt;&lt;P&gt;- Played around with JLink console: I can read and write onto specific addresses, but I can't flash.&lt;/P&gt;&lt;P&gt;I've tried different builds, NXP examples and Zephyr samples (Blinky): does't work.&lt;/P&gt;&lt;P&gt;Here's an example of error message from JLink:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;loadfile /Users/nunoguterres/Downloads/zephyr.elf 0x18000000
'loadfile': Performing implicit reset &amp;amp; halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 113ms
Downloading file [/Users/nunoguterres/Downloads/zephyr.elf]...
J-Link: Flash download: Bank 1 @ 0x18000000: 1 range affected (65536 bytes)
J-Link: Flash download: Total: 0.648s (Prepare: 0.165s, Compare: 0.150s, Erase: 0.004s, Program: 0.145s, Verify: 0.107s, Restore: 0.075s)
J-Link: Flash download: Program speed: 440 KB/s

****** Error: Verification failed @ address 0x18000000
Error while programming flash: Verify failed.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And here is the example of a connection to JLink:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;JLinkExe -Device RW612 -speed 4000 -if swd
SEGGER J-Link Commander V8.10 (Compiled Sep 25 2024 14:15:06)
DLL version V8.10, compiled Sep 25 2024 14:14:53

Connecting to J-Link via USB...O.K.
Firmware: J-Link MCU-Link V1 compiled Sep 24 2024 10:57:33
Hardware version: V1.00
J-Link uptime (since boot): 0d 00h 22m 48s
S/N: 1066319194
USB speed mode: High speed (480 MBit/s)
VTref=3.300V


Type "connect" to establish a target connection, '?' for help
J-Link&amp;gt;connect
Device "RW612" selected.


Connecting to target via SWD
InitTarget() start
SWD selected. Executing JTAG -&amp;gt; SWD switching sequence.
DAP initialized successfully.
  DMAP_REG_ID: DM-AP IDCODE detected: 0x002A0000
  DHCSR: 0x05100000
InitTarget() end - Took 2.71ms
Found SW-DP with ID 0x6BA02477
DPIDR: 0x6BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)
Feature set: Mainline
Cache: No cache
Found Cortex-M33 r0p4, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
Security extension: implemented
Secure debug: enabled
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105900D PID 000BBD21 DEVARCH 47702A04 DEVTYPE 00 Cortex-M33
[0][1]: E0001000 CID B105900D PID 000BBD21 DEVARCH 47701A02 DEVTYPE 00 DWT
[0][2]: E0002000 CID B105900D PID 000BBD21 DEVARCH 47701A03 DEVTYPE 00 FPB
[0][3]: E0000000 CID B105900D PID 000BBD21 DEVARCH 47701A01 DEVTYPE 43 ITM
[0][5]: E0041000 CID B105900D PID 002BBD21 DEVARCH 47724A13 DEVTYPE 13 ETM
[0][6]: E0042000 CID B105900D PID 000BBD21 DEVARCH 47701A14 DEVTYPE 14 CSS600-CTI
Memory zones:
  Zone: "Default" Description: Default access mode
Cortex-M33 identified.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I've noticed this behavior has happened twice (in two boards). I really want to believe this has nothing to do with the LCD, since it would place the responsibility of this not working onto NXP/Adafruit hands and faulty design.&lt;/P&gt;&lt;P&gt;Has anyone experienced something like this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Dec 2024 12:21:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2012840#M2172</guid>
      <dc:creator>nguterresn</dc:creator>
      <dc:date>2024-12-12T12:21:12Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013084#M2176</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Are you able to write on flash?&lt;/P&gt;
&lt;P&gt;Do you recall what was the last application you were able to flash?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Dec 2024 18:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013084#M2176</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-12-12T18:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013468#M2182</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;blhost --port /dev/tty.usbmodem0010663191941 get-property 0x19 0x09
Response status = 0 (0x0) Success.
Response word 1 = 31 (0x1f)
Response word 2 = 134217728 (0x8000000)
Response word 3 = 65536 (0x10000)
Response word 4 = 256 (0x100)
Response word 5 = 4096 (0x1000)
Response word 6 = 32768 (0x8000)
External Memory Attributes = Start Address: 0x08000000, Total Size:    64.0 MiB, Page Size:     256 B, Sector Size:   4.0 kiB, Block Size:    32.0 kiB&lt;/LI-CODE&gt;&lt;LI-CODE lang="markup"&gt;blhost --port /dev/tty.usbmodem0010663191941 read-memory 0x08000400 100
Reading memory  [####################################]  100%
46 42 00 00 00 00 00 00 00 00 01 03 03 00 01 00
00 00 01 02 00 00 40 c7 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 01 04 07 00 00 00 00 00 00 00 00 00 00 00
00 04 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00
Response status = 0 (0x0) Success.
Response word 1 = 100 (0x64)
Read 100 of 100 bytes.&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;FCB (@x400) looks odd!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;blhost --port /dev/tty.usbmodem0010663191941 get-property 0x11              
Response status = 0 (0x0) Success.
Response word 1 = 1520786085 (0x5aa55aa5)
Response word 2 = 3 (0x3)
Security State = UNSECURE&lt;/LI-CODE&gt;&lt;LI-CODE lang="markup"&gt;blhost --port /dev/tty.usbmodem0010663191941 get-property 0x0a              
Response status = 0 (0x0) Success.
Response word 1 = 1 (0x1)
Verify Writes = ON&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;I'm not able to write using blhost, but with JLink:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;blhost --port /dev/tty.usbmodem0010663191941 fill-memory 0x08001000 10 0x01 
Response status = 10203 (0x27db) Memory Cumulative Write.&lt;/LI-CODE&gt;&lt;LI-CODE lang="markup"&gt;blhost --port /dev/tty.usbmodem0010663191941 write-memory 0x08000000 {{aabbccdd}}
Writing memory  [####################################]  100%
Response status = 10203 (0x27db) Memory Cumulative Write.&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;Write1 0x08001000, 0x01
Writing 01 -&amp;gt; 08001000&lt;/LI-CODE&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;mem8  0x08001000, 10
08001000 = 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 &lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;gt;&amp;nbsp;Do you recall what was the last application you were able to flash?&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;It was probably the zephyr sample Blinky for this board. But can't be 100% sure.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 08:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013468#M2182</guid>
      <dc:creator>nguterresn</dc:creator>
      <dc:date>2024-12-13T08:49:57Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013471#M2183</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;erase
No address range specified, 'Erase Chip' will be executed
'erase': Performing implicit reset &amp;amp; halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 113ms
Erasing device...
J-Link: Flash download: Only internal flash banks will be erased.
To enable erasing of other flash banks like QSPI or CFI, it needs to be enabled via "exec EnableEraseAllFlashBanks"
J-Link: Flash download: Total time needed: 1.482s (Prepare: 0.199s, Compare: 0.000s, Erase: 1.176s, Program: 0.000s, Verify: 0.000s, Restore: 0.106s)
Erasing done.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;r
Reset delay: 0 ms
Reset type NORMAL: Resets core &amp;amp; peripherals via SYSRESETREQ &amp;amp; VECTRESET bit.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 119ms&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;After erasing, this is the data at 0x0800_0000:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;mem8  0x08001000, 10
08001000 = 01 4B 0C 10 ED FC 05 18 31 14 0A 18 D9 FC 05 18 &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;I really don't know what's going on.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 08:52:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013471#M2183</guid>
      <dc:creator>nguterresn</dc:creator>
      <dc:date>2024-12-13T08:52:48Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013476#M2184</link>
      <description>&lt;P&gt;&amp;nbsp;I also have the feeling the JLink is targeting the secure zone (0x1800_0000) whereas the blhost is targeting the non-secure zone (0x0800_0000)&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;erase
No address range specified, 'Erase Chip' will be executed
'erase': Performing implicit reset &amp;amp; halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 113ms
Erasing device...
J-Link: Flash download: Only internal flash banks will be erased.
To enable erasing of other flash banks like QSPI or CFI, it needs to be enabled via "exec EnableEraseAllFlashBanks"
J-Link: Flash download: Total time needed: 1.482s (Prepare: 0.199s, Compare: 0.000s, Erase: 1.176s, Program: 0.000s, Verify: 0.000s, Restore: 0.106s)
Erasing done.
J-Link&amp;gt;r
Reset delay: 0 ms
Reset type NORMAL: Resets core &amp;amp; peripherals via SYSRESETREQ &amp;amp; VECTRESET bit.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 119ms
J-Link&amp;gt;mem8  0x08001000, 10
08001000 = 01 4B 0C 10 ED FC 05 18 31 14 0A 18 D9 FC 05 18 
J-Link&amp;gt;mem8  0x18001000, 10
18001000 = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 &lt;/LI-CODE&gt;</description>
      <pubDate>Fri, 13 Dec 2024 08:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013476#M2184</guid>
      <dc:creator>nguterresn</dc:creator>
      <dc:date>2024-12-13T08:56:31Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013487#M2185</link>
      <description>&lt;P&gt;This also happens when trying to load an image to flash:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;blhost --port /dev/tty.usbmodem0010663191941 flash-image /Users/nunoguterres/mcu-expresso/RW612_Project/Debug/RW612_Project.hex erase 0x09
WARNING:spsdk.mboot.mcuboot:Note: memoryId is not required when accessing mapped external memory (149ms since start, mcuboot.py:1782)
Response status = 20106 (0x4e8a) FlexSPINOR: Command Failure.
blhost --port /dev/tty.usbmodem0010663191941 load-image /Users/nunoguterres/mcu-expresso/RW612_Project/Debug/RW612_Project.bin
Loading image  [------------------------------------]    0%ERROR:spsdk.mboot.mcuboot:RX: No Response, Timeout Error ! (5142ms since start, mcuboot.py:242)

McuBootConnectionError: MBoot: Connection issue -&amp;gt; No Response from Device
See debug log file: /Users/nunoguterres/Library/Logs/spsdk/2.4.0/debug.log for more info&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 09:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013487#M2185</guid>
      <dc:creator>nguterresn</dc:creator>
      <dc:date>2024-12-13T09:06:02Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013587#M2187</link>
      <description>&lt;P&gt;Another update.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I built a binary and skipped the validation (L2, the one causing the error). The board flashes BUT, it still doesn't run properly.&lt;/P&gt;&lt;P&gt;So, I downloaded (through Jlink save bbin command) the flashed program inside the rw612. It matches the one I tried to flash sniping the verification. So, my guess now is that the Bootloader (boot ROM) is pointing to the secure area (0x1800_0000) instead of pointing to the non-secure area (0x0800_0000). This guess gains traction with the fact the the default zephyr configuration has the following options:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;CONFIG_ARM_MPU=y
CONFIG_HW_STACK_PROTECTION=y
CONFIG_TRUSTED_EXECUTION_SECURE=y&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 12:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013587#M2187</guid>
      <dc:creator>nguterresn</dc:creator>
      <dc:date>2024-12-13T12:00:53Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013629#M2189</link>
      <description>&lt;P&gt;Here is a list of all the boot registers/fuses&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;shadowregs -i jlink -f rw612 printregs                  
  #   Interface   Id           Description             
-------------------------------------------------------
  0   Jlink       1066319194   Segger J-Link MCU-Link  
Register Name:        LOCK_CFG0
Register value:       0x2000
Register raw value:   0x2000

Register Name:        LOCK_CFG1
Register value:       0x0000
Register raw value:   0x0000

Register Name:        LOCK_CFG2
Register value:       0x000B
Register raw value:   0x000B

Register Name:        BOOT_CFG0
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG1
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG2
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG3
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG4
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG5
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        BOOT_CFG6
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        SEC_BOOT_CFG0
Register value:       0x0000
Register raw value:   0x0000

Register Name:        SEC_BOOT_CFG1
Register value:       0x0000
Register raw value:   0x0000

Register Name:        SEC_BOOT_CFG2
Register value:       0x0000
Register raw value:   0x0000

Register Name:        SEC_BOOT_CFG3
Register value:       0x0000
Register raw value:   0x0000

Register Name:        SEC_BOOT_CFG4
Register value:       0x0000
Register raw value:   0x0000

Register Name:        SEC_BOOT_CFG5
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        SEC_BOOT_CFG6
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        SEC_BOOT_CFG7
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        SEC_BOOT_CFG8
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        DCFG_CC_SOCU_NS
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        DCFG_CC_SOCU
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        LIFE_CYCLE_STATE
Register value:       0x0303
Register raw value:   0x0303

Register Name:        CUST_SK_MK[31:0]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[63:32]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[95:64]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[127:96]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[159:128]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[191:160]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[223:192]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[255:224]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[287:256]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[319:288]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[351:320]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        CUST_SK_MK[383:352]
Register value:       0x00000000
Register raw value:   0x00000000

Register Name:        RKTH
Register value:       0000000000000000000000000000000000000000000000000000000000000000
Register raw value:   0000000000000000000000000000000000000000000000000000000000000000&lt;/LI-CODE&gt;</description>
      <pubDate>Fri, 13 Dec 2024 13:24:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2013629#M2189</guid>
      <dc:creator>nguterresn</dc:creator>
      <dc:date>2024-12-13T13:24:56Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2014602#M2195</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I haven't seen a similar problem before.&lt;BR /&gt;&lt;BR /&gt;Are you able to execute a mass erase?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Mon, 16 Dec 2024 16:48:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2014602#M2195</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-12-16T16:48:17Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2014990#M2199</link>
      <description>&lt;P&gt;Hi, yes.&lt;/P&gt;&lt;P&gt;In theory, yes. Mass erase works, at least the command doesn't fail.&lt;/P&gt;&lt;P&gt;However, it doesn't seem to do anything.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any other idea? We have a few more boards but are a bit afraid to test it out due to the instability state of this board.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Dec 2024 07:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2014990#M2199</guid>
      <dc:creator>nguterresn</dc:creator>
      <dc:date>2024-12-17T07:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2019744#M2265</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Are you able to execute a mass erase from MCUXpresso?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Dec 2024 16:51:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2019744#M2265</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-12-26T16:51:18Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2023102#M2302</link>
      <description>&lt;P&gt;Yes. The program finishes the mass erase process but doesn't change anything, I still can't flash.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jan 2025 08:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2023102#M2302</guid>
      <dc:creator>nguterresn</dc:creator>
      <dc:date>2025-01-07T08:26:28Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2056474#M2593</link>
      <description>&lt;P&gt;I ran into this same problem when working with FRDM-RW612 boards. I encountered this problem once and was able to reproduce it on another board. It seems that attempting to flash the 0x18000000-0x1FFFFFFF section using zephyr stops the board from being able to re-flashed.&lt;/P&gt;&lt;P&gt;Here are the steps I used to reproduce this problem:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Start with a&amp;nbsp;FRDM-RW612 board fresh out of the box.&lt;/LI&gt;&lt;LI&gt;Build&amp;nbsp;frdmrw612_hello_world example in MCUXpresso IDE v11.10.0.&lt;/LI&gt;&lt;LI&gt;Flash&amp;nbsp;frdmrw612_hello_world onto the board using JLink v7.98h triggered via MCUXpresso. Flash is successful.&lt;/LI&gt;&lt;LI&gt;Run&amp;nbsp;frdmrw612_hello_world a few times and see "hello world." message appear in the serial terminal.&lt;/LI&gt;&lt;LI&gt;In a separate window, pull the latest changes from the &lt;A href="https://github.com/zephyrproject-rtos/zephyr" target="_self"&gt;Zephyr Project&lt;/A&gt; main branch and initialize west.&lt;/LI&gt;&lt;LI&gt;Using west, build Zephyr example "samples/hello_world" for the "frdm_rw612" board configuration.&amp;nbsp;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="javascript"&gt;west build -b frdm_rw612 "samples/hello_world"​&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Using west, flash the FRDM RW612 board (adding verbosity flag for debug messages). This fails with the "Verification failed @ address 0x18000000" error reported above.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="javascript"&gt;west -v flash​&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Try reflashing board using the&amp;nbsp;frdmrw612_hello_world in MCUXpresso. This now fails with&amp;nbsp;"Verification failed @ address 0x08000000" error reported above.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Things I've tried to restore device to a usable state:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Mass erase (this seems to no longer work)&lt;/LI&gt;&lt;LI&gt;Flash using an external JLink debugger (this yields the same results as using the MCU Link)&lt;/LI&gt;&lt;LI&gt;Running MCU-Link installer scripts to update firmware&lt;/LI&gt;&lt;LI&gt;Power cycling with different jumper configurations&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Wed, 05 Mar 2025 17:51:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2056474#M2593</guid>
      <dc:creator>jmitchell</dc:creator>
      <dc:date>2025-03-05T17:51:58Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2057252#M2603</link>
      <description>&lt;P&gt;Let me check.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Mar 2025 17:34:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2057252#M2603</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2025-03-06T17:34:29Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058048#M2611</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am having some dependency issues with the&amp;nbsp;&lt;EM&gt;west flash&lt;/EM&gt; command; I will try to solve them and test it.&lt;/P&gt;
&lt;P&gt;Meanwhile, I tested using the J-Link command line to flash it, and the example is able to boot. Does this also happen on your side?&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;*** Booting Zephyr OS build v4.1.0-rc3-147-gfb4bb5d7688f ***
Hello World! frdm_rw612/rw612&lt;/LI-CODE&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Mar 2025 17:19:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058048#M2611</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2025-03-07T17:19:46Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058055#M2612</link>
      <description>&lt;P&gt;UPDATE:&lt;/P&gt;
&lt;P&gt;I just solve the dependency issues. I am able to flash using&amp;nbsp;&lt;EM&gt;west flash&lt;/EM&gt; without problem.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;hello world.
hello world.
hello world.
hello world.
hello world.
hello world.
*** Booting Zephyr OS build v4.1.0-rc3-147-gfb4bb5d7688f ***
Hello World! frdm_rw612/rw612
&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Flash log:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;C:\zephyrproject\zephyr\samples\hello_world&amp;gt;west flash
-- west flash: rebuilding
ninja: no work to do.
-- west flash: using runner jlink
-- runners.jlink: reset after flashing requested
-- runners.jlink: JLink version: 7.96c
-- runners.jlink: Flashing file: C:\zephyrproject\zephyr\samples\hello_world\build\zephyr\zephyr.bin

C:\zephyrproject\zephyr\samples\hello_world&amp;gt;&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For those that can't use the west flash command, I did the following:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;pip install -U -r scripts\requirements.txt&lt;/LI-CODE&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Mar 2025 17:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058055#M2612</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2025-03-07T17:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058056#M2613</link>
      <description>&lt;P&gt;What commands did you use on the JLink command line? Essentially how Zephyr is trying to flash the board is by generating a JLink commander script file with the following contents (some path names removed).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Generated commander script file:&lt;/P&gt;&lt;LI-CODE lang="javascript"&gt;ExitOnError 1
r
LE
loadfile "&amp;lt;path_to_workspace&amp;gt;\build\zephyr\zephyr.bin" 0x18000000
r
g
writeDP 1 0
readDP 1
q&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The command being run:&lt;/P&gt;&lt;LI-CODE lang="javascript"&gt;'C:\Program Files\SEGGER\JLink\JLink.exe' -nogui 1 -if swd -speed auto -device RW612 -CommanderScript '&amp;lt;the_commander_script_file&amp;gt;' -nogui 1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Mar 2025 17:30:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058056#M2613</guid>
      <dc:creator>jmitchell</dc:creator>
      <dc:date>2025-03-07T17:30:11Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058060#M2614</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the J-Link CLI I used:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;loadbin hello_world\build\zephyr\zephyr.bin 0x08000000&lt;/LI-CODE&gt;</description>
      <pubDate>Fri, 07 Mar 2025 17:44:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058060#M2614</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2025-03-07T17:44:16Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058061#M2615</link>
      <description>&lt;P&gt;Right, so the thing we're trying to troubleshoot here is loadbin to address "0x18000000" and how to recover from that.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Mar 2025 17:47:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058061#M2615</guid>
      <dc:creator>jmitchell</dc:creator>
      <dc:date>2025-03-07T17:47:15Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 Error: Verification failed @ address 0x18000000</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058091#M2617</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Even on address 0x18000000 I didn't find any issue.&lt;/P&gt;
&lt;P&gt;Please find my log down below.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;PS C:\zephyrproject\zephyr\samples\hello_world&amp;gt; west build -bfrdm_rw612 --pristine
-- west build: making build dir C:\zephyrproject\zephyr\samples\hello_world\build pristine
-- west build: generating a build system
Loading Zephyr default modules (Zephyr base).
-- Application: C:/zephyrproject/zephyr/samples/hello_world
-- CMake version: 3.28.1
-- Found Python3: C:/Users/Daniel/AppData/Local/Programs/Python/Python311/python.exe (found suitable version "3.11.9", minimum required is "3.10") found components: Interpreter
-- Cache files will be written to: C:/zephyrproject/zephyr/.cache
-- Zephyr version: 4.1.0-rc3 (C:/zephyrproject/zephyr)
-- Found west (found suitable version "1.3.0", minimum required is "0.14.0")
-- Board: frdm_rw612, qualifiers: rw612
-- ZEPHYR_TOOLCHAIN_VARIANT not set, trying to locate Zephyr SDK
-- Found host-tools: zephyr 0.17.0 (C:/Users/Daniel/zephyr-sdk-0.17.0)
-- Found toolchain: zephyr 0.17.0 (C:/Users/Daniel/zephyr-sdk-0.17.0)
-- Found Dtc: C:/Users/Daniel/.mcuxpressotools/dtc-msys2/tools/usr/bin/dtc.exe (found suitable version "1.6.1", minimum required is "1.4.6")
-- Found BOARD.dts: C:/zephyrproject/zephyr/boards/nxp/frdm_rw612/frdm_rw612.dts
-- Generated zephyr.dts: C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/zephyr.dts
-- Generated pickled edt: C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/edt.pickle
-- Generated devicetree_generated.h: C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/include/generated/zephyr/devicetree_generated.h
-- Including generated dts.cmake file: C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/dts.cmake
Parsing C:/zephyrproject/zephyr/Kconfig
Loaded configuration 'C:/zephyrproject/zephyr/boards/nxp/frdm_rw612/frdm_rw612_defconfig'
Merged configuration 'C:/zephyrproject/zephyr/samples/hello_world/prj.conf'
Configuration saved to 'C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/.config'
Kconfig header saved to 'C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/include/generated/zephyr/autoconf.h'
-- Found GnuLd: c:/users/Daniel/zephyr-sdk-0.17.0/arm-zephyr-eabi/arm-zephyr-eabi/bin/ld.bfd.exe (found version "2.38")
-- The C compiler identification is GNU 12.2.0
-- The CXX compiler identification is GNU 12.2.0
-- The ASM compiler identification is GNU
-- Found assembler: C:/Users/Daniel/zephyr-sdk-0.17.0/arm-zephyr-eabi/bin/arm-zephyr-eabi-gcc.exe
Load components for RW612:
driver_common component is included.
driver_reset component is included.
device_CMSIS component is included.
CMSIS_Include_core_cm component is included.
device_startup component is included.
driver_lpc_gpio component is included.
driver_pint component is included.
driver_inputmux component is included.
driver_inputmux_connections component is included.
driver_ostimer component is included.
driver_flexcomm component is included.
driver_flexcomm_usart component is included.
driver_cache_cache64 component is included.
component_osa_zephyr component is included from C:/zephyrproject/modules/hal/nxp/mcux/mcux-sdk/components/osa/set_component_osa.cmake.
-- Configuring done (14.4s)
-- Generating done (0.5s)
-- Build files have been written to: C:/zephyrproject/zephyr/samples/hello_world/build
-- west build: building application
[1/147] Generating include/generated/zephyr/version.h
-- Zephyr version: 4.1.0-rc3 (C:/zephyrproject/zephyr), build: v4.1.0-rc3-147-gfb4bb5d7688f
[147/147] Linking C executable zephyr\zephyr.elf
Memory region         Used Size  Region Size  %age Used
           FLASH:       27912 B        64 MB      0.04%
             RAM:        6952 B       960 KB      0.71%
            SMU1:        510 KB       510 KB    100.00%
            SMU2:        140 KB       140 KB    100.00%
        IDT_LIST:          0 GB        32 KB      0.00%
Generating files from C:/zephyrproject/zephyr/samples/hello_world/build/zephyr/zephyr.elf for board: frdm_rw612
PS C:\zephyrproject\zephyr\samples\hello_world&amp;gt;
PS C:\zephyrproject\zephyr\samples\hello_world&amp;gt; west -v flash
-- west flash: rebuilding
cmake version 3.28.1 is OK; minimum version is 3.13.1
Running CMake: 'C:\Users\Daniel\.mcuxpressotools\cmake-3.28.1-windows-x86_64\bin\cmake.EXE' --build 'C:\zephyrproject\zephyr\samples\hello_world\build'
ninja: no work to do.
-- west flash: using runner jlink
-- runners.jlink: reset after flashing requested
runners.jlink: JLINKARM_GetDLLVersion()=79603
-- runners.jlink: JLink version: 7.96c
runners.jlink: JLink commander script:
ExitOnError 1
r
LE
loadfile "C:\zephyrproject\zephyr\samples\hello_world\build\zephyr\zephyr.bin" 0x18000000
r
g
writeDP 1 0
readDP 1
q
-- runners.jlink: Flashing file: C:\zephyrproject\zephyr\samples\hello_world\build\zephyr\zephyr.bin
runners.jlink: 'C:\Program Files\SEGGER\JLink\JLink.exe' -nogui 1 -if swd -speed auto -device RW612 -CommanderScript 'C:\Users\Daniel\AppData\Local\Temp\tmp4uj63qihjlink\runner.jlink' -nogui 1
SEGGER J-Link Commander V7.96c (Compiled Apr  2 2024 12:35:23)
DLL version V7.96c, compiled Apr  2 2024 12:34:28


J-Link Command File read successfully.
Processing script file...
J-Link&amp;gt;ExitOnError 1
J-Link Commander will now exit on Error
J-Link&amp;gt;r
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link MCU-Link V1 compiled Oct  9 2024 11:01:41
Hardware version: V1.00
J-Link uptime (since boot): 0d 00h 10m 38s
S/N: 1060061514
USB speed mode: High speed (480 MBit/s)
VTref=3.300V
Target connection not established yet but required for command.
Device "RW612" selected.


Connecting to target via SWD
InitTarget() start
SWD selected. Executing JTAG -&amp;gt; SWD switching sequence.
DAP initialized successfully.
  DMAP_REG_ID: DM-AP IDCODE detected: 0x002A0000
  DHCSR: 0xFFFFFFFF
ROM entered ISP command handling loop. Re-enable the debug access.
InitTarget() end - Took 22.1ms
Found SW-DP with ID 0x6BA02477
DPIDR: 0x6BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x84770001)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)
Feature set: Mainline
Cache: No cache
Found Cortex-M33 r0p4, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
Security extension: implemented
Secure debug: enabled
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105900D PID 000BBD21 DEVARCH 47702A04 DEVTYPE 00 Cortex-M33
[0][1]: E0001000 CID B105900D PID 000BBD21 DEVARCH 47701A02 DEVTYPE 00 DWT
[0][2]: E0002000 CID B105900D PID 000BBD21 DEVARCH 47701A03 DEVTYPE 00 FPB
[0][3]: E0000000 CID B105900D PID 000BBD21 DEVARCH 47701A01 DEVTYPE 43 ITM
[0][5]: E0041000 CID B105900D PID 002BBD21 DEVARCH 47724A13 DEVTYPE 13 ETM
[0][6]: E0042000 CID B105900D PID 000BBD21 DEVARCH 47701A14 DEVTYPE 14 CSS600-CTI
Memory zones:
  Zone: "Default" Description: Default access mode
Cortex-M33 identified.
Reset delay: 0 ms
Reset type NORMAL: Resets core &amp;amp; peripherals via SYSRESETREQ &amp;amp; VECTRESET bit.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 134ms
J-Link&amp;gt;LE
J-Link&amp;gt;loadfile "C:\zephyrproject\zephyr\samples\hello_world\build\zephyr\zephyr.bin" 0x18000000
'loadfile': Performing implicit reset &amp;amp; halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
  MSPLIM cleared
ResetTarget() end - Took 123ms
Downloading file [C:\zephyrproject\zephyr\samples\hello_world\build\zephyr\zephyr.bin]...
Comparing flash   [100%] Done.
Erasing flash     [100%] Done.
Programming flash [100%] Done.
Verifying flash   [100%] Done.
J-Link: Flash download: Bank 1 @ 0x18000000: 1 range affected (65536 bytes)
J-Link: Flash download: Total: 1.116s (Prepare: 0.280s, Compare: 0.106s, Erase: 0.268s, Program: 0.216s, Verify: 0.110s, Restore: 0.132s)
J-Link: Flash download: Program speed: 296 KB/s
O.K.
J-Link&amp;gt;r
Reset delay: 0 ms
Reset type NORMAL: Resets core &amp;amp; peripherals via SYSRESETREQ &amp;amp; VECTRESET bit.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
  MSPLIM cleared
ResetTarget() end - Took 155ms
J-Link&amp;gt;g
Memory map 'after startup completion point' is active
J-Link&amp;gt;writeDP 1 0
Writing DP register 1 = 0x00000000 (0 write repetitions needed)
J-Link&amp;gt;readDP 1
Reading DP register 1 = 0x00000040 (0 read repetitions needed)
J-Link&amp;gt;q

Script processing completed.

PS C:\zephyrproject\zephyr\samples\hello_world&amp;gt;&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Danie&lt;/P&gt;</description>
      <pubDate>Fri, 07 Mar 2025 19:42:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/FRDM-RW612-Error-Verification-failed-address-0x18000000/m-p/2058091#M2617</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2025-03-07T19:42:00Z</dc:date>
    </item>
  </channel>
</rss>