<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCXC and EEPROM emulation in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXC-and-EEPROM-emulation/m-p/2005888#M2096</link>
    <description>&lt;P&gt;Hi there,&lt;BR /&gt;Please, Is able to use internal FLASH memory in the MCXC242 as a emulated EEPROM/Non-Volatile Memory for store users application settings (few bytes) during running application?&lt;BR /&gt;In some LPC microcontrollers is API for In-Application programming which make it possible. How about MCXC242?&lt;BR /&gt;Or one and only way is to connect external EEPROM?&lt;/P&gt;&lt;P&gt;Thanks.&lt;BR /&gt;Regards,&lt;BR /&gt;Peter&lt;/P&gt;</description>
    <pubDate>Tue, 03 Dec 2024 09:04:55 GMT</pubDate>
    <dc:creator>pepoja</dc:creator>
    <dc:date>2024-12-03T09:04:55Z</dc:date>
    <item>
      <title>MCXC and EEPROM emulation</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXC-and-EEPROM-emulation/m-p/2005888#M2096</link>
      <description>&lt;P&gt;Hi there,&lt;BR /&gt;Please, Is able to use internal FLASH memory in the MCXC242 as a emulated EEPROM/Non-Volatile Memory for store users application settings (few bytes) during running application?&lt;BR /&gt;In some LPC microcontrollers is API for In-Application programming which make it possible. How about MCXC242?&lt;BR /&gt;Or one and only way is to connect external EEPROM?&lt;/P&gt;&lt;P&gt;Thanks.&lt;BR /&gt;Regards,&lt;BR /&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 03 Dec 2024 09:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXC-and-EEPROM-emulation/m-p/2005888#M2096</guid>
      <dc:creator>pepoja</dc:creator>
      <dc:date>2024-12-03T09:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: MCXC and EEPROM emulation</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXC-and-EEPROM-emulation/m-p/2008074#M2111</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/116244"&gt;@pepoja&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you mean software emulate EEPROM, yes, mcxc242 supports&lt;SPAN&gt;&amp;nbsp;emulated EEPROM.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;You can refer to:&amp;nbsp;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN13542.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com.cn/docs/en/application-note/AN13542.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 26 Dec 2024 07:22:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXC-and-EEPROM-emulation/m-p/2008074#M2111</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-12-26T07:22:21Z</dc:date>
    </item>
  </channel>
</rss>