<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT600/700 GPIO Slew Rate Control in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/RT600-700-GPIO-Slew-Rate-Control/m-p/1845814#M209</link>
    <description>&lt;P&gt;Hi Aaron,&lt;/P&gt;
&lt;P&gt;as a part of MCUxpresso Config Tools, there is Pin tool available. The tool allows to generate code for pin routing and also for electrical pin configuration.&lt;/P&gt;
&lt;P&gt;MCUxpresso Config Tools can be downloaded as standalone tool or they are also integrated into MCUxpresso IDE.&lt;/P&gt;
&lt;P&gt;Hope this help&lt;/P&gt;</description>
    <pubDate>Fri, 12 Apr 2024 06:10:16 GMT</pubDate>
    <dc:creator>marek-trmac</dc:creator>
    <dc:date>2024-04-12T06:10:16Z</dc:date>
    <item>
      <title>RT600/700 GPIO Slew Rate Control</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/RT600-700-GPIO-Slew-Rate-Control/m-p/1845506#M208</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;In the RT600 and RT700 reference manual there is a GPIO setting to configure a GPIO's slew rate. This setting is either "disabled (default)" or "enabled." How is this setting tuning the internal driving circuit of the GPIO in its disabled and enabled state?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="434544897_2453569051697205_5100220487723441969_n.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/273267iDD7DFBBF96A2318E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="434544897_2453569051697205_5100220487723441969_n.png" alt="434544897_2453569051697205_5100220487723441969_n.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;434544897_2453569051697205_5100220487723441969_n.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;</description>
      <pubDate>Thu, 11 Apr 2024 21:39:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/RT600-700-GPIO-Slew-Rate-Control/m-p/1845506#M208</guid>
      <dc:creator>aaronchin</dc:creator>
      <dc:date>2024-04-11T21:39:09Z</dc:date>
    </item>
    <item>
      <title>Re: RT600/700 GPIO Slew Rate Control</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/RT600-700-GPIO-Slew-Rate-Control/m-p/1845814#M209</link>
      <description>&lt;P&gt;Hi Aaron,&lt;/P&gt;
&lt;P&gt;as a part of MCUxpresso Config Tools, there is Pin tool available. The tool allows to generate code for pin routing and also for electrical pin configuration.&lt;/P&gt;
&lt;P&gt;MCUxpresso Config Tools can be downloaded as standalone tool or they are also integrated into MCUxpresso IDE.&lt;/P&gt;
&lt;P&gt;Hope this help&lt;/P&gt;</description>
      <pubDate>Fri, 12 Apr 2024 06:10:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/RT600-700-GPIO-Slew-Rate-Control/m-p/1845814#M209</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2024-04-12T06:10:16Z</dc:date>
    </item>
  </channel>
</rss>