<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 回复： The start signal is not responding of PT2001 in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/The-start-signal-is-not-responding-of-PT2001/m-p/1994489#M1984</link>
    <description>&lt;P&gt;Hi LexLiu,&lt;/P&gt;&lt;P&gt;Thank you for your help. Due to our special engineering requirements, we may need to connect 1, 2, 3, or 4 fuel injectors in actual use. My current demo only connects 1 and 2 fuel injectors. During the self-test process, the Bootstrap check's rxData=send_stngle_SPI_Cmd (READ, ioobuttostrap_charged, 0x00); I read 0xD394, and this self-test failed, so I annotated this check. May I ask if this is related to the fact that the startup signal is not working after me? Additionally, how can I configure an application that meets my requirement for connecting the number of fuel injectors freely?&lt;/P&gt;</description>
    <pubDate>Thu, 14 Nov 2024 08:52:15 GMT</pubDate>
    <dc:creator>richer</dc:creator>
    <dc:date>2024-11-14T08:52:15Z</dc:date>
    <item>
      <title>The start signal is not responding of PT2001</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/The-start-signal-is-not-responding-of-PT2001/m-p/1993728#M1974</link>
      <description>&lt;P&gt;We designed the circuit using the recommended circuit diagram from PT2001 and generated microcode using the default code from PT2001Dev studio. The current problem is that the BOOST voltage can be boosted to 65V normally, but after driving the DRVEN and START signals, the fuel injector has no response. How can I troubleshoot this situation?&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 12:56:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/The-start-signal-is-not-responding-of-PT2001/m-p/1993728#M1974</guid>
      <dc:creator>richer</dc:creator>
      <dc:date>2024-11-13T12:56:46Z</dc:date>
    </item>
    <item>
      <title>Re: The start signal is not responding of PT2001</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/The-start-signal-is-not-responding-of-PT2001/m-p/1993915#M1975</link>
      <description>&lt;P&gt;Hi Lex (&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199702" target="_blank"&gt;@LexLiu&lt;/A&gt;),&lt;/P&gt;
&lt;P&gt;Could you please help with this question regarding the PT2001 from&amp;nbsp;Beijing Yi'an Hengrui Technology?&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 18:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/The-start-signal-is-not-responding-of-PT2001/m-p/1993915#M1975</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-11-13T18:33:17Z</dc:date>
    </item>
    <item>
      <title>回复： The start signal is not responding of PT2001</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/The-start-signal-is-not-responding-of-PT2001/m-p/1994489#M1984</link>
      <description>&lt;P&gt;Hi LexLiu,&lt;/P&gt;&lt;P&gt;Thank you for your help. Due to our special engineering requirements, we may need to connect 1, 2, 3, or 4 fuel injectors in actual use. My current demo only connects 1 and 2 fuel injectors. During the self-test process, the Bootstrap check's rxData=send_stngle_SPI_Cmd (READ, ioobuttostrap_charged, 0x00); I read 0xD394, and this self-test failed, so I annotated this check. May I ask if this is related to the fact that the startup signal is not working after me? Additionally, how can I configure an application that meets my requirement for connecting the number of fuel injectors freely?&lt;/P&gt;</description>
      <pubDate>Thu, 14 Nov 2024 08:52:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/The-start-signal-is-not-responding-of-PT2001/m-p/1994489#M1984</guid>
      <dc:creator>richer</dc:creator>
      <dc:date>2024-11-14T08:52:15Z</dc:date>
    </item>
  </channel>
</rss>