<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: Obsolescence &amp;quot;MC9RS08LA8CLF&amp;quot;</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1993313#M1970</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As Jennie recommended, you can use MCXC44x family, it has 64 pin BGA or 64 pins LQFP package, both package have the LCD module&lt;/P&gt;
&lt;P&gt;Regarding the LCD, it can support 24x8 or 28x4 segment LCD, in other words, there are 32 LCD pins which can be configured as either front plane signals or back plane signals, it supports up to 8 back planes.&lt;/P&gt;
&lt;P&gt;This is the website of MCXC44x family:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-c-series-microcontrollers/mcx-c14x-24x-44x-mcus-with-arm-cortex-m0-plus-entry-level-mcus-with-usb-segment-lcd-and-classical-peripherals:MCX-C14x-24x-44x?page=2&amp;amp;nrnd=false" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-c-series-microcontrollers/mcx-c14x-24x-44x-mcus-with-arm-cortex-m0-plus-entry-level-mcus-with-usb-segment-lcd-and-classical-peripherals:MCX-C14x-24x-44x?page=2&amp;amp;nrnd=false&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1731470077593.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310184iF50AB723D91AD6ED/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1731470077593.png" alt="xiangjun_rong_0-1731470077593.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Wed, 13 Nov 2024 03:56:22 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-11-13T03:56:22Z</dc:date>
    <item>
      <title>Obsolescence "MC9RS08LA8CLF"</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1989986#M1932</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is there a uC fully compatible with "MC9RS08LA8CLF" (HW and SW) ?&lt;BR /&gt;I saw that to migrate between "MC9RS08LA8CLF" and "MC9S08LL8CLF" SW changes are needed (for example the pin-out of the LCD controller pins are not the same).&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Demetrio Magrin&lt;/P&gt;</description>
      <pubDate>Thu, 07 Nov 2024 08:31:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1989986#M1932</guid>
      <dc:creator>DemetrioMagrin</dc:creator>
      <dc:date>2024-11-07T08:31:39Z</dc:date>
    </item>
    <item>
      <title>Re: Obsolescence "MC9RS08LA8CLF"</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1990137#M1934</link>
      <description>&lt;P&gt;Hello&amp;nbsp;DemetrioMagrin,&lt;/P&gt;
&lt;P&gt;There is no pin to pin replacement for "MC9RS08LA8CLF".&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you considering function replacement part MCXC04x&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-c-series-microcontrollers/mcx-c04x-mcus-with-arm-cortex-m0-plus-entry-level-mcus-with-classical-peripherals:MCX-C04x" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-c-series-microcontrollers/mcx-c04x-mcus-with-arm-cortex-m0-plus-entry-level-mcus-with-classical-peripherals:MCX-C04x&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Or LPC80x.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc800-arm-cortex-m0-plus-/lpc800-32-bit-arm-cortex-m0-plus-based-low-cost-mcu:LPC80X" target="_blank" rel="noopener"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc800-arm-cortex-m0-plus-/lpc800-32-bit-arm-cortex-m0-plus-based-low-cost-mcu:LPC80X&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If this doesn't meet your requirement. What peripherals are nencessary for you? and what is your memeory size requirement? You could let me know thus I can check it further.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Thu, 07 Nov 2024 11:01:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1990137#M1934</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2024-11-07T11:01:35Z</dc:date>
    </item>
    <item>
      <title>Re: Obsolescence "MC9RS08LA8CLF"</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1990907#M1941</link>
      <description>&lt;P&gt;Hello Mr.&amp;nbsp;&lt;SPAN&gt;Jun Zhang,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Thank you for your reply, my main requirement is not to modify the current PCB where the uC "MC9RS08LA8CLF" used has 48 pins.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Attached I have put the pin-out schematich of the current uC "MC9RS08LA8CLF" where you can see how many pins I used for the LCD controller.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;The only solution to replace the uC "MC9RS08LA8CLF" (48 pins) is to use the uC "MC9S08LL8CLF" (48 pins) by modifying the FW (different pin-out of the LCD controller).&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;If you have another solution it is welcome.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;Thank you.&lt;BR /&gt;&lt;BR /&gt;Demetrio Magrin&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Nov 2024 08:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1990907#M1941</guid>
      <dc:creator>DemetrioMagrin</dc:creator>
      <dc:date>2024-11-08T08:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: Obsolescence "MC9RS08LA8CLF"</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1993313#M1970</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As Jennie recommended, you can use MCXC44x family, it has 64 pin BGA or 64 pins LQFP package, both package have the LCD module&lt;/P&gt;
&lt;P&gt;Regarding the LCD, it can support 24x8 or 28x4 segment LCD, in other words, there are 32 LCD pins which can be configured as either front plane signals or back plane signals, it supports up to 8 back planes.&lt;/P&gt;
&lt;P&gt;This is the website of MCXC44x family:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-c-series-microcontrollers/mcx-c14x-24x-44x-mcus-with-arm-cortex-m0-plus-entry-level-mcus-with-usb-segment-lcd-and-classical-peripherals:MCX-C14x-24x-44x?page=2&amp;amp;nrnd=false" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-c-series-microcontrollers/mcx-c14x-24x-44x-mcus-with-arm-cortex-m0-plus-entry-level-mcus-with-usb-segment-lcd-and-classical-peripherals:MCX-C14x-24x-44x?page=2&amp;amp;nrnd=false&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1731470077593.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310184iF50AB723D91AD6ED/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1731470077593.png" alt="xiangjun_rong_0-1731470077593.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 03:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1993313#M1970</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-11-13T03:56:22Z</dc:date>
    </item>
    <item>
      <title>Re: Obsolescence "MC9RS08LA8CLF"</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1993494#M1972</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Thanks for the reply, as I said before my main need is not to modify the current PCB where the uC "MC9RS08LA8CLF" used has 48 pins.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt; It seems to me that the only possible solution is to replace the uC "MC9RS08LA8CLF" (48 pins) with the uC "MC9S08LL8CLF" (48 pins) by modifying the FW (different pin-out of the LCD controller).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;In order to use the "MCXC44x" family I should modify the PCB.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Thanks.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Demetrio Magrin&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 08:35:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1993494#M1972</guid>
      <dc:creator>DemetrioMagrin</dc:creator>
      <dc:date>2024-11-13T08:35:00Z</dc:date>
    </item>
    <item>
      <title>Re: Obsolescence "MC9RS08LA8CLF"</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1997658#M2010</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Okay, pls download data sheet of the two chip the &lt;SPAN class=""&gt;MC9RS08LA8CLF&lt;/SPAN&gt; and &lt;SPAN class=""&gt;"MC9S08LL8CLF,&lt;/SPAN&gt; check if they are pin to pin compatible.&lt;/P&gt;
&lt;P&gt;If they are pin to pin compatible, it is okay.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xiangjun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 03:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Obsolescence-quot-MC9RS08LA8CLF-quot/m-p/1997658#M2010</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-11-20T03:57:11Z</dc:date>
    </item>
  </channel>
</rss>